<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Kernel Panic error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-error/m-p/259948#M25758</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have exactly the same problem, very frustrating. I need to establish a working toolchain, or abandon this and find something that works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I installed the Linux VM on a Windows system.&amp;nbsp; BTE: The system REALLY should ship with an errata sheet -- just getting thru the apt updates was annoying. But set that aside.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ran the config, set in a few options, did a build, and made an SD card.&amp;nbsp; Kernel panic.&lt;/P&gt;&lt;P&gt;Examine the config about 12 times, same thing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Okay, maybe I did something horribly wrong.&amp;nbsp; Build a pristine VM, run configure and accept the defaults.&amp;nbsp; Build a new image, copy to SD card.&lt;/P&gt;&lt;P&gt;Same crap.&amp;nbsp; Boot file is attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas where to go from here ? Or should I give up ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 02 Mar 2013 18:50:56 GMT</pubDate>
    <dc:creator>carlosorriento</dc:creator>
    <dc:date>2013-03-02T18:50:56Z</dc:date>
    <item>
      <title>Kernel Panic error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-error/m-p/259943#M25753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am facing a kernel panic error when booting iMX25 PDK with SD Card. Need help to resolve this error. Screen shot is attached&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Arumugam R&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2013 05:46:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-error/m-p/259943#M25753</guid>
      <dc:creator>arumugamramasam</dc:creator>
      <dc:date>2013-02-15T05:46:37Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel Panic error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-error/m-p/259944#M25754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you share the full kernel log before the kernel panic?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2013 15:46:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-error/m-p/259944#M25754</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2013-02-15T15:46:02Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel Panic error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-error/m-p/259945#M25755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems you have a bad rootfs flashed into the SD card. For a quick test, you can try to booting via NFS.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2013 15:55:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-error/m-p/259945#M25755</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2013-02-15T15:55:12Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel Panic error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-error/m-p/259946#M25756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Please find below full log. Please let me know if you find anything wrong...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2009.08 (Jan 10 2013 - 17:01:27)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX25 at 398 MHz&lt;/P&gt;&lt;P&gt;mx25 cpu clock: 398MHz&lt;/P&gt;&lt;P&gt;ipg clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 66498560Hz&lt;/P&gt;&lt;P&gt;Board: i.MX25 MAX PDK (3DS)&lt;/P&gt;&lt;P&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;/P&gt;&lt;P&gt;DRAM:&amp;nbsp; 64 MB&lt;/P&gt;&lt;P&gt;NAND:&amp;nbsp; Unrecognized NAND Flash device.&lt;/P&gt;&lt;P&gt;256 MiB&lt;/P&gt;&lt;P&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_ESDHC: 0&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Net:&amp;nbsp;&amp;nbsp; smc911x-0 [PRIME], FEC0&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 3&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MMC read: dev # 0, block # 2048, count 4096 ... 4096 blocks read: OK&lt;/P&gt;&lt;P&gt;## Booting kernel from Legacy Image at 80800000 ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; Linux-2.6.31-207-g7286c01&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; ARM Linux Kernel Image (uncompressed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 2026988 Bytes =&amp;nbsp; 1.9 MB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Load Address: 80008000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 80008000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Loading Kernel Image ... OK&lt;/P&gt;&lt;P&gt;OK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Uncompressing Linux.............................................................&lt;/P&gt;&lt;P&gt;................................................................................&lt;/P&gt;&lt;P&gt;.. done, booting the kernel.&lt;/P&gt;&lt;P&gt;Linux version 2.6.31-207-g7286c01 (arumugam@arumugam-laptop) (gcc version 4.1.2)&lt;/P&gt;&lt;P&gt; #2 PREEMPT Mon Feb 11 16:18:16 IST 2013&lt;/P&gt;&lt;P&gt;CPU: ARM926EJ-S [41069264] revision 4 (ARMv5TEJ), cr=00053177&lt;/P&gt;&lt;P&gt;CPU: VIVT data cache, VIVT instruction cache&lt;/P&gt;&lt;P&gt;Machine: Freescale MX25 3-Stack Board&lt;/P&gt;&lt;P&gt;Memory policy: ECC disabled, Data cache writeback&lt;/P&gt;&lt;P&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 16256&lt;/P&gt;&lt;P&gt;Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p1 ip=none rootfsty&lt;/P&gt;&lt;P&gt;pe=ext2 init=/etc/inittab&lt;/P&gt;&lt;P&gt;PID hash table entries: 256 (order: 8, 1024 bytes)&lt;/P&gt;&lt;P&gt;Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)&lt;/P&gt;&lt;P&gt;Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;Memory: 64MB = 64MB total&lt;/P&gt;&lt;P&gt;Memory: 60156KB available (3768K code, 454K data, 420K init, 0K highmem)&lt;/P&gt;&lt;P&gt;NR_IRQS:272&lt;/P&gt;&lt;P&gt;MXC IRQ initialized&lt;/P&gt;&lt;P&gt;Clock input source is 24000000&lt;/P&gt;&lt;P&gt;Console: colour dummy device 80x30&lt;/P&gt;&lt;P&gt;Calibrating delay loop... 199.06 BogoMIPS (lpj=995328)&lt;/P&gt;&lt;P&gt;Mount-cache hash table entries: 512&lt;/P&gt;&lt;P&gt;CPU: Testing write buffer coherency: ok&lt;/P&gt;&lt;P&gt;regulator: core version 0.5&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 16&lt;/P&gt;&lt;P&gt;AIPS1 VA base: 0xfc000000&lt;/P&gt;&lt;P&gt;CPU is i.MX25 Revision 1.0&lt;/P&gt;&lt;P&gt;MXC GPIO hardware&lt;/P&gt;&lt;P&gt;Using SDMA I.API&lt;/P&gt;&lt;P&gt;MXC DMA API initialized&lt;/P&gt;&lt;P&gt;bio: create slab &amp;lt;bio-0&amp;gt; at 0&lt;/P&gt;&lt;P&gt;SCSI subsystem initialized&lt;/P&gt;&lt;P&gt;CSPI: mxc_spi-0 probed&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usbfs&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver hub&lt;/P&gt;&lt;P&gt;usbcore: registered new device driver usb&lt;/P&gt;&lt;P&gt;MXC I2C driver&lt;/P&gt;&lt;P&gt;regulator: REG1_BKLT: 4500 &amp;lt;--&amp;gt; 5500 mV &lt;/P&gt;&lt;P&gt;regulator: REG2_CPU: 2640 &amp;lt;--&amp;gt; 3877 mV &lt;/P&gt;&lt;P&gt;regulator: REG3_CORE: 1160 &amp;lt;--&amp;gt; 1703 mV &lt;/P&gt;&lt;P&gt;regulator: REG4_DDR: 1440 &amp;lt;--&amp;gt; 2115 mV &lt;/P&gt;&lt;P&gt;regulator: REG5_PERS: 2640 &amp;lt;--&amp;gt; 3877 mV &lt;/P&gt;&lt;P&gt;mc34704 0-0054: Loaded&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 2&lt;/P&gt;&lt;P&gt;IP route cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;/P&gt;&lt;P&gt;TCP established hash table entries: 2048 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;TCP bind hash table entries: 2048 (order: 1, 8192 bytes)&lt;/P&gt;&lt;P&gt;TCP: Hash tables configured (established 2048 bind 2048)&lt;/P&gt;&lt;P&gt;TCP reno registered&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 1&lt;/P&gt;&lt;P&gt;Bus freq driver module loaded&lt;/P&gt;&lt;P&gt;Registering the CPLD Driver&lt;/P&gt;&lt;P&gt;3-Stack Debug board detected, rev = 0x3000300&lt;/P&gt;&lt;P&gt;usb: Host 2 host (serial) registered&lt;/P&gt;&lt;P&gt;usb: DR OTG registered&lt;/P&gt;&lt;P&gt;usb: DR host (utmi) registered&lt;/P&gt;&lt;P&gt;usb: DR gadget (utmi) registered&lt;/P&gt;&lt;P&gt;i.MXC CPU frequency driver&lt;/P&gt;&lt;P&gt;JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;/P&gt;&lt;P&gt;msgmni has been set to 117&lt;/P&gt;&lt;P&gt;io scheduler noop registered&lt;/P&gt;&lt;P&gt;io scheduler anticipatory registered&lt;/P&gt;&lt;P&gt;io scheduler deadline registered&lt;/P&gt;&lt;P&gt;io scheduler cfq registered (default)&lt;/P&gt;&lt;P&gt;MXC Backlight Device mxc_lcdc_bl.0 Initialized.&lt;/P&gt;&lt;P&gt;Console: switching to colour frame buffer device 80x30&lt;/P&gt;&lt;P&gt;mxc_sdc_fb mxc_sdc_fb.0: fb0: DISP0 BG fb device registered successfully.&lt;/P&gt;&lt;P&gt;mxc_sdc_fb mxc_sdc_fb.0: fb1: DISP0 FG fb device registered successfully.&lt;/P&gt;&lt;P&gt;Serial: MXC Internal UART driver&lt;/P&gt;&lt;P&gt;mxcintuart.0: ttymxc0 at MMIO 0x43f90000 (irq = 45) is a Freescale i.MX&lt;/P&gt;&lt;P&gt;console [ttymxc0] enabled&lt;/P&gt;&lt;P&gt;mxcintuart.1: ttymxc1 at MMIO 0x43f94000 (irq = 32) is a Freescale i.MX&lt;/P&gt;&lt;P&gt;brd: module loaded&lt;/P&gt;&lt;P&gt;loop: module loaded&lt;/P&gt;&lt;P&gt;Freescale FlexCAN Driver &lt;/P&gt;&lt;P&gt;MXC MTD nand Driver 2.5&lt;/P&gt;&lt;P&gt;NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron NAND 256MiB 3,3V 8-bit&lt;/P&gt;&lt;P&gt;)&lt;/P&gt;&lt;P&gt;Unrecognized NAND Flash device.&lt;/P&gt;&lt;P&gt;Initializing USB Mass Storage driver...&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usb-storage&lt;/P&gt;&lt;P&gt;USB Mass Storage support registered.&lt;/P&gt;&lt;P&gt;MXC keypad loaded&lt;/P&gt;&lt;P&gt;input: mxckpd as /class/input/input0&lt;/P&gt;&lt;P&gt;IMXDI Realtime Clock Driver (RTC)&lt;/P&gt;&lt;P&gt;imxdi_rtc imxdi_rtc.0: rtc core: registered imxdi_rtc as rtc0&lt;/P&gt;&lt;P&gt;Linux video capture interface: v2.00&lt;/P&gt;&lt;P&gt;PMIC Character device: successfully loaded&lt;/P&gt;&lt;P&gt;i.MX ADC at 0x50030000 irq 46&lt;/P&gt;&lt;P&gt;mxsdhci: MXC Secure Digital Host Controller Interface driver&lt;/P&gt;&lt;P&gt;mxsdhci: MXC SDHCI Controller Driver. &lt;/P&gt;&lt;P&gt;mmc0: SDHCI detect irq 161 irq 9 INTERNAL DMA&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usbhid&lt;/P&gt;&lt;P&gt;usbhid: v2.6:USB HID core driver&lt;/P&gt;&lt;P&gt;Advanced Linux Sound Architecture Driver Version 1.0.20.&lt;/P&gt;&lt;P&gt;regulator: Unable to get requested regulator: VDDD&lt;/P&gt;&lt;P&gt;sgtl5000-i2c 0-000a: SGTL5000 revision 17&lt;/P&gt;&lt;P&gt;No device for DAI imx-ssi-1-0&lt;/P&gt;&lt;P&gt;No device for DAI imx-ssi-1-1&lt;/P&gt;&lt;P&gt;No device for DAI imx-ssi-2-0&lt;/P&gt;&lt;P&gt;No device for DAI imx-ssi-2-1&lt;/P&gt;&lt;P&gt;DMA Sound Buffers Allocated:UseIram=1 buf-&amp;gt;addr=78001000 buf-&amp;gt;area=c4880000 size&lt;/P&gt;&lt;P&gt;=65536&lt;/P&gt;&lt;P&gt;DMA Sound Buffers Allocated:UseIram=1 buf-&amp;gt;addr=83a90000 buf-&amp;gt;area=fdf2d000 size&lt;/P&gt;&lt;P&gt;=65536&lt;/P&gt;&lt;P&gt;asoc: SGTL5000 &amp;lt;-&amp;gt; imx-ssi-1-0 mapping ok&lt;/P&gt;&lt;P&gt;mmc0: new high speed SDHC card at address e624&lt;/P&gt;&lt;P&gt;mmcblk0: mmc0:e624 SU04G 3.69 GiB &lt;/P&gt;&lt;P&gt; mmcblk0: p1&lt;/P&gt;&lt;P&gt;ALSA device list:&lt;/P&gt;&lt;P&gt;&amp;nbsp; #0: imx-3stack (SGTL5000)&lt;/P&gt;&lt;P&gt;oprofile: using timer interrupt.&lt;/P&gt;&lt;P&gt;TCP cubic registered&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 17&lt;/P&gt;&lt;P&gt;can: controller area network core (rev 20090105 abi 8)&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 29&lt;/P&gt;&lt;P&gt;can: raw protocol (rev 20090105)&lt;/P&gt;&lt;P&gt;RPC: Registered udp transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered tcp transport module.&lt;/P&gt;&lt;P&gt;smsc911x: Driver version 2008-10-21.&lt;/P&gt;&lt;P&gt;smsc911x-mdio: probed&lt;/P&gt;&lt;P&gt;eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1)&lt;/P&gt;&lt;P&gt;net eth0: MAC Address: 00:04:9f:01:d6:c3&lt;/P&gt;&lt;P&gt;Static Power Management for Freescale i.MX25&lt;/P&gt;&lt;P&gt;regulator_init_complete: incomplete constraints, leaving REG5_PERS on&lt;/P&gt;&lt;P&gt;regulator_init_complete: incomplete constraints, leaving REG1_BKLT on&lt;/P&gt;&lt;P&gt;input: imx_adc_ts as /class/input/input1&lt;/P&gt;&lt;P&gt;i.MX ADC input touchscreen loaded.&lt;/P&gt;&lt;P&gt;imxdi_rtc imxdi_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)&lt;/P&gt;&lt;P&gt;EXT2-fs warning: mounting unchecked fs, running e2fsck is recommended&lt;/P&gt;&lt;P&gt;VFS: Mounted root (ext2 filesystem) on device 179:1.&lt;/P&gt;&lt;P&gt;Freeing init memory: 420K&lt;/P&gt;&lt;P&gt;Failed to execute /etc/inittab.&amp;nbsp; Attempting defaults...&lt;/P&gt;&lt;P&gt;Kernel panic - not syncing: No init found.&amp;nbsp; Try passing init= option to kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Arumugam R&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Feb 2013 11:20:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-error/m-p/259946#M25756</guid>
      <dc:creator>arumugamramasam</dc:creator>
      <dc:date>2013-02-16T11:20:49Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel Panic error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-error/m-p/259947#M25757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It's preferred to use ext3 instead of ext2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Try the command line below as per mx25 Linux BSP User guide document:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;noinitrd console=ttymxc0 root=/dev/mmcblk0p1 rootfstype=ext3 rw ip=dhcp&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Feb 2013 16:16:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-error/m-p/259947#M25757</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2013-02-16T16:16:29Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel Panic error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-error/m-p/259948#M25758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have exactly the same problem, very frustrating. I need to establish a working toolchain, or abandon this and find something that works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I installed the Linux VM on a Windows system.&amp;nbsp; BTE: The system REALLY should ship with an errata sheet -- just getting thru the apt updates was annoying. But set that aside.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ran the config, set in a few options, did a build, and made an SD card.&amp;nbsp; Kernel panic.&lt;/P&gt;&lt;P&gt;Examine the config about 12 times, same thing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Okay, maybe I did something horribly wrong.&amp;nbsp; Build a pristine VM, run configure and accept the defaults.&amp;nbsp; Build a new image, copy to SD card.&lt;/P&gt;&lt;P&gt;Same crap.&amp;nbsp; Boot file is attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas where to go from here ? Or should I give up ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Mar 2013 18:50:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-error/m-p/259948#M25758</guid>
      <dc:creator>carlosorriento</dc:creator>
      <dc:date>2013-03-02T18:50:56Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel Panic error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-error/m-p/259949#M25759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I looked at your log, and it does seem to be a different issue as the one reported in this thread.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your log does not show your complete kernel command line, but you are passing "gpmi" and trying to boot from SD card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is not correct as per the mx28evk Linux BSP User Guide document. You should pass "ssp1" instead.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Other than that, you are using a 2.6.31 kernel on mx28evk and I would strongly recommend to upgrade this kernel and the options are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- 2.6.35 kernel from FSL + LTIB root file system &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- 3.8 kernel from kernel.org + Yocto root file system&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both options work well. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way, Yocto generates an image that you can simply do a 'dd' into your SD card and you have a bootable system.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Mar 2013 21:29:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-error/m-p/259949#M25759</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2013-03-02T21:29:29Z</dc:date>
    </item>
  </channel>
</rss>