<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Linux Boot to Monitor not to Console</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Boot-to-Monitor-not-to-Console/m-p/259268#M25550</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SOLVED: Found that the code in rc_mxc.S was going into a sleep mode if no console was attached. Changed the else statement to use my video source instead and everything worked fine!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Feb 2013 16:48:25 GMT</pubDate>
    <dc:creator>PaulDeMetrotion</dc:creator>
    <dc:date>2013-02-20T16:48:25Z</dc:date>
    <item>
      <title>Linux Boot to Monitor not to Console</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Boot-to-Monitor-not-to-Console/m-p/259265#M25547</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Need help getting local video to work on a Linux kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have built a Linux 3.0.35 kernel for a custom SBC in development. The kernel boots fine on the console display. I am able to log on as the root and perform basic Linux commands. This is great, but I want to have the Linux display on one of the local monitors and use a local keyboard to control the kernel. How do I redirect the Linux display to a supported monitor? I assume I should be able to see video on the console and the selected monitor simultaneously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to remove the 'console=' command line argument in u-boot and this almost worked. This did redirect the video to my desired monitor but the boot stops and the file system does not mount.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the bottom of the monitor output. I have noted where the boot process stops when I disable the console.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;kjournald starting.&amp;nbsp; Commit interval 5 seconds&lt;BR /&gt;EXT3-fs (mmcblk0p1): using internal journal&lt;BR /&gt;EXT3-fs (mmcblk0p1): recovery complete&lt;BR /&gt;EXT3-fs (mmcblk0p1): mounted filesystem with writeback data mode&lt;BR /&gt;VFS: Mounted root (ext3 filesystem) on device 179:1.&lt;BR /&gt;Freeing init memory: 192K&lt;BR /&gt;starting pid 1279, tty '': '/etc/rc.d/rcS'&lt;BR /&gt;Mounting /proc and /sys&lt;BR /&gt;Starting the hotplug events dispatcher udevd&lt;BR /&gt;udevd (1288): /proc/1288/oom_adj is deprecated, please use /proc/1288/oom_score_adj instead.&lt;BR /&gt;Synthesizing initial hotplug events&lt;BR /&gt;Setting the hostname to freescale&lt;BR /&gt;Mounting filesystems&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;cp: write error: No space left on device&lt;BR /&gt;mount: mounting usbfs on /proc/bus/usb failed: No such file or directory&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DISPLAY STOPS HERE WHEN CONSOLE DISABLED – Following only displayed when console enabled&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;starting pid 2439, tty '': '/etc/rc.d/rc_gpu.S'&lt;BR /&gt;starting pid 2445, tty '': '/etc/rc.d/rc_mxc.S'&lt;/P&gt;&lt;P&gt;arm-none-linux-gnueabi-gcc (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) 4.6.2 20110630 (prerelease)&lt;BR /&gt;root filesystem built on Mon, 17 Dec 2012 11:24:04 -0800&lt;BR /&gt;Freescale Semiconductor, Inc.&lt;/P&gt;&lt;P&gt;freescale login:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2013 21:00:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-Boot-to-Monitor-not-to-Console/m-p/259265#M25547</guid>
      <dc:creator>PaulDeMetrotion</dc:creator>
      <dc:date>2013-02-14T21:00:22Z</dc:date>
    </item>
    <item>
      <title>Re: Linux Boot to Monitor not to Console</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Boot-to-Monitor-not-to-Console/m-p/259266#M25548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nobody has any ideas???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Feb 2013 17:34:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-Boot-to-Monitor-not-to-Console/m-p/259266#M25548</guid>
      <dc:creator>PaulDeMetrotion</dc:creator>
      <dc:date>2013-02-18T17:34:38Z</dc:date>
    </item>
    <item>
      <title>Re: Linux Boot to Monitor not to Console</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Boot-to-Monitor-not-to-Console/m-p/259267#M25549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not sure if this is what you want, but you can leave the console as it is and connect to the board through a SSH connection. On the SSH session, run any command you want and on the serial console, monitor your kernel messages.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Feb 2013 17:49:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-Boot-to-Monitor-not-to-Console/m-p/259267#M25549</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2013-02-18T17:49:48Z</dc:date>
    </item>
    <item>
      <title>Re: Linux Boot to Monitor not to Console</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-Boot-to-Monitor-not-to-Console/m-p/259268#M25550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SOLVED: Found that the code in rc_mxc.S was going into a sleep mode if no console was attached. Changed the else statement to use my video source instead and everything worked fine!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2013 16:48:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-Boot-to-Monitor-not-to-Console/m-p/259268#M25550</guid>
      <dc:creator>PaulDeMetrotion</dc:creator>
      <dc:date>2013-02-20T16:48:25Z</dc:date>
    </item>
  </channel>
</rss>