<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Question, i.MX6S ESAI SSI</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-ESAI-SSI/m-p/259138#M25520</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For (1);&lt;/P&gt;&lt;P&gt;In my customer’s understanding, High Frequency Clock Divider which should be set by ESAI_RCCR and ESAI_TCCR registers cannot be configured per each section independently.&lt;/P&gt;&lt;P&gt;From the above, the bit-clocks of the each section shall be the same.&lt;/P&gt;&lt;P&gt;Correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Feb 2014 08:19:35 GMT</pubDate>
    <dc:creator>Aemj</dc:creator>
    <dc:date>2014-02-05T08:19:35Z</dc:date>
    <item>
      <title>Question, i.MX6S ESAI SSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-ESAI-SSI/m-p/259136#M25518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about ESAI and SSI features.&lt;/P&gt;&lt;P&gt;(1)&lt;/P&gt;&lt;P&gt;Is it possible for ESAI to handle different format audio data, such like I2S, 8slot TDM and so on, simultaneously?&lt;/P&gt;&lt;P&gt;In my customer’s understanding, it is not possible for i.MX6 ESAI to handle different formats simultaneously because High Frequency Clock Divider cannot specify bitclocks per each port.&lt;/P&gt;&lt;P&gt;Is the customer’s understanding correct?&lt;/P&gt;&lt;P&gt;Do you have any solutions to handle different audio format data that has different bit clocks simultaneously?&lt;/P&gt;&lt;P&gt;(2)&lt;/P&gt;&lt;P&gt;For SSI,&lt;/P&gt;&lt;P&gt;The customer believes that the each of SSIs(SSI1, SSI2 and SSI3) can be configured with different slot and clock divider independently.&lt;/P&gt;&lt;P&gt;Then he believes SSIs can be used with different audio format per ports simultaneously, such as;&lt;/P&gt;&lt;P&gt; SSI1 = I2S, SS2 = 8slot TDM&lt;/P&gt;&lt;P&gt;Is it true?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jan 2014 07:04:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-ESAI-SSI/m-p/259136#M25518</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2014-01-27T07:04:34Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6S ESAI SSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-ESAI-SSI/m-p/259137#M25519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;1.&lt;BR /&gt;&amp;nbsp; The ESAI provides a full-duplex serial port. Generally it is a single port ; in this sense it is not similar&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;to the AUDMUX, which supports multiports, working simultaneously.&amp;nbsp; In the same time, the ESAI consists &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;of independent transmitter and receiver sections, each section with its own clock generator; this &lt;BR /&gt;means the transmitter and receiver may work as two separate channels. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;2.You are right - the SSI(s) may be configured fully independently.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Feb 2014 07:37:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-ESAI-SSI/m-p/259137#M25519</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-02-05T07:37:32Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6S ESAI SSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-ESAI-SSI/m-p/259138#M25520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For (1);&lt;/P&gt;&lt;P&gt;In my customer’s understanding, High Frequency Clock Divider which should be set by ESAI_RCCR and ESAI_TCCR registers cannot be configured per each section independently.&lt;/P&gt;&lt;P&gt;From the above, the bit-clocks of the each section shall be the same.&lt;/P&gt;&lt;P&gt;Correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Feb 2014 08:19:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-ESAI-SSI/m-p/259138#M25520</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2014-02-05T08:19:35Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6S ESAI SSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-ESAI-SSI/m-p/259139#M25521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I mean that the customer wants to set independent bit-clock per TX0-5 or per RX0-3.&lt;/P&gt;&lt;P&gt;Does it make sense?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Feb 2014 04:48:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-ESAI-SSI/m-p/259139#M25521</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2014-02-06T04:48:24Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6S ESAI SSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-ESAI-SSI/m-p/259140#M25522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, "In the synchronous mode (SYN=1), the bit clock defined for the transmitter &lt;/P&gt;&lt;P&gt;determines the receiver bit clock as well." &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Feb 2014 07:38:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-ESAI-SSI/m-p/259140#M25522</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-02-06T07:38:10Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6S ESAI SSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-ESAI-SSI/m-p/259141#M25523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"When SYN is cleared, the ESAI transmitter and receiver clocks and frame sync sources&lt;/P&gt;&lt;P&gt;are independent. If SYN is set, the ESAI transmitter and receiver clocks and frame sync&lt;/P&gt;&lt;P&gt;come from the transmitter section (either external or internal sources).&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;" So, basically&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;it is possible to have different frequencies.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Feb 2014 07:40:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6S-ESAI-SSI/m-p/259141#M25523</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-02-06T07:40:39Z</dc:date>
    </item>
  </channel>
</rss>