<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.mx6s Custom Board booting problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6s-Custom-Board-booting-problem/m-p/258990#M25454</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, were you able to change the DDR clock speed inside u-boot? If so can you shared how you did it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks a lot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Jun 2013 18:28:11 GMT</pubDate>
    <dc:creator>patricesarrasin</dc:creator>
    <dc:date>2013-06-21T18:28:11Z</dc:date>
    <item>
      <title>i.mx6s Custom Board booting problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6s-Custom-Board-booting-problem/m-p/258986#M25450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've made a custom board with i.mx6 solo and i'm encountering some problems to make it boot!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Powrers and clocks are ok, BOOT_CFG are 0/0 and USB SERIAL DOWNLOADER is correctly prompted when attached to pc!&lt;/P&gt;&lt;P&gt;Uploading trough USB is fine (just doing boot and jump) but nothing happens after "jump" on the console neither on several clock pins (that remains high pulled).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After had same situation with several u-boot images (precompiled from freescale and my own), I think that there is some problem on DDR3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I made a little u-boot image and I'm trying to load it to OCRAM (&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;TEXT_BASE = 0x009077e0&lt;/SPAN&gt;), but &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;nothng is happening the same, so the problem must be elsewhere!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you help me to find a way to make it boot?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Really thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 May 2013 15:00:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6s-Custom-Board-booting-problem/m-p/258986#M25450</guid>
      <dc:creator>politoleo</dc:creator>
      <dc:date>2013-05-27T15:00:55Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6s Custom Board booting problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6s-Custom-Board-booting-problem/m-p/258987#M25451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try memory test linked below, at least to check if codes can be loaded to i.MX6 system and run there.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/servlet/JiveServlet/download/322206-258321/DDR_Stress_Tester_V0.042.zip" title="https://community.freescale.com/servlet/JiveServlet/download/322206-258321/DDR_Stress_Tester_V0.042.zip"&gt;https://community.freescale.com/servlet/JiveServlet/download/322206-258321/DDR_Stress_Tester_V0.042.zip&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-objectid="305794" data-objecttype="1" href="https://community.nxp.com/thread/305794"&gt;https://community.freescale.com/thread/305794&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2013 02:02:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6s-Custom-Board-booting-problem/m-p/258987#M25451</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-05-28T02:02:23Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6s Custom Board booting problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6s-Custom-Board-booting-problem/m-p/258988#M25452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was able to start the board by scaling the DDR clock to 400Mhz, but booting from internal ram.&lt;/P&gt;&lt;P&gt;Booting from DDR3 was not successfull!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now it's time to start the DDR stress tester, to find out the correct register to set to make it works!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfrotunatly it hangs here:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MX6DL opened.&lt;/P&gt;&lt;P&gt;HAB_TYPE: DEVELOP&lt;/P&gt;&lt;P&gt;Image loading...&lt;/P&gt;&lt;P&gt;download Image to IRAM OK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Re-open MX6x device.&lt;/P&gt;&lt;P&gt;Running DDR test..., press "ESC" key to exit.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any tips to make it start?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Jun 2013 17:33:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6s-Custom-Board-booting-problem/m-p/258988#M25452</guid>
      <dc:creator>politoleo</dc:creator>
      <dc:date>2013-06-04T17:33:33Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6s Custom Board booting problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6s-Custom-Board-booting-problem/m-p/258989#M25453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Now the DDR test is running but it ends/hangs here:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Beginning stress test&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;loop: 1&lt;/P&gt;&lt;P&gt;DDR Freq: 327 MHz&lt;/P&gt;&lt;P&gt;t0.1: data is addr test&lt;/P&gt;&lt;P&gt;Address of failure: 0x10000000&lt;/P&gt;&lt;P&gt;Data was: 0xff000000&lt;/P&gt;&lt;P&gt;But pattern&amp;nbsp; should match address&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any tips?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Jun 2013 18:07:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6s-Custom-Board-booting-problem/m-p/258989#M25453</guid>
      <dc:creator>politoleo</dc:creator>
      <dc:date>2013-06-04T18:07:58Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6s Custom Board booting problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6s-Custom-Board-booting-problem/m-p/258990#M25454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, were you able to change the DDR clock speed inside u-boot? If so can you shared how you did it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks a lot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 18:28:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6s-Custom-Board-booting-problem/m-p/258990#M25454</guid>
      <dc:creator>patricesarrasin</dc:creator>
      <dc:date>2013-06-21T18:28:11Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6s Custom Board booting problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6s-Custom-Board-booting-problem/m-p/258991#M25455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please check memory design, using recommendations of the Design Checklist in the &lt;/P&gt;&lt;P&gt;Hardware Development Guide for i.MX6.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Aug 2013 02:30:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6s-Custom-Board-booting-problem/m-p/258991#M25455</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-08-14T02:30:59Z</dc:date>
    </item>
  </channel>
</rss>