<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Problem on bare metal application using SABRE AI and DS-5</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problem-on-bare-metal-application-using-SABRE-AI-and-DS-5/m-p/258869#M25402</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yuri,&lt;/P&gt;&lt;P&gt;thanks for that fast reply!&lt;/P&gt;&lt;P&gt;I already tried to use those scripts, and it looks like i get connected to the target. But when trying to load the application i get the following messages in the debug window:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stopping running target Freescale - i.MX6 Quad (Generic) on USB:001567 on connection&lt;/P&gt;&lt;P&gt;Connected to running target Freescale - i.MX6 Quad (Generic) on USB:001567&lt;/P&gt;&lt;P&gt;Execution stopped at: S:0x00000FC4&lt;/P&gt;&lt;P&gt;S:0x00000FC4&amp;nbsp;&amp;nbsp; BX&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; lr&lt;/P&gt;&lt;P&gt;loadfile "C:\XXX\Debug\testARM.axf"&lt;/P&gt;&lt;P&gt;ERROR(CMD16-TAD274-NAL18):&lt;/P&gt;&lt;P&gt;! Failed to load "testARM.axf"&lt;/P&gt;&lt;P&gt;! Failed to write 5.068 bytes to address S:0x00008000 while writing block of 4.096 bytes to address S:0x00008000&lt;/P&gt;&lt;P&gt;! Bus error on memory operation.&lt;/P&gt;&lt;P&gt;Target Message: Memory access caused precise abort.&lt;/P&gt;&lt;P&gt;Debug Precise Abort Registers : DFSR = 0x00001808, DFAR = 0x00008000&lt;/P&gt;&lt;P&gt;cd "C:\XXX\WorkspaceARM"&lt;/P&gt;&lt;P&gt;Working directory "C:\XXX\WorkspaceARM"&lt;/P&gt;&lt;P&gt;set debug-from main&lt;/P&gt;&lt;P&gt;start&lt;/P&gt;&lt;P&gt;WARNING(CMD399-COR168): &lt;/P&gt;&lt;P&gt;! Failed to start the target&lt;/P&gt;&lt;P&gt;! No function named "main" could be found&lt;/P&gt;&lt;P&gt;WARNING(CMD407): Trying the entry point instead&lt;/P&gt;&lt;P&gt;ERROR(CMD426): Cannot find symbol to start or entrypoint, the file or load commands may be used to set the entrypoint&lt;/P&gt;&lt;P&gt;wait&lt;/P&gt;&lt;P&gt;source /v "C:\opt\imx6_platform_sdk\tools\ds5\MX6Q_SabreSD_DDR3_v1.6.ds"&lt;/P&gt;&lt;P&gt;+stop&lt;/P&gt;&lt;P&gt;WARNING(CMD315): Target is not running&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And here i am not sure how to fix that issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Jul 2013 09:22:03 GMT</pubDate>
    <dc:creator>falcobapp</dc:creator>
    <dc:date>2013-07-08T09:22:03Z</dc:date>
    <item>
      <title>Problem on bare metal application using SABRE AI and DS-5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-on-bare-metal-application-using-SABRE-AI-and-DS-5/m-p/258867#M25400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i just started on working with an i.MX6 Sabre AI platform and want to work bare metal.&lt;/P&gt;&lt;P&gt;Is there anybody who knows the configuration and scripts needed to execute to get DS-5 connected to the board to load the application?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Falco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jul 2013 08:06:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-on-bare-metal-application-using-SABRE-AI-and-DS-5/m-p/258867#M25400</guid>
      <dc:creator>falcobapp</dc:creator>
      <dc:date>2013-07-08T08:06:42Z</dc:date>
    </item>
    <item>
      <title>Re: Problem on bare metal application using SABRE AI and DS-5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-on-bare-metal-application-using-SABRE-AI-and-DS-5/m-p/258868#M25401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please use scripts from the Platform SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&amp;amp;location=null&amp;amp;fpsp=1&amp;amp;WT_TYPE=Lab%20and%20Test%20Software&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=tgz&amp;amp;WT_ASSET=Downloads&amp;amp;sr=100&amp;amp;Parent_nodeId=1337637154535695831062&amp;amp;Parent_pageType=product" title="https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&amp;amp;location=null&amp;amp;fpsp=1&amp;amp;WT_TYPE=Lab%20and%20Test%20Software&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=tgz&amp;amp;WT_ASSET=Downloads&amp;amp;sr=100&amp;amp;Parent_nodeId=1337637154535695831062&amp;amp;Parent_pageType=product"&gt;https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&amp;amp;location=null&amp;amp;fpsp=1&amp;amp;WT_TYPE=Lab%20and%20Test%20Software&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=tgz&amp;amp;WT_ASSET=Downloads&amp;amp;sr=100&amp;amp;Parent_nodeId=1337637154535695831062&amp;amp;Parent_pageType=product&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jul 2013 09:10:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-on-bare-metal-application-using-SABRE-AI-and-DS-5/m-p/258868#M25401</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-07-08T09:10:33Z</dc:date>
    </item>
    <item>
      <title>Re: Problem on bare metal application using SABRE AI and DS-5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-on-bare-metal-application-using-SABRE-AI-and-DS-5/m-p/258869#M25402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yuri,&lt;/P&gt;&lt;P&gt;thanks for that fast reply!&lt;/P&gt;&lt;P&gt;I already tried to use those scripts, and it looks like i get connected to the target. But when trying to load the application i get the following messages in the debug window:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stopping running target Freescale - i.MX6 Quad (Generic) on USB:001567 on connection&lt;/P&gt;&lt;P&gt;Connected to running target Freescale - i.MX6 Quad (Generic) on USB:001567&lt;/P&gt;&lt;P&gt;Execution stopped at: S:0x00000FC4&lt;/P&gt;&lt;P&gt;S:0x00000FC4&amp;nbsp;&amp;nbsp; BX&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; lr&lt;/P&gt;&lt;P&gt;loadfile "C:\XXX\Debug\testARM.axf"&lt;/P&gt;&lt;P&gt;ERROR(CMD16-TAD274-NAL18):&lt;/P&gt;&lt;P&gt;! Failed to load "testARM.axf"&lt;/P&gt;&lt;P&gt;! Failed to write 5.068 bytes to address S:0x00008000 while writing block of 4.096 bytes to address S:0x00008000&lt;/P&gt;&lt;P&gt;! Bus error on memory operation.&lt;/P&gt;&lt;P&gt;Target Message: Memory access caused precise abort.&lt;/P&gt;&lt;P&gt;Debug Precise Abort Registers : DFSR = 0x00001808, DFAR = 0x00008000&lt;/P&gt;&lt;P&gt;cd "C:\XXX\WorkspaceARM"&lt;/P&gt;&lt;P&gt;Working directory "C:\XXX\WorkspaceARM"&lt;/P&gt;&lt;P&gt;set debug-from main&lt;/P&gt;&lt;P&gt;start&lt;/P&gt;&lt;P&gt;WARNING(CMD399-COR168): &lt;/P&gt;&lt;P&gt;! Failed to start the target&lt;/P&gt;&lt;P&gt;! No function named "main" could be found&lt;/P&gt;&lt;P&gt;WARNING(CMD407): Trying the entry point instead&lt;/P&gt;&lt;P&gt;ERROR(CMD426): Cannot find symbol to start or entrypoint, the file or load commands may be used to set the entrypoint&lt;/P&gt;&lt;P&gt;wait&lt;/P&gt;&lt;P&gt;source /v "C:\opt\imx6_platform_sdk\tools\ds5\MX6Q_SabreSD_DDR3_v1.6.ds"&lt;/P&gt;&lt;P&gt;+stop&lt;/P&gt;&lt;P&gt;WARNING(CMD315): Target is not running&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And here i am not sure how to fix that issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jul 2013 09:22:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-on-bare-metal-application-using-SABRE-AI-and-DS-5/m-p/258869#M25402</guid>
      <dc:creator>falcobapp</dc:creator>
      <dc:date>2013-07-08T09:22:03Z</dc:date>
    </item>
    <item>
      <title>Re: Problem on bare metal application using SABRE AI and DS-5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-on-bare-metal-application-using-SABRE-AI-and-DS-5/m-p/258870#M25403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Your load address (0x8000) seems me suspicious :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt; font-family: 'Arial','sans-serif'; color: #333333;"&gt;"Failed to write 5.068 bytes to address S:0x00008000" &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt; font-family: 'Arial','sans-serif'; color: #333333;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;i.MX6 has following address ranges for applications (Table 2-1. System memory map of the Reference &lt;BR /&gt;Manual) :&lt;/P&gt;&lt;P&gt;0090_0000 - 0093_FFFF&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; internal RAM (OCRAM), useful for small applications, since there is no need for DRAM init.&lt;/P&gt;&lt;P&gt;1000_0000 - FFFF_FFFF&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DRAM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, please try to rebuild the application using correct link file, or just correct application memory map. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jul 2013 09:48:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-on-bare-metal-application-using-SABRE-AI-and-DS-5/m-p/258870#M25403</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-07-08T09:48:41Z</dc:date>
    </item>
    <item>
      <title>Re: Problem on bare metal application using SABRE AI and DS-5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-on-bare-metal-application-using-SABRE-AI-and-DS-5/m-p/258871#M25404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Got the problem solved. The change of the setting in DS-5 eclipse worked when setting up the adress spaces corectly and update the apropriate linker skript and use of debugger-script.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot Yuri!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jul 2013 14:37:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-on-bare-metal-application-using-SABRE-AI-and-DS-5/m-p/258871#M25404</guid>
      <dc:creator>falcobapp</dc:creator>
      <dc:date>2013-07-08T14:37:39Z</dc:date>
    </item>
  </channel>
</rss>