<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックpthreads</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/pthreads/m-p/146693#M254</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello everyone,&lt;/P&gt;&lt;P&gt;when i'm using eclipse to build an application that is using threads, i have to attach the library pthread in order that the&lt;/P&gt;&lt;P&gt;#include &amp;lt;pthread.h&amp;gt; will resolved.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;is it possible to run a program that uses threads on the min bootable FS LTIB generates? i've created this filesystem and added some pacakges for my project.&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;is there anything i need to change on the build process while cross compiling except from the regular settings for builder linker and assembler and the linker add library path?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;snir.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Mar 2012 22:16:07 GMT</pubDate>
    <dc:creator>snirnisim</dc:creator>
    <dc:date>2012-03-19T22:16:07Z</dc:date>
    <item>
      <title>pthreads</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/pthreads/m-p/146693#M254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello everyone,&lt;/P&gt;&lt;P&gt;when i'm using eclipse to build an application that is using threads, i have to attach the library pthread in order that the&lt;/P&gt;&lt;P&gt;#include &amp;lt;pthread.h&amp;gt; will resolved.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;is it possible to run a program that uses threads on the min bootable FS LTIB generates? i've created this filesystem and added some pacakges for my project.&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;is there anything i need to change on the build process while cross compiling except from the regular settings for builder linker and assembler and the linker add library path?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;snir.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Mar 2012 22:16:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/pthreads/m-p/146693#M254</guid>
      <dc:creator>snirnisim</dc:creator>
      <dc:date>2012-03-19T22:16:07Z</dc:date>
    </item>
    <item>
      <title>Re: pthreads</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/pthreads/m-p/146694#M255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nope, you don't need anything extra to add to use pthread aside from the include and the lib. Try changing the “hello world” &amp;nbsp;to thread example and it should compile just fine. I have used the lib without any issues on minimal ltib build.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Mar 2012 03:37:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/pthreads/m-p/146694#M255</guid>
      <dc:creator>IvicaEftimovski</dc:creator>
      <dc:date>2012-03-20T03:37:13Z</dc:date>
    </item>
  </channel>
</rss>