<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PCIe resource collisions in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-resource-collisions/m-p/258733#M25342</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have fitted a PCIe video capture card to the SabreSD board and built and installed the driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I type lsmod I can see the driver is present, but there are no /dev/videox nodes present.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I type dmesg I can see the following information about the driver:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Linux video capture interface: v2.00&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;avc8000 driver version 1.0.2 loaded&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;avc8000 driver dma_mode=1, debug=0&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;PCI: Device 0000:01:00.0 not available because of resource collisions&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;avc8k: probe of 0000:01:00.0 failed with error -5&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;I have already applied the patch from &lt;A href="https://github.com/boundarydevices/linux-imx6/blob/d4d655aa6420d5ae9c4354b86cc750b53e703e1e/arch/arm/mach-mx6/pcie.c"&gt;https://github.com/boundarydevices/linux-imx6/blob/d4d655aa6420d5ae9c4354b86cc750b53e703e1e/arch/arm/mach-mx6/pcie.c&lt;/A&gt; to the kernel, but it hasn't fixed the problem. Does anyone have any suggestion for how to fix this please?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Andrew&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Apr 2013 17:21:28 GMT</pubDate>
    <dc:creator>andrewellis</dc:creator>
    <dc:date>2013-04-09T17:21:28Z</dc:date>
    <item>
      <title>PCIe resource collisions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-resource-collisions/m-p/258733#M25342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have fitted a PCIe video capture card to the SabreSD board and built and installed the driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I type lsmod I can see the driver is present, but there are no /dev/videox nodes present.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I type dmesg I can see the following information about the driver:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Linux video capture interface: v2.00&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;avc8000 driver version 1.0.2 loaded&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;avc8000 driver dma_mode=1, debug=0&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;PCI: Device 0000:01:00.0 not available because of resource collisions&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;avc8k: probe of 0000:01:00.0 failed with error -5&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;I have already applied the patch from &lt;A href="https://github.com/boundarydevices/linux-imx6/blob/d4d655aa6420d5ae9c4354b86cc750b53e703e1e/arch/arm/mach-mx6/pcie.c"&gt;https://github.com/boundarydevices/linux-imx6/blob/d4d655aa6420d5ae9c4354b86cc750b53e703e1e/arch/arm/mach-mx6/pcie.c&lt;/A&gt; to the kernel, but it hasn't fixed the problem. Does anyone have any suggestion for how to fix this please?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Andrew&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2013 17:21:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-resource-collisions/m-p/258733#M25342</guid>
      <dc:creator>andrewellis</dc:creator>
      <dc:date>2013-04-09T17:21:28Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe resource collisions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-resource-collisions/m-p/258734#M25343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrew&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think I have a solution to the above problem. Try the attached patch&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Troy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2013 03:19:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-resource-collisions/m-p/258734#M25343</guid>
      <dc:creator>troy_kisky</dc:creator>
      <dc:date>2013-04-11T03:19:14Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe resource collisions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-resource-collisions/m-p/258735#M25344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Troy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the patch, it solved my problem :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2013 21:40:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-resource-collisions/m-p/258735#M25344</guid>
      <dc:creator>andrewellis</dc:creator>
      <dc:date>2013-04-11T21:40:14Z</dc:date>
    </item>
  </channel>
</rss>