<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MfgTool MX6Q Linux Update SabreSD-eMMC fails</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-MX6Q-Linux-Update-SabreSD-eMMC-fails/m-p/257891#M25003</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marcel, I just tested flashing the eMMC with linux in the SabreQuad without problems.&lt;/P&gt;&lt;P&gt;Can you please download the MfgTool again (latest version)?, you don't need to do any changes into the XML file, just set the init file to SabreSD-eMMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Make sure you do not have an SD Card attached to the board before starting, and that you have all dip switches to "0".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me know how it goes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Feb 2014 19:19:33 GMT</pubDate>
    <dc:creator>SergioSolis</dc:creator>
    <dc:date>2014-02-25T19:19:33Z</dc:date>
    <item>
      <title>MfgTool MX6Q Linux Update SabreSD-eMMC fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-MX6Q-Linux-Update-SabreSD-eMMC-fails/m-p/257890#M25002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to flash linux from &lt;EM&gt;Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER/Profiles/MX6Q Linux Update/OS Firmware&lt;/EM&gt; to the eMMC of my sabre sd quad board via MfgTool without success using the following configuration:&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;[profiles]&lt;/P&gt;
&lt;P&gt;chip = MX6Q Linux Update&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;[platform]&lt;/P&gt;
&lt;P&gt;board = SabreSD&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;[LIST]&lt;/P&gt;
&lt;P&gt;name = SabreSD-eMMC&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MfgTool.log ends up with:&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;ModuleID[2] LevelID[1]: CmdOpreation[0]--set m_hDeviceArriveEvent.&lt;/P&gt;
&lt;P&gt;ModuleID[2] LevelID[10]: CmdOpreation[0]--WaitforEvents device arrive1&lt;/P&gt;
&lt;P&gt;ModuleID[2] LevelID[10]: CmdOperation[0] device chagned and reset to state 1&lt;/P&gt;
&lt;P&gt;ModuleID[2] LevelID[10]: ExecuteCommand--Push[WndIndex:0], Body is $ ls /dev/*&lt;/P&gt;
&lt;P&gt;ModuleID[2] LevelID[1]: PortMgrDlg(0)--MSCDevice--Command Push(no file) excute failed&lt;/P&gt;
&lt;P&gt;ModuleID[2] LevelID[10]: CmdOperation[0], current command executed failed, so SetEvent(hDevCanDeleteEvent)&lt;/P&gt;
&lt;P&gt;ModuleID[2] LevelID[10]: CCmdOpreation[0] thread is Closed&lt;/P&gt;
&lt;P&gt;ModuleID[2] LevelID[10]: CCmdOpreation[0] thread is Closed&lt;/P&gt;
&lt;P&gt;ModuleID[2] LevelID[10]: DeviceManager::OnMsgDeviceEvent() - EVENT_KILL&lt;/P&gt;
&lt;P&gt;ModuleID[2] LevelID[10]: CMyExceptionHandler::OnMsgExceptionEvent() - KillExceptionHandlerThread&lt;/P&gt;
&lt;P&gt;ModuleID[2] LevelID[10]: Exception Handler thread is closed&lt;/P&gt;
&lt;P&gt;ModuleID[2] LevelID[1]: delete MxHidDeviceClass&lt;/P&gt;
&lt;P&gt;ModuleID[2] LevelID[10]: Device Manager thread is closed&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;&lt;P&gt;The serial log shows the following:&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;Starting UTP&lt;BR /&gt;ln: /etc/mtab: File exists&lt;BR /&gt;disable turn off display&lt;BR /&gt;Starting the hotplug events dispatcher udevd&lt;BR /&gt;udevd (2000): /proc/2000/oom_adj is deprecated, please use /proc/2000/oom_score_adj instead.&lt;BR /&gt;Synthesizing initial hotplug evenmmc0: new high speed DDR MMC card at address 0001&lt;BR /&gt;ts&lt;BR /&gt;mmcblk0: mmc0:0001 SEM08G 7.39 GiB &lt;BR /&gt;mmcblk0boot0: mmc0:0001 SEM08G partition 1 2.00 MiB&lt;BR /&gt;mmcblk0boot1: mmc0:0001 SEM08G partition 2 2.00 MiB&lt;BR /&gt; mmcblk0: p1&lt;BR /&gt; mmcblk0boot1: unknown partition table&lt;BR /&gt; mmcblk0boot0: unknown partition table&lt;BR /&gt;g_file_storage gadget: high speed config #1&lt;BR /&gt;uuc 0.4 [built Aug 16 2013 01:24:08]&lt;BR /&gt;UTP: Waiting for device to appear&lt;BR /&gt;UTP: file/device node /dev/utp already exists&lt;BR /&gt;cpu_id is 0&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;&lt;P&gt;For me it seems like the MfgTool fails running the following ls /dev/* command from ucl2.xml:&lt;/P&gt;&lt;PRE __default_attr="xml" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_1393327493290808" jivemacro_uid="_1393327493290808"&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;CMD state="BootStrap" type="jump" &amp;gt; Jumping to OS image. &amp;lt;/CMD&amp;gt; 
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;CMD state="Updater" type="push" body="$ ls /dev/*"/&amp;gt;&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My assumption is that there are no device nodes in /dev, otherwise I could not understand why the script fails at a simple ls.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anybody see what the error could be or had a similar problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Feb 2014 11:35:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MfgTool-MX6Q-Linux-Update-SabreSD-eMMC-fails/m-p/257890#M25002</guid>
      <dc:creator>marcelgrosshans</dc:creator>
      <dc:date>2014-02-25T11:35:31Z</dc:date>
    </item>
    <item>
      <title>Re: MfgTool MX6Q Linux Update SabreSD-eMMC fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-MX6Q-Linux-Update-SabreSD-eMMC-fails/m-p/257891#M25003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marcel, I just tested flashing the eMMC with linux in the SabreQuad without problems.&lt;/P&gt;&lt;P&gt;Can you please download the MfgTool again (latest version)?, you don't need to do any changes into the XML file, just set the init file to SabreSD-eMMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Make sure you do not have an SD Card attached to the board before starting, and that you have all dip switches to "0".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me know how it goes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Feb 2014 19:19:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MfgTool-MX6Q-Linux-Update-SabreSD-eMMC-fails/m-p/257891#M25003</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2014-02-25T19:19:33Z</dc:date>
    </item>
    <item>
      <title>Re: MfgTool MX6Q Linux Update SabreSD-eMMC fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-MX6Q-Linux-Update-SabreSD-eMMC-fails/m-p/257892#M25004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Serch,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for your help. Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER.tar.gz is the latest version I found.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the tool was &lt;STRONG&gt;not&lt;/STRONG&gt; the problem. I didn't know that the MfgTool has to be &lt;STRONG&gt;run as administrator&lt;/STRONG&gt;. I'm sorry for this, but I didn't know that the MfgTool needs admin rights for sending commands via UTP. :smileyconfused:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2014 11:28:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MfgTool-MX6Q-Linux-Update-SabreSD-eMMC-fails/m-p/257892#M25004</guid>
      <dc:creator>marcelgrosshans</dc:creator>
      <dc:date>2014-02-27T11:28:59Z</dc:date>
    </item>
    <item>
      <title>Re: MfgTool MX6Q Linux Update SabreSD-eMMC fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-MX6Q-Linux-Update-SabreSD-eMMC-fails/m-p/257893#M25005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I facing same issue to flash eMMC in i.MX6 SebreSD board, i changed cfg.ini file as below:&lt;/P&gt;&lt;P&gt;[profiles]&lt;/P&gt;&lt;P&gt;chip = MX6Q Linux Update&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[platform]&lt;/P&gt;&lt;P&gt;board = SabreSD&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[LIST]&lt;/P&gt;&lt;P&gt;name = SabreSD-eMMC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and set SW6 all zero(00000000) then start flash by using MFGTool (Latest version) after finishing, changed the SW6 11010110 as given in the i.MX6 Rebre SD Linux User Guide, u-boot does not come mean nothing comes on minicom.&lt;/P&gt;&lt;P&gt;Attaching eMMC flash log here, Please suggest me how to solve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sagar &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 May 2014 12:52:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MfgTool-MX6Q-Linux-Update-SabreSD-eMMC-fails/m-p/257893#M25005</guid>
      <dc:creator>vidyasagar</dc:creator>
      <dc:date>2014-05-28T12:52:00Z</dc:date>
    </item>
    <item>
      <title>Re: MfgTool MX6Q Linux Update SabreSD-eMMC fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-MX6Q-Linux-Update-SabreSD-eMMC-fails/m-p/257894#M25006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi vidya,&lt;/P&gt;&lt;P&gt;You want to flash eMMC, the configuration of cfg.ini is correct. When you use the MFGTOOL to download please set the SW6= 00001100(low to high). Then boot up with SW6 11010110. You can have a try.&lt;/P&gt;&lt;P&gt;Hope this can help you~~&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 May 2014 01:56:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MfgTool-MX6Q-Linux-Update-SabreSD-eMMC-fails/m-p/257894#M25006</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2014-05-30T01:56:34Z</dc:date>
    </item>
    <item>
      <title>Re: MfgTool MX6Q Linux Update SabreSD-eMMC fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-MX6Q-Linux-Update-SabreSD-eMMC-fails/m-p/257895#M25007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for reply.&lt;/P&gt;&lt;P&gt;I tried to flash eMMC with SW6= 00001100(Low to High) by use of MFGTOOL, flashed successfully then changed SW6 11010110 but boot log does not initiate.&lt;/P&gt;&lt;P&gt;I attached eMMC flashed log with SW6= 00001100, please help me to solve this issue.&lt;/P&gt;&lt;P&gt;Could i.MX6 SabreSD eMMC flash without MFGTOOL if available please suggest me ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Vidya ! ! &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 May 2014 06:43:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MfgTool-MX6Q-Linux-Update-SabreSD-eMMC-fails/m-p/257895#M25007</guid>
      <dc:creator>vidyasagar</dc:creator>
      <dc:date>2014-05-30T06:43:52Z</dc:date>
    </item>
  </channel>
</rss>