<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx53 i2c1 on (PAD_EIM_D21 and PAD_EIM_D28) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx53-i2c1-on-PAD-EIM-D21-and-PAD-EIM-D28/m-p/257889#M25001</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For your reference, attached is the BSP porting guide. There is talk about porting I2C. Although it is for i.MX6, the porting is similar to i.MX53.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Apr 2013 04:11:38 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2013-04-17T04:11:38Z</dc:date>
    <item>
      <title>imx53 i2c1 on (PAD_EIM_D21 and PAD_EIM_D28)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx53-i2c1-on-PAD-EIM-D21-and-PAD-EIM-D28/m-p/257888#M25000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like on a mx53 QSB the i2c1 on pin :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IMX53_PAD_EIM_D21_I2C1_SCL,&lt;/P&gt;&lt;P&gt;IMX53_PAD_EIM_D28_I2C1_SDA,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've added this two line in mx53_loco_pads[] in arch/arm/mach-mx5/board-mx53_loco.h (in linux 2.6.38 from freescale). And remove this line :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MX53_PAD_EIM_D21__IPU_DISPB0_SER_CLK,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the linux boot /dev/i2c-0 is created but I've no signal on scl or sda pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is missing in my modification?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cordially,&lt;/P&gt;&lt;P&gt;Cyril crocquesel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2013 13:02:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx53-i2c1-on-PAD-EIM-D21-and-PAD-EIM-D28/m-p/257888#M25000</guid>
      <dc:creator>cyrilcrocquesel</dc:creator>
      <dc:date>2013-04-09T13:02:41Z</dc:date>
    </item>
    <item>
      <title>Re: imx53 i2c1 on (PAD_EIM_D21 and PAD_EIM_D28)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx53-i2c1-on-PAD-EIM-D21-and-PAD-EIM-D28/m-p/257889#M25001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For your reference, attached is the BSP porting guide. There is talk about porting I2C. Although it is for i.MX6, the porting is similar to i.MX53.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2013 04:11:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx53-i2c1-on-PAD-EIM-D21-and-PAD-EIM-D28/m-p/257889#M25001</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2013-04-17T04:11:38Z</dc:date>
    </item>
  </channel>
</rss>