<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6 IVT structure -- question in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IVT-structure-question/m-p/257600#M24955</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yongcai,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; About image_len:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word _end_of_copy&amp;nbsp; - TEXT_BASE + CONFIG_FLASH_HEADER_OFFSET&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Why there is the " + CONFIG_FLASH_HEADER_OFFSET".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; In my opinion, _end_of_copy&amp;nbsp; - TEXT_BASE has already been the length of uboot image.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Does " + CONFIG_FLASH_HEADER_OFFSET" mean that ROM loads uboot image from the beginning of emmc instead of from IVT offeset?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Simmis.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Jun 2014 08:15:19 GMT</pubDate>
    <dc:creator>simmisxu</dc:creator>
    <dc:date>2014-06-13T08:15:19Z</dc:date>
    <item>
      <title>i.MX6 IVT structure -- question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IVT-structure-question/m-p/257595#M24950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a generic question regarding i.MX6 IVT structure. I will refer to i.MX6 Platform SDK apps and u-boot binaries. &lt;/P&gt;&lt;P&gt;DCD section is used for setting up DDR memory both in SDK tests and in u-boot. DCD section itself is linked to DDR memory address space. Also if you look inside a binary you can find that ivt.dcd is pointing to DDR memory location:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# ./ivt_dump ./power_modes_test.bin&lt;/P&gt;&lt;P&gt; DCD: 0x10000430 (DDR)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# ./ivt_dump ./u-boot.bin&lt;/P&gt;&lt;P&gt; DCD: 0x2780042C (DDR)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So it looks like we should have DCD placed in DDR, but DDR is not yet initialized by DCD. I know that DCD should reside in initial load region and thus ti will be loaded to OCRAM. But how ROM will find the real DCD location based only on ivt.dcd, which is poiniting to non-initialized DDR?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Nov 2013 09:54:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IVT-structure-question/m-p/257595#M24950</guid>
      <dc:creator>dmitryv</dc:creator>
      <dc:date>2013-11-05T09:54:21Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 IVT structure -- question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IVT-structure-question/m-p/257596#M24951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Dmitry&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; When power up the board, ROM will be executed first, then it will scan the boot mode setting to get which boot mode it should run, take SD/MMC boot for example, if user set the board to boot from SD/MMC, ROM will read first 2K data from SD/MMC to OCRAM, and the IVT header will be contained in this 2K data, then execute the DCD to initialize the DDR, then copy rest of uboot to DDR and jump to DDR to run. That means we always need to put IVT header in front of uboot binary and need to program this ivt+uboot into dedicated place of boot media. You can read the DCD header definition, you will see &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Nov 2013 02:28:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IVT-structure-question/m-p/257596#M24951</guid>
      <dc:creator>AnsonHuang</dc:creator>
      <dc:date>2013-11-06T02:28:29Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 IVT structure -- question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IVT-structure-question/m-p/257597#M24952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Dmitry&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Did you have other question about this IVT? Anything you need me to help? If no, could you please check the correct answer and close this ticket? Thanks in advanced!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Nov 2013 05:55:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IVT-structure-question/m-p/257597#M24952</guid>
      <dc:creator>AnsonHuang</dc:creator>
      <dc:date>2013-11-06T05:55:02Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 IVT structure -- question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IVT-structure-question/m-p/257598#M24953</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yongcai,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand the process of booting but I was asking another question. Let me explain in more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here's the structure of boot stream (first 4K which will be loaded to OCRAM). On left side there are absolute addresses from the beginning of the file. On right side I placed values that are stored in this file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="01.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41903i28E73B07EA77D161/image-size/large?v=v2&amp;amp;px=999" role="button" title="01.png" alt="01.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now when the boot ROM fetches the stream from boot source, the same 4K bytes are placed to some location in OCRAM (I will assume that they are placed from the beginning just for easy of understanding).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="02.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41978iC9CE3867365D077D/image-size/large?v=v2&amp;amp;px=999" role="button" title="02.png" alt="02.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can see that DCD physycal location is 0x0900_0430, but the pointer is pointing to location in DDR which is even not yet initialized.&lt;/P&gt;&lt;P&gt;I have an assumption that ROM will calculate the real address as ( dcd - self + OCRAM_BEGIN ) in this case. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Nov 2013 08:15:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IVT-structure-question/m-p/257598#M24953</guid>
      <dc:creator>dmitryv</dc:creator>
      <dc:date>2013-11-06T08:15:06Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 IVT structure -- question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IVT-structure-question/m-p/257599#M24954</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Dmitry&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DCD table will be copied to OCRAM within the first 4K copy from SD/MMC. And the "dcd" and "self" will be used to count the "offset" of DCD table address, and ROM will read DCD table using this offset from OCRAM. For your case, the offset will be "0x10000430 - 0x10000000 = 0x430". I just dump my uboot, I can see the "dcd" is 0x2780042c, and "self" is 0x27800400, so the offset would be 0x2c = 44, which means the real dcd table is at the 44 / 4&amp;nbsp; + 1= 12nd data of the first 4K data(containing the IVT offset) copied to OCRAM, below is my ivt header definition, you can see the dcd table is at 12nd.&amp;nbsp; So, ROM will use these two value to count the offset, so there will be no DDR address accessed before DCD table is executed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; 43 ivt_header:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word 0x402000D1 /* Tag=0xD1, Len=0x0020, Ver=0x40 */&lt;/P&gt;&lt;P&gt; 44 app_code_jump_v:&amp;nbsp; .word _start&lt;/P&gt;&lt;P&gt; 45 reserv1:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word 0x0&lt;/P&gt;&lt;P&gt; 46 dcd_ptr:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word dcd_hdr&lt;/P&gt;&lt;P&gt; 47 boot_data_ptr:&amp;nbsp;&amp;nbsp;&amp;nbsp; .word boot_data&lt;/P&gt;&lt;P&gt; 48 self_ptr:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word ivt_header&lt;/P&gt;&lt;P&gt; 49 #ifdef CONFIG_SECURE_BOOT&lt;/P&gt;&lt;P&gt; 50 app_code_csf:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word __hab_data&lt;/P&gt;&lt;P&gt; 51 #else&lt;/P&gt;&lt;P&gt; 52 app_code_csf:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word 0x0&lt;/P&gt;&lt;P&gt; 53 #endif&lt;/P&gt;&lt;P&gt; 54 reserv2:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word 0x0&lt;/P&gt;&lt;P&gt; 55 &lt;/P&gt;&lt;P&gt; 56 boot_data:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word TEXT_BASE&lt;/P&gt;&lt;P&gt; 57 #ifdef CONFIG_SECURE_BOOT&lt;/P&gt;&lt;P&gt; 58 image_len:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word __hab_data_end - TEXT_BASE + CONFIG_FLASH_HEADER_OFFSET&lt;/P&gt;&lt;P&gt; 59 #else&lt;/P&gt;&lt;P&gt; 60 image_len:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word _end_of_copy&amp;nbsp; - TEXT_BASE + CONFIG_FLASH_HEADER_OFFSET&lt;/P&gt;&lt;P&gt; 61 #endif&lt;/P&gt;&lt;P&gt; 62 plugin:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word 0x0&lt;/P&gt;&lt;P&gt; 63 &lt;/P&gt;&lt;P&gt; 64 #if defined CONFIG_MX6DL_DDR3&lt;/P&gt;&lt;P&gt; 65 #if defined CONFIG_DDR_32BIT&lt;/P&gt;&lt;P&gt; 66 &lt;STRONG&gt;dcd_hdr&lt;/STRONG&gt;:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word 0x40E001D2 /* Tag=0xD2, Len=59*8 + 4 + 4, Ver=0x40 */&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Nov 2013 09:19:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IVT-structure-question/m-p/257599#M24954</guid>
      <dc:creator>AnsonHuang</dc:creator>
      <dc:date>2013-11-06T09:19:37Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 IVT structure -- question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IVT-structure-question/m-p/257600#M24955</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yongcai,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; About image_len:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word _end_of_copy&amp;nbsp; - TEXT_BASE + CONFIG_FLASH_HEADER_OFFSET&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Why there is the " + CONFIG_FLASH_HEADER_OFFSET".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; In my opinion, _end_of_copy&amp;nbsp; - TEXT_BASE has already been the length of uboot image.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Does " + CONFIG_FLASH_HEADER_OFFSET" mean that ROM loads uboot image from the beginning of emmc instead of from IVT offeset?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Simmis.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jun 2014 08:15:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-IVT-structure-question/m-p/257600#M24955</guid>
      <dc:creator>simmisxu</dc:creator>
      <dc:date>2014-06-13T08:15:19Z</dc:date>
    </item>
  </channel>
</rss>