<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Skype Video call performance on IMX6q</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257577#M24948</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have not tried the non USB camera.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are also able to do video call without an issue for VGA camera. &lt;/P&gt;&lt;P&gt;I have connected HD camera (USB) , which creates an issue after 10 to 15 min of video call.&lt;/P&gt;&lt;P&gt;Temperature detail is as below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After boot completed :- 50 C&lt;/P&gt;&lt;P&gt;Skype Video call, Call is not received at other end, Just preview your camera in screen. :- 60 C&lt;/P&gt;&lt;P&gt;Skype video call, with both video display :- 67 C&lt;/P&gt;&lt;P&gt;Skype video call, with both video display after 1 min :- 75 C&lt;/P&gt;&lt;P&gt;Skype video call, with both video display after 5 min :- 80 C&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you look at the CPU utilization during this process&lt;/P&gt;&lt;P&gt;Skype takes around 50 % of CPU.&lt;/P&gt;&lt;P&gt;Media server takes around 35 to 40 % of CPU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Mar 2014 08:04:44 GMT</pubDate>
    <dc:creator>saurabh206</dc:creator>
    <dc:date>2014-03-04T08:04:44Z</dc:date>
    <item>
      <title>Skype Video call performance on IMX6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257570#M24941</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our Setup is as follows:&lt;/P&gt;&lt;P&gt;Hardware :- Custom hardware based on imx6q&lt;/P&gt;&lt;P&gt;Jellybean 4.3&lt;/P&gt;&lt;P&gt;USB camera connected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Skype Video call performance on IMX6q based Android device is very poor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that Skype is not able to use the Hardware encoder/decoder and it is trying to used software codec.&lt;/P&gt;&lt;P&gt;Because of this all cpu core occupied and chip temperature will increase rapidly. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;System is too hot. GPU3D will work at 3/64 clock.&lt;/P&gt;&lt;P&gt;cooling: cpu cur freq is 996000000&lt;/P&gt;&lt;P&gt;cooling: cpu max freq set to 792000000&lt;/P&gt;&lt;P&gt;W/AudioFlinger( 2349): RecordThread: buffer overflow&lt;/P&gt;&lt;P&gt;D/dalvikvm( 3442): GC_CONCURRENT freed 2174K, 24% free 9581K/12492K, paused 4ms+22ms, total 168ms&lt;/P&gt;&lt;P&gt;Hot alarm is canceled. GPU3D clock will return to 64/64&lt;/P&gt;&lt;P&gt;cooling: cpu cur freq is 792000000&lt;/P&gt;&lt;P&gt;cooling: cpu max freq set to 996000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can we improve the performance? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Feb 2014 09:26:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257570#M24941</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-02-25T09:26:35Z</dc:date>
    </item>
    <item>
      <title>Re: Skype Video call performance on IMX6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257571#M24942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found than any video calling application takes more than 80% of time.&lt;/P&gt;&lt;P&gt;Any update from Freescale team member on this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Feb 2014 18:36:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257571#M24942</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-02-28T18:36:09Z</dc:date>
    </item>
    <item>
      <title>Re: Skype Video call performance on IMX6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257572#M24943</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;VP8 encoding is not supported by the VPU (VP8 decoding is). H.264 BP/CBP encoding + decoding is supported by the VPU. Can you configure skype to use H.264? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also USB camera may not use VPU by default (openmax android layer). It may be doing the encoding in software. Try running with a camera that uses the freescale mxc camera interface (and hence the OpenMax layer)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Mar 2014 16:45:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257572#M24943</guid>
      <dc:creator>varsmolta</dc:creator>
      <dc:date>2014-03-03T16:45:02Z</dc:date>
    </item>
    <item>
      <title>Re: Skype Video call performance on IMX6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257573#M24944</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;I need to check how to configure skype. And verify which codec it uses for the encoding + decoding.&lt;/P&gt;&lt;P&gt;I don't have skype source code, I have just install skype from google play store.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you explain the "USB camera may not use VPU by default (openmax android layer)"? From debug i only found that Due to UVC camera camera frameworks is doing software color conversion.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Mar 2014 17:34:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257573#M24944</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-03-03T17:34:17Z</dc:date>
    </item>
    <item>
      <title>Re: Skype Video call performance on IMX6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257574#M24945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did some research and according to this: &lt;A class="loading" href="http://www.pathpartnertech.com/wp-content/uploads/2013/08/PathPartner_Case_Study_Skype_OMAP4_ICS1.pdf" title="http://www.pathpartnertech.com/wp-content/uploads/2013/08/PathPartner_Case_Study_Skype_OMAP4_ICS1.pdf"&gt;http://www.pathpartnertech.com/wp-content/uploads/2013/08/PathPartner_Case_Study_Skype_OMAP4_ICS1.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Skype for Android uses H.264 for encoding + decoding but does it all in software. These guys used SkypeKit API to support accelerated encoding + decoding on an OMAP4&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alas, Skype discontinued SkypeKit API recently:&lt;/P&gt;&lt;P&gt;&lt;A class="loading" href="https://aragonresearch.com/microsoft-kills-skype-desktop-apis-leaves-developers-scrambling/" title="https://aragonresearch.com/microsoft-kills-skype-desktop-apis-leaves-developers-scrambling/"&gt;https://aragonresearch.com/microsoft-kills-skype-desktop-apis-leaves-developers-scrambling/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="loading" href="https://support.skype.com/en/faq/FA12322/what-is-skypekit" title="https://support.skype.com/en/faq/FA12322/what-is-skypekit"&gt;https://support.skype.com/en/faq/FA12322/what-is-skypekit&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So looks like you can't get accelerated skype performace anymore.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Linphone is an open source SIP video conferencing solution (&lt;A class="loading" href="http://www.linphone.org/eng/download/packages/linphone-for-android-2.0.html" title="http://www.linphone.org/eng/download/packages/linphone-for-android-2.0.html"&gt;http://www.linphone.org/eng/download/packages/linphone-for-android-2.0.html&lt;/A&gt;). I have played with it on i.mx6 running android but have not used the video capability and so I don't know&amp;nbsp; if it uses VPU for accelerating encoding+decoding. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Mar 2014 18:13:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257574#M24945</guid>
      <dc:creator>varsmolta</dc:creator>
      <dc:date>2014-03-03T18:13:18Z</dc:date>
    </item>
    <item>
      <title>Re: Skype Video call performance on IMX6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257575#M24946</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just tried it with our i.MX6Q Sabre Board and it didn't have any problems at all.&lt;/P&gt;&lt;P&gt;Have you tried with a "non usb" camera?.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Mar 2014 21:53:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257575#M24946</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2014-03-03T21:53:17Z</dc:date>
    </item>
    <item>
      <title>Re: Skype Video call performance on IMX6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257576#M24947</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't think I've seen the USB camera trigger thermal cooling, but I've seen video performance issues (glitches) with the SabreSD and our custom board with an iMX6Q.&amp;nbsp; Android JB 4.2.2-1.1.0-ga.&amp;nbsp; The glitches usually appear on the local side preview of the USB camera in Skype and on the far end.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Mar 2014 22:01:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257576#M24947</guid>
      <dc:creator>Chris1z</dc:creator>
      <dc:date>2014-03-03T22:01:24Z</dc:date>
    </item>
    <item>
      <title>Re: Skype Video call performance on IMX6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257577#M24948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have not tried the non USB camera.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are also able to do video call without an issue for VGA camera. &lt;/P&gt;&lt;P&gt;I have connected HD camera (USB) , which creates an issue after 10 to 15 min of video call.&lt;/P&gt;&lt;P&gt;Temperature detail is as below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After boot completed :- 50 C&lt;/P&gt;&lt;P&gt;Skype Video call, Call is not received at other end, Just preview your camera in screen. :- 60 C&lt;/P&gt;&lt;P&gt;Skype video call, with both video display :- 67 C&lt;/P&gt;&lt;P&gt;Skype video call, with both video display after 1 min :- 75 C&lt;/P&gt;&lt;P&gt;Skype video call, with both video display after 5 min :- 80 C&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you look at the CPU utilization during this process&lt;/P&gt;&lt;P&gt;Skype takes around 50 % of CPU.&lt;/P&gt;&lt;P&gt;Media server takes around 35 to 40 % of CPU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Mar 2014 08:04:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257577#M24948</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-03-04T08:04:44Z</dc:date>
    </item>
    <item>
      <title>Re: Skype Video call performance on IMX6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257578#M24949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;&lt;STRONG&gt;&lt;A href="https://community.nxp.com/people/SerchMX"&gt;SerchMX&lt;/A&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is your resolution of camera which have tested?&lt;/P&gt;&lt;P&gt;And in which format it gives the output?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Mar 2014 08:06:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Skype-Video-call-performance-on-IMX6q/m-p/257578#M24949</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-03-04T08:06:53Z</dc:date>
    </item>
  </channel>
</rss>