<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: WiFi encryption support using WPA in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-encryption-support-using-WPA/m-p/257459#M24930</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;P&gt;This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this &lt;/P&gt;&lt;P&gt;discussion, or create another discussion.&lt;BR /&gt;Thanks,&lt;BR /&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Feb 2014 06:39:22 GMT</pubDate>
    <dc:creator>YixingKong</dc:creator>
    <dc:date>2014-02-25T06:39:22Z</dc:date>
    <item>
      <title>WiFi encryption support using WPA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-encryption-support-using-WPA/m-p/257455#M24926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question regarding the WPA in Linux for a imx6q board. e.g. Nitrogen6x.&amp;nbsp; Does any one know how to add code to support the WPA function in WiFi? Thanks advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Aug 2013 16:30:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WiFi-encryption-support-using-WPA/m-p/257455#M24926</guid>
      <dc:creator>billyang</dc:creator>
      <dc:date>2013-08-15T16:30:09Z</dc:date>
    </item>
    <item>
      <title>Re: WiFi encryption support using WPA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-encryption-support-using-WPA/m-p/257456#M24927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;WPA should already be supported in linux. You need to edit the your /etc/wpa_supplicant.conf file in order to properly communicate with your wifi network. Look here for a sample wpa_supplicant.conf file:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/341087"&gt;Re: Embedded system friendly WiFi dongle?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The steps to take are:&lt;/P&gt;&lt;P&gt;1. Edit your /etc/wpa_supplicant.conf file&lt;/P&gt;&lt;P&gt;2. Insert usb wifi dongle (if you don't already have wifi on your board)&lt;/P&gt;&lt;P&gt;3. Type "ifconfig wlan0 up"&lt;/P&gt;&lt;P&gt;4. Type "wpa_supplicant -B -c/etc/wpa_supplicant.conf -iwlan0 -Dwext". This will start the wpa_supplicant daemon and make it use your config file&lt;/P&gt;&lt;P&gt;5. Type "ifconfig wlan0 &amp;lt;ip_addr&amp;gt; netmask 255.255.255.0" where &amp;lt;ip_addr&amp;gt; is the ip address you want to assign to your wlan0 interface&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;test with a ping to another device on your network and if the above works, then you can edit your /etc/network/interfaces file to make the above steps permanent such that you don't have to do this on every bootup&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Aug 2013 18:52:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WiFi-encryption-support-using-WPA/m-p/257456#M24927</guid>
      <dc:creator>varsmolta</dc:creator>
      <dc:date>2013-08-15T18:52:03Z</dc:date>
    </item>
    <item>
      <title>Re: WiFi encryption support using WPA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-encryption-support-using-WPA/m-p/257457#M24928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your help. However, after Step 4 implemented, I got the message as below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@boundary ~$ wpa_supplicant -B -Dwext -iwlan0 -c/etc/wpa_supplicant/wpa_supp&lt;BR /&gt;licant.conf&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;wl1271: firmware booted (Rev 6.1.5.50.74)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;ioctl[SIOCSIWAUTH]: Operation not supported&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;WEXT auth param 4 value 0x0 - root@boundary ~$&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder if you have an idea what "ioctl[SIOCSIWAUTH]: Operation not supported" means?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2013 17:41:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WiFi-encryption-support-using-WPA/m-p/257457#M24928</guid>
      <dc:creator>billyang</dc:creator>
      <dc:date>2013-08-22T17:41:08Z</dc:date>
    </item>
    <item>
      <title>Re: WiFi encryption support using WPA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-encryption-support-using-WPA/m-p/257458#M24929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;P&gt;Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel &lt;/P&gt;&lt;P&gt;free to reply with an update to this discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2014 06:54:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WiFi-encryption-support-using-WPA/m-p/257458#M24929</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-20T06:54:32Z</dc:date>
    </item>
    <item>
      <title>Re: WiFi encryption support using WPA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-encryption-support-using-WPA/m-p/257459#M24930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;P&gt;This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this &lt;/P&gt;&lt;P&gt;discussion, or create another discussion.&lt;BR /&gt;Thanks,&lt;BR /&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Feb 2014 06:39:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WiFi-encryption-support-using-WPA/m-p/257459#M24930</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-25T06:39:22Z</dc:date>
    </item>
  </channel>
</rss>