<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 i.MX6 USB OTG in host mode</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB-OTG-in-host-mode/m-p/257182#M24873</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone successfully used the i.MX6's USB OTG port in host mode?&amp;nbsp; In our hardware design the USB OTG port works great for bootstrapping the processor.&amp;nbsp; However I cannot seem to get it to operate in a host only mode (for use with thumb drives, etc.).&amp;nbsp; It never seems to detect the attached device.&amp;nbsp; Has anyone gotten this to work on one of the Freescale or Boundary development boards?&amp;nbsp; In their own HW design?&amp;nbsp; If so what changes if any were needed to the kernel or its configuration?&amp;nbsp; Thanks for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Sep 2013 19:05:01 GMT</pubDate>
    <dc:creator>JasonDavis</dc:creator>
    <dc:date>2013-09-30T19:05:01Z</dc:date>
    <item>
      <title>i.MX6 USB OTG in host mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB-OTG-in-host-mode/m-p/257182#M24873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone successfully used the i.MX6's USB OTG port in host mode?&amp;nbsp; In our hardware design the USB OTG port works great for bootstrapping the processor.&amp;nbsp; However I cannot seem to get it to operate in a host only mode (for use with thumb drives, etc.).&amp;nbsp; It never seems to detect the attached device.&amp;nbsp; Has anyone gotten this to work on one of the Freescale or Boundary development boards?&amp;nbsp; In their own HW design?&amp;nbsp; If so what changes if any were needed to the kernel or its configuration?&amp;nbsp; Thanks for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Sep 2013 19:05:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB-OTG-in-host-mode/m-p/257182#M24873</guid>
      <dc:creator>JasonDavis</dc:creator>
      <dc:date>2013-09-30T19:05:01Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 USB OTG in host mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB-OTG-in-host-mode/m-p/257183#M24874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt; On SABRE AI CPU card, USB VBUS is controlled thru MAX7310, which in fact is controlled via I2C3,&lt;/P&gt;&lt;P&gt;but both spi nor and weim nor have conflict pad (EIM_D17 EIM_D18) with I2C3. When spi nor or weim nor&lt;/P&gt;&lt;P&gt;is enabled, the I2C3 can't be used, so that USB VBUS can't be powered on - as result the USB OTG can't &lt;BR /&gt;act as host.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;Please check if USB cable is proper for host operations :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/314655#314655"&gt;https://community.freescale.com/message/314655#314655&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Oct 2013 06:22:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB-OTG-in-host-mode/m-p/257183#M24874</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-10-01T06:22:05Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 USB OTG in host mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB-OTG-in-host-mode/m-p/257184#M24875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you setting the USBOTG ID pin to GND ?, that should work to set it as host&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Oct 2013 15:45:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB-OTG-in-host-mode/m-p/257184#M24875</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2013-10-01T15:45:26Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 USB OTG in host mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB-OTG-in-host-mode/m-p/257185#M24876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks guys, adding a pulldown to the USBOTG pin did the trick.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Oct 2013 11:30:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB-OTG-in-host-mode/m-p/257185#M24876</guid>
      <dc:creator>JasonDavis</dc:creator>
      <dc:date>2013-10-02T11:30:15Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 USB OTG in host mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB-OTG-in-host-mode/m-p/257186#M24877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Usually, the USB Mini/Micro cable should do the trick for you.&lt;/P&gt;&lt;P&gt;If you want to have an OTG port, then you design in an AB-plug, where both connectors fit.&lt;/P&gt;&lt;P&gt;Generally speaking, the A connectors (which sets host mode of OTG port) are bigger than B, and hence the former only fit in AB-plugs, whereas the latter fit in both.&lt;/P&gt;&lt;P&gt;An A cable connects the ID pin to GND, and a B does not.&lt;/P&gt;&lt;P&gt;If you want to connect a thumb drive, then get an adapter from Mini/Micro-A to A-plug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Harald Krapfenbauer&lt;/P&gt;&lt;P&gt;Bluetechnix&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2013 18:21:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB-OTG-in-host-mode/m-p/257186#M24877</guid>
      <dc:creator>harald_krapfenb</dc:creator>
      <dc:date>2013-10-03T18:21:51Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 USB OTG in host mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB-OTG-in-host-mode/m-p/257187#M24878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HiSergioSolis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my i.MX6S design, USB_ID pin is directly connected to GND. USD_VBUS is directly connected to 5V supply generated by a buck converter with enough supply capacity.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board easily works in slave mode when it is connected to a host PC (USB_ID=1). but when I change the USB_ID pin to GND and try to use a slave device like USB&amp;nbsp;pen drive, it does not show anything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, I have not used USB_OC and USB_PWR pins in my design. Is it the reason&amp;nbsp;of non-functional&amp;nbsp;host mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 14:54:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-USB-OTG-in-host-mode/m-p/257187#M24878</guid>
      <dc:creator>rahulsoni</dc:creator>
      <dc:date>2016-12-15T14:54:16Z</dc:date>
    </item>
  </channel>
</rss>