<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: LIBUSB_ERROR_NO_DEVICE</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-NO-DEVICE/m-p/2416781#M246874</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442"&gt;@JosephAtNXP&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Sorry for the inconvenience,it was a simple current shortage that caused the issue,when i raised the current to the required level,everything is working fine.&lt;/P&gt;</description>
    <pubDate>Mon, 28 Sep 2026 12:48:18 GMT</pubDate>
    <dc:creator>ap3415</dc:creator>
    <dc:date>2026-09-28T12:48:18Z</dc:date>
    <item>
      <title>LIBUSB_ERROR_NO_DEVICE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-NO-DEVICE/m-p/2416114#M246848</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am having an issue while flashing.i am using an imx8mp processor.&lt;/P&gt;&lt;P&gt;vougavent@vougavent-work-station1:~/Desktop/imx-yocto-bsp/build-wayland2/tmp/deploy/images/imx8mp-lpddr4-evk$ sudo uuu -v -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk core-image-weston-imx8mp-lpddr4-evk-20260725065928.rootfs.wic.bz2&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- lib1.4.193&lt;/P&gt;&lt;P&gt;Build in config:&lt;BR /&gt;Pctl Chip Vid Pid BcdVersion&lt;BR /&gt;==================================================&lt;BR /&gt;SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]&lt;BR /&gt;SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]&lt;BR /&gt;SDPS: MX8DXL 0x1fc9 0x0147&lt;BR /&gt;SDPS: MX28 0x15a2 0x004f&lt;BR /&gt;SDPS: MX815 0x1fc9 0x013e&lt;BR /&gt;SDPS: MX865 0x1fc9 0x0146&lt;BR /&gt;SDPS: MX8ULP 0x1fc9 0x014a&lt;BR /&gt;SDPS: MX8ULP 0x1fc9 0x014b&lt;BR /&gt;SDP: MX7D 0x15a2 0x0076&lt;BR /&gt;SDP: MX6Q 0x15a2 0x0054&lt;BR /&gt;SDP: MX6D 0x15a2 0x0061&lt;BR /&gt;SDP: MX6SL 0x15a2 0x0063&lt;BR /&gt;SDP: MX6SX 0x15a2 0x0071&lt;BR /&gt;SDP: MX6UL 0x15a2 0x007d&lt;BR /&gt;SDP: MX6ULL 0x15a2 0x0080&lt;BR /&gt;SDP: MX6SLL 0x1fc9 0x0128&lt;BR /&gt;SDP: MX7ULP 0x1fc9 0x0126&lt;BR /&gt;SDP: MXRT106X 0x1fc9 0x0135&lt;BR /&gt;SDP: MX8MM 0x1fc9 0x0134&lt;BR /&gt;SDP: MX8MQ 0x1fc9 0x012b&lt;BR /&gt;SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]&lt;BR /&gt;SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]&lt;BR /&gt;SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998]&lt;BR /&gt;SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]&lt;BR /&gt;SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]&lt;BR /&gt;SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]&lt;BR /&gt;FBK: 0x066f 0x9afe&lt;BR /&gt;FBK: 0x066f 0x9bff&lt;BR /&gt;FBK: 0x1fc9 0x0153&lt;BR /&gt;FB: 0x0525 0xa4a5&lt;BR /&gt;FB: 0x18d1 0x0d02&lt;BR /&gt;FB: 0x3016 0x0001&lt;BR /&gt;FB: 0x1fc9 0x0152&lt;/P&gt;&lt;P&gt;Run built-in script:&lt;BR /&gt;&lt;BR /&gt;uuu_version 1.4.149&lt;/P&gt;&lt;P&gt;# @_flash.bin | bootloader, which can extract from wic image&lt;BR /&gt;# @_image [_flash.bin] | wic image burn to emmc.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ&lt;BR /&gt;SDP: boot -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk -scanlimited 0x800000&lt;/P&gt;&lt;P&gt;# This command will be run when ROM support stream mode&lt;BR /&gt;# i.MX8QXP, i.MX8QM&lt;BR /&gt;SDPS: boot -scanterm -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk -scanlimited 0x800000&lt;/P&gt;&lt;P&gt;# These commands will be run when use SPL and will be skipped if no spl&lt;BR /&gt;# SDPU will be deprecated. please use SDPV instead of SDPU&lt;BR /&gt;# {&lt;BR /&gt;SDPU: delay 1000&lt;BR /&gt;SDPU: write -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk -offset 0x57c00&lt;BR /&gt;SDPU: jump -scanlimited 0x800000&lt;BR /&gt;# }&lt;/P&gt;&lt;P&gt;# These commands will be run when use SPL and will be skipped if no spl&lt;BR /&gt;# if (SPL support SDPV)&lt;BR /&gt;# {&lt;BR /&gt;SDPV: delay 1000&lt;BR /&gt;SDPV: write -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk -skipspl -scanterm -scanlimited 0x800000&lt;BR /&gt;SDPV: jump -scanlimited 0x800000&lt;BR /&gt;# }&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;FB: ucmd setenv fastboot_dev mmc&lt;BR /&gt;FB: ucmd setenv mmcdev ${emmc_dev}&lt;BR /&gt;FB: ucmd mmc dev ${emmc_dev}&lt;BR /&gt;FB: flash -raw2sparse all core-image-weston-imx8mp-lpddr4-evk-20260725065928.rootfs.wic.bz2/*&lt;BR /&gt;FB: flash -scanterm -scanlimited 0x800000 bootloader imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk&lt;BR /&gt;FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;&lt;BR /&gt;FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0&lt;BR /&gt;FB: done&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wait for Known USB Device Appear...&lt;BR /&gt;New USB Device Attached at 1:10&lt;BR /&gt;1:10&amp;gt;Start Cmd:SDPS: boot -scanterm -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk -scanlimited 0x800000&lt;BR /&gt;33%1:10&amp;gt;Fail HID(W):LIBUSB_ERROR_NO_DEVICE(0.786s)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Sep 2026 12:36:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-NO-DEVICE/m-p/2416114#M246848</guid>
      <dc:creator>ap3415</dc:creator>
      <dc:date>2026-09-24T12:36:28Z</dc:date>
    </item>
    <item>
      <title>Re: LIBUSB_ERROR_NO_DEVICE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-NO-DEVICE/m-p/2416366#M246860</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;In your setup do you use a custom board or an i.MX 8M Plus EVK? If you are using a custom board I would advise to modify the necessary code, focusing in memory and power necessary differences. Then confirming your porting is valid and being applied.&lt;/P&gt;
&lt;P&gt;The error is seen when using an invalid imx-boot firmware image, another reasons can be defective cables or some USB power sources reset, you could try using a wall mount USB charger.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2026 15:04:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-NO-DEVICE/m-p/2416366#M246860</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2026-09-25T15:04:30Z</dc:date>
    </item>
    <item>
      <title>Re: LIBUSB_ERROR_NO_DEVICE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-NO-DEVICE/m-p/2416781#M246874</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442"&gt;@JosephAtNXP&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Sorry for the inconvenience,it was a simple current shortage that caused the issue,when i raised the current to the required level,everything is working fine.&lt;/P&gt;</description>
      <pubDate>Mon, 28 Sep 2026 12:48:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-NO-DEVICE/m-p/2416781#M246874</guid>
      <dc:creator>ap3415</dc:creator>
      <dc:date>2026-09-28T12:48:18Z</dc:date>
    </item>
  </channel>
</rss>