<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX 8M Plus: RGMII to MII Migration – ENET_RXC / RX_ER Pin Assignment</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-RGMII-to-MII-Migration-ENET-RXC-RX-ER-Pin/m-p/2416214#M246853</link>
    <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I am working on a custom Ethernet design using the NXP i.MX 8M Plus SoC with a PHYTEC phyCORE-i.MX8M Plus SOM.&lt;/P&gt;&lt;P&gt;We currently have an Ethernet design based on RGMII, and we are evaluating a migration from RGMII to MII for our custom board.&lt;/P&gt;&lt;P&gt;During the pinmux review, I found the following functions for the i.MX 8M Plus ENET_RXC pad:&lt;/P&gt;&lt;P&gt;ALT0: CCM_ENET_QOS_CLOCK_GENERATE_RX_CLK&lt;BR /&gt;ALT1: ENET_QOS_RX_ER&lt;BR /&gt;ALT5: GPIO1_IO25&lt;/P&gt;&lt;P&gt;In our PHYTEC SOM allocation, this signal is associated with SOM pin A25.&lt;/P&gt;&lt;P&gt;My concern is related to the RGMII to MII migration. The required Ethernet signals are different between RGMII and MII.&lt;/P&gt;&lt;P&gt;I would like to clarify the following points:&lt;/P&gt;&lt;P&gt;1. Does the i.MX 8M Plus ENET_QOS MAC support a true MII interface in addition to RGMII and RMII?&lt;/P&gt;&lt;P&gt;2. If true MII is supported, what is the correct i.MX 8M Plus pin mapping for MII_RX_CLK, MII_RX_DV, MII_RX_ER, MII_RXD0 to MII_RXD3, MII_TX_CLK, MII_TX_EN, and MII_TXD0 to MII_TXD3?&lt;/P&gt;&lt;P&gt;3. For the ENET_RXC pad, is ALT0, CCM_ENET_QOS_CLOCK_GENERATE_RX_CLK, intended only for RGMII, or can this function be used as the MII receive clock?&lt;/P&gt;&lt;P&gt;4. During an RGMII to MII migration, is ENET_QOS_RX_ER on the ENET_RXC pad required for the MII interface?&lt;/P&gt;&lt;P&gt;5. If MII_RX_ER is required, can it be assigned to another available i.MX 8M Plus pad through IOMUX, or is this signal internally associated with the ENET_RXC pad?&lt;/P&gt;&lt;P&gt;6. Since we are using a PHYTEC phyCORE-i.MX8M Plus SOM, are there any SOM routing limitations that need to be considered for implementing the MII interface?&lt;/P&gt;&lt;P&gt;7. If MII is supported, could someone provide an example or reference for the correct i.MX 8M Plus MII MAC-to-PHY pin configuration and device-tree configuration?&lt;/P&gt;&lt;P&gt;The reason for this clarification is that we are currently preparing the pinmux and schematic for a Bosch custom carrier board. We want to confirm the correct MII signal mapping before changing the SOM and carrier-board pin allocation.&lt;/P&gt;&lt;P&gt;The relevant pinmux information from our BSP is:&lt;/P&gt;&lt;P&gt;ENET_RXC&lt;BR /&gt;ALT0: CCM_ENET_QOS_CLOCK_GENERATE_RX_CLK&lt;BR /&gt;ALT1: ENET_QOS_RX_ER&lt;BR /&gt;ALT5: GPIO1_IO25&lt;/P&gt;&lt;P&gt;Could someone please confirm whether a true RGMII-to-MII migration is supported on the i.MX 8M Plus ENET_QOS MAC and, if so, how ENET_RXC and RX_ER should be handled?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Fri, 25 Sep 2026 05:38:41 GMT</pubDate>
    <dc:creator>Rameshkumar-PHYTEC</dc:creator>
    <dc:date>2026-09-25T05:38:41Z</dc:date>
    <item>
      <title>i.MX 8M Plus: RGMII to MII Migration – ENET_RXC / RX_ER Pin Assignment</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-RGMII-to-MII-Migration-ENET-RXC-RX-ER-Pin/m-p/2416214#M246853</link>
      <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I am working on a custom Ethernet design using the NXP i.MX 8M Plus SoC with a PHYTEC phyCORE-i.MX8M Plus SOM.&lt;/P&gt;&lt;P&gt;We currently have an Ethernet design based on RGMII, and we are evaluating a migration from RGMII to MII for our custom board.&lt;/P&gt;&lt;P&gt;During the pinmux review, I found the following functions for the i.MX 8M Plus ENET_RXC pad:&lt;/P&gt;&lt;P&gt;ALT0: CCM_ENET_QOS_CLOCK_GENERATE_RX_CLK&lt;BR /&gt;ALT1: ENET_QOS_RX_ER&lt;BR /&gt;ALT5: GPIO1_IO25&lt;/P&gt;&lt;P&gt;In our PHYTEC SOM allocation, this signal is associated with SOM pin A25.&lt;/P&gt;&lt;P&gt;My concern is related to the RGMII to MII migration. The required Ethernet signals are different between RGMII and MII.&lt;/P&gt;&lt;P&gt;I would like to clarify the following points:&lt;/P&gt;&lt;P&gt;1. Does the i.MX 8M Plus ENET_QOS MAC support a true MII interface in addition to RGMII and RMII?&lt;/P&gt;&lt;P&gt;2. If true MII is supported, what is the correct i.MX 8M Plus pin mapping for MII_RX_CLK, MII_RX_DV, MII_RX_ER, MII_RXD0 to MII_RXD3, MII_TX_CLK, MII_TX_EN, and MII_TXD0 to MII_TXD3?&lt;/P&gt;&lt;P&gt;3. For the ENET_RXC pad, is ALT0, CCM_ENET_QOS_CLOCK_GENERATE_RX_CLK, intended only for RGMII, or can this function be used as the MII receive clock?&lt;/P&gt;&lt;P&gt;4. During an RGMII to MII migration, is ENET_QOS_RX_ER on the ENET_RXC pad required for the MII interface?&lt;/P&gt;&lt;P&gt;5. If MII_RX_ER is required, can it be assigned to another available i.MX 8M Plus pad through IOMUX, or is this signal internally associated with the ENET_RXC pad?&lt;/P&gt;&lt;P&gt;6. Since we are using a PHYTEC phyCORE-i.MX8M Plus SOM, are there any SOM routing limitations that need to be considered for implementing the MII interface?&lt;/P&gt;&lt;P&gt;7. If MII is supported, could someone provide an example or reference for the correct i.MX 8M Plus MII MAC-to-PHY pin configuration and device-tree configuration?&lt;/P&gt;&lt;P&gt;The reason for this clarification is that we are currently preparing the pinmux and schematic for a Bosch custom carrier board. We want to confirm the correct MII signal mapping before changing the SOM and carrier-board pin allocation.&lt;/P&gt;&lt;P&gt;The relevant pinmux information from our BSP is:&lt;/P&gt;&lt;P&gt;ENET_RXC&lt;BR /&gt;ALT0: CCM_ENET_QOS_CLOCK_GENERATE_RX_CLK&lt;BR /&gt;ALT1: ENET_QOS_RX_ER&lt;BR /&gt;ALT5: GPIO1_IO25&lt;/P&gt;&lt;P&gt;Could someone please confirm whether a true RGMII-to-MII migration is supported on the i.MX 8M Plus ENET_QOS MAC and, if so, how ENET_RXC and RX_ER should be handled?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2026 05:38:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-RGMII-to-MII-Migration-ENET-RXC-RX-ER-Pin/m-p/2416214#M246853</guid>
      <dc:creator>Rameshkumar-PHYTEC</dc:creator>
      <dc:date>2026-09-25T05:38:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Plus: RGMII to MII Migration – ENET_RXC / RX_ER Pin Assignment</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-RGMII-to-MII-Migration-ENET-RXC-RX-ER-Pin/m-p/2416373#M246862</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;This issue is related to &lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ENET-RXC-A25-Pinmux-Clarification-for-MII-Interface/m-p/2416236" target="_self"&gt;this topic&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;I will add in this thread the ENET_QOS details since they were not asked previously.&lt;/P&gt;
&lt;P&gt;Neither ENET nor ENET_QOS / EQOS support MII, please refer to the following information from RM of EQOS:&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;RMII (10/100Mbps), RGMII (10/100/1000Mbps)&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;From DS:&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;1.8 V/3.3 V RMII operation, 1.8 V RGMII operation&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Post mentions ENET signals interfacing EQOS signals. ENET signals correspond to ENET module, while ENET_QOS correspond to EQOS module, make sure to review that an available signal in PHYTEC SOM can be mapped to your desired function, you can base in &lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.18.y/arch/arm64/boot/dts/freescale/imx8mp-pinfunc.h" target="_self"&gt;pinfunc.h&lt;/A&gt;&amp;nbsp;&amp;nbsp;or config tools.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JosephAtNXP_0-1790354711558.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/396873iD3BFB2D99A5B37F0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JosephAtNXP_0-1790354711558.png" alt="JosephAtNXP_0-1790354711558.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Download Config Tools for i.MX &lt;A href="https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX" target="_self"&gt;here&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2026 16:45:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-RGMII-to-MII-Migration-ENET-RXC-RX-ER-Pin/m-p/2416373#M246862</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2026-09-25T16:45:50Z</dc:date>
    </item>
  </channel>
</rss>