<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックInline ECC validation method</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Inline-ECC-validation-method/m-p/2414978#M246786</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I am working on Inline ECC implementation for iMX8M Plus on external DDR memory.&lt;BR /&gt;ECC appears to be working (U-Boot modifications done, EDAC driver showing up in Linux,&amp;nbsp;/sys/devices/system/edac/mc/mc0/ virtual files are present).&lt;BR /&gt;&lt;BR /&gt;I'm looking for ways to test and validate the protection.&lt;BR /&gt;&lt;BR /&gt;My understanding is that error injection is not possible into the data itself, and that ECC parity bits must be corrupted instead.&lt;BR /&gt;&lt;BR /&gt;AN 13566 section 3.2.9 states : "Further information on this feature is available on request."&lt;BR /&gt;&lt;BR /&gt;How can I request this information ? Is there a specific NXP contact/channel for this ?&lt;BR /&gt;&lt;BR /&gt;Thank you in advance,&lt;/P&gt;</description>
    <pubDate>Mon, 21 Sep 2026 11:35:46 GMT</pubDate>
    <dc:creator>pinkpr_6408</dc:creator>
    <dc:date>2026-09-21T11:35:46Z</dc:date>
    <item>
      <title>Inline ECC validation method</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inline-ECC-validation-method/m-p/2414978#M246786</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I am working on Inline ECC implementation for iMX8M Plus on external DDR memory.&lt;BR /&gt;ECC appears to be working (U-Boot modifications done, EDAC driver showing up in Linux,&amp;nbsp;/sys/devices/system/edac/mc/mc0/ virtual files are present).&lt;BR /&gt;&lt;BR /&gt;I'm looking for ways to test and validate the protection.&lt;BR /&gt;&lt;BR /&gt;My understanding is that error injection is not possible into the data itself, and that ECC parity bits must be corrupted instead.&lt;BR /&gt;&lt;BR /&gt;AN 13566 section 3.2.9 states : "Further information on this feature is available on request."&lt;BR /&gt;&lt;BR /&gt;How can I request this information ? Is there a specific NXP contact/channel for this ?&lt;BR /&gt;&lt;BR /&gt;Thank you in advance,&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2026 11:35:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inline-ECC-validation-method/m-p/2414978#M246786</guid>
      <dc:creator>pinkpr_6408</dc:creator>
      <dc:date>2026-09-21T11:35:46Z</dc:date>
    </item>
    <item>
      <title>Re: Inline ECC validation method</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inline-ECC-validation-method/m-p/2415178#M246804</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am implementing Inline ECC on an i.MX 8M Plus with external DDR. ECC appears to be working correctly: U-Boot has been configured, the Linux EDAC driver is active, and /sys/devices/system/edac/mc/mc0/ is present.&lt;/P&gt;&lt;P&gt;I would now like to validate the ECC protection by deliberately generating correctable and uncorrectable errors.&lt;/P&gt;&lt;P&gt;AN13566, section 3.2.9, states that Inline ECC errors can be injected by unlocking the ECC region using ECC_REGION_PARITY_LOCK and overriding the ECC parity bits. It also mentions that further information on this feature is available on request.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Sep 2026 08:04:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inline-ECC-validation-method/m-p/2415178#M246804</guid>
      <dc:creator>natasha052gandhi</dc:creator>
      <dc:date>2026-09-22T08:04:00Z</dc:date>
    </item>
    <item>
      <title>Re: Inline ECC validation method</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inline-ECC-validation-method/m-p/2415461#M246815</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Sure we can provide it, but for this I would require you to create a support ticket&lt;BR /&gt;&lt;A href="https://support.nxp.com/s/?language=en_US" target="_blank"&gt;https://support.nxp.com/s/?language=en_US&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;You may mention me in the body of the request so I can track the ticket and provide the material.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Sep 2026 21:22:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inline-ECC-validation-method/m-p/2415461#M246815</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2026-09-22T21:22:20Z</dc:date>
    </item>
  </channel>
</rss>