<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Unable to get serial console or boot linux on MCIMX8Q!XP-CPU (Si B0) - only garbage on UART in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-get-serial-console-or-boot-linux-on-MCIMX8Q-XP-CPU-Si/m-p/2407789#M246486</link>
    <description>also i want to run windows can you help to choose the file for this board.</description>
    <pubDate>Mon, 24 Aug 2026 11:15:50 GMT</pubDate>
    <dc:creator>drupadh</dc:creator>
    <dc:date>2026-08-24T11:15:50Z</dc:date>
    <item>
      <title>Unable to get serial console or boot linux on MCIMX8Q!XP-CPU (Si B0) - only garbage on UART</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-get-serial-console-or-boot-linux-on-MCIMX8Q-XP-CPU-Si/m-p/2404414#M246350</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am facing issues bringing up the &lt;STRONG&gt;MCIMX8QXP-CPU (Silicon Revision B0)&lt;/STRONG&gt; board.&lt;/P&gt;&lt;H3&gt;Hardware:&lt;/H3&gt;&lt;UL&gt;&lt;LI&gt;MCIMX8QXP-CPU (Si B0)&lt;/LI&gt;&lt;LI&gt;MCIMX8-8X-BB baseboard&lt;/LI&gt;&lt;LI&gt;IMX-LVDS-HDMI adapter connected to J1&lt;/LI&gt;&lt;LI&gt;Original 16 GB SD card that came with the kit&lt;/LI&gt;&lt;LI&gt;Also tried a newly flashed 32 GB SD card with official Linux BSP (L6.18.20 / MX8QXPC0 image)&lt;/LI&gt;&lt;/UL&gt;&lt;H3&gt;Problem:&lt;/H3&gt;&lt;OL&gt;&lt;LI&gt;&lt;STRONG&gt;Serial console (J11)&lt;/STRONG&gt; always shows only garbage characters (□□□□) at 115200 8N1.&lt;UL&gt;&lt;LI&gt;Tried multiple COM ports&lt;/LI&gt;&lt;LI&gt;Tried different terminal software (PuTTY, Docklight)&lt;/LI&gt;&lt;LI&gt;Tried on two different Windows laptops&lt;/LI&gt;&lt;LI&gt;Installed latest FTDI VCP drivers&lt;/LI&gt;&lt;LI&gt;Same result with original kit SD card and newly flashed card&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;UUU&lt;/STRONG&gt; never detects the board in Serial Download Mode (SW2 = 1000). &lt;SPAN&gt;uuu -lsusb&lt;/SPAN&gt; shows no device. Board does not appear in Device Manager when in download mode.&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;HDMI&lt;/STRONG&gt; – no display output so far (using IMX-LVDS-HDMI on J1).&lt;/LI&gt;&lt;/OL&gt;&lt;H3&gt;Boot switches tried:&lt;/H3&gt;&lt;UL&gt;&lt;LI&gt;SD boot: SW2 = ON ON OFF OFF&lt;/LI&gt;&lt;LI&gt;Serial Download: SW2 = ON OFF OFF OFF&lt;/LI&gt;&lt;LI&gt;eMMC: SW2 = OFF ON OFF OFF&lt;/LI&gt;&lt;/UL&gt;&lt;H3&gt;What I have already done:&lt;/H3&gt;&lt;UL&gt;&lt;LI&gt;Flashed official &lt;SPAN&gt;.Sdcard&amp;nbsp;&lt;/SPAN&gt;image using Balena Etcher and Rufus&lt;/LI&gt;&lt;LI&gt;Verified SD card is properly inserted in J12&lt;/LI&gt;&lt;LI&gt;Used original power supply&lt;/LI&gt;&lt;LI&gt;Checked multiple USB cables for the debug port&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Could someone please advise:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Is there any known issue with Si B0 boards regarding the debug UART?&lt;/LI&gt;&lt;LI&gt;Any additional steps to get clean console output?&lt;/LI&gt;&lt;LI&gt;Recommended way to recover / verify the board is healthy?&lt;P&gt;  &lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Aug 2026 05:37:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-get-serial-console-or-boot-linux-on-MCIMX8Q-XP-CPU-Si/m-p/2404414#M246350</guid>
      <dc:creator>drupadh</dc:creator>
      <dc:date>2026-08-13T05:37:28Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to get serial console or boot linux on MCIMX8Q!XP-CPU (Si B0) - only garbage on UART</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-get-serial-console-or-boot-linux-on-MCIMX8Q-XP-CPU-Si/m-p/2407124#M246472</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/265559"&gt;@drupadh&lt;/a&gt;,&lt;BR /&gt;Thank you for contacting NXP Support!&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;The error you are experiencing occurs because the image was built for the C0 silicon revision.&lt;/P&gt;
&lt;P&gt;Unfortunately, we do not provide a precompiled 6.18.20 kernel image for the B0 silicon revision. However, you can build it yourself using Yocto.&lt;/P&gt;
&lt;P&gt;For the build, please use the following machine configuration "&lt;SPAN&gt;imx8qxpmek&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please let me know if you need any assistance with the build process.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Alejandro Garcia&lt;/P&gt;
&lt;P&gt;&lt;LI-WRAPPER&gt;&lt;/LI-WRAPPER&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Aug 2026 21:52:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-get-serial-console-or-boot-linux-on-MCIMX8Q-XP-CPU-Si/m-p/2407124#M246472</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2026-08-20T21:52:58Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to get serial console or boot linux on MCIMX8Q!XP-CPU (Si B0) - only garbage on UART</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-get-serial-console-or-boot-linux-on-MCIMX8Q-XP-CPU-Si/m-p/2407787#M246485</link>
      <description>&lt;P&gt;Is there any step by step guide to follow that will be very much helpful.&lt;/P&gt;</description>
      <pubDate>Mon, 24 Aug 2026 11:08:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-get-serial-console-or-boot-linux-on-MCIMX8Q-XP-CPU-Si/m-p/2407787#M246485</guid>
      <dc:creator>drupadh</dc:creator>
      <dc:date>2026-08-24T11:08:16Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to get serial console or boot linux on MCIMX8Q!XP-CPU (Si B0) - only garbage on UART</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-get-serial-console-or-boot-linux-on-MCIMX8Q-XP-CPU-Si/m-p/2407789#M246486</link>
      <description>also i want to run windows can you help to choose the file for this board.</description>
      <pubDate>Mon, 24 Aug 2026 11:15:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-get-serial-console-or-boot-linux-on-MCIMX8Q-XP-CPU-Si/m-p/2407789#M246486</guid>
      <dc:creator>drupadh</dc:creator>
      <dc:date>2026-08-24T11:15:50Z</dc:date>
    </item>
  </channel>
</rss>