<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Unable to successfully program the eMMC on the i.MX93EVK using UUU in Download Mode in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-successfully-program-the-eMMC-on-the-i-MX93EVK-using/m-p/2405833#M246431</link>
    <description>&lt;P&gt;I had the very same issue with an FRDM-imx93. Flashing from Linux can be a solution, but if someone else faces the problem, the following worked for me.&lt;/P&gt;&lt;P&gt;When you get the U-Boot shell:&lt;/P&gt;&lt;P&gt;No USB device found USB init failed: -19 u-boot=&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;You can try:&lt;/P&gt;&lt;PRE&gt;=&amp;gt; usb stop
=&amp;gt; usb start
=&amp;gt; fastboot usb 0&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If it fails, unplug/replug (board side) only the USB dedicated to serial downloading and repeat those commands. At that point, USB should be discoverable by uuu, so uuu can proceed.&lt;BR /&gt;Note that uuu shall continue to run in the meantime (waiting for a USB device to appear).&lt;/P&gt;</description>
    <pubDate>Mon, 17 Aug 2026 16:37:34 GMT</pubDate>
    <dc:creator>gabriserra</dc:creator>
    <dc:date>2026-08-17T16:37:34Z</dc:date>
    <item>
      <title>Unable to successfully program the eMMC on the i.MX93EVK using UUU in Download Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-successfully-program-the-eMMC-on-the-i-MX93EVK-using/m-p/2349760#M244861</link>
      <description>&lt;UL&gt;&lt;LI&gt;WSL ubuntu 20.04&lt;BR /&gt;&lt;BR /&gt;&lt;/LI&gt;&lt;LI&gt;LF_v6.12.49-2.2.0_images_IMX93EVK.zip&lt;BR /&gt;&lt;BR /&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;sudo uuu uuu.auto&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-4-ga377d1e&lt;/P&gt;&lt;P&gt;Success 0 Failure 0&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;1:1-6458439E 1/ 1 [=================100%=================] SDPS: boot -f imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;Uboot info&lt;BR /&gt;&lt;P&gt;U-Boot 2025.04-g4ddbad60eff3 (Nov 19 2025 - 07:56:58 +0000)&lt;/P&gt;&lt;P&gt;Reset Status: POR&lt;/P&gt;&lt;P&gt;CPU: NXP i.MX93(52) Rev1.1 A55 at 1700 MHz&lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 40C&lt;BR /&gt;Model: NXP i.MX93 11X11 EVK board&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C2 0x52]&lt;BR /&gt;SNK.Power3.0 on CC1&lt;BR /&gt;tcpc_pd_receive_message: Polling ALERT register, TCPC_ALERT_RX_STATUS bit failed, ret = -62&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C2 0x51]&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C2 0x50]&lt;BR /&gt;Core: 251 devices, 38 uclasses, devicetree: separate&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Loading Environment from nowhere... OK&lt;BR /&gt;[*]-Video Link 0adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device hdmi@3d&lt;BR /&gt;fail to get display timings&lt;BR /&gt;probe video device failed, ret -19&lt;/P&gt;&lt;P&gt;[0] lcd-controller@4ae30000, video&lt;BR /&gt;[1] dsi@4ae10000, video_bridge&lt;BR /&gt;[2] hdmi@3d, panel&lt;BR /&gt;adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device hdmi@3d&lt;BR /&gt;fail to get display timings&lt;BR /&gt;probe video device failed, ret -19&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ELE firmware version 2.0.4-e804f3c9&lt;/P&gt;&lt;P&gt;MMC: no card present&lt;BR /&gt;UID: 6458439e25d046af8f674c2455dfa2dd&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Net: eth0: ethernet@42890000, eth1: ethernet@428a0000 [PRIME]&lt;BR /&gt;Fastboot: Normal&lt;/P&gt;&lt;P&gt;Boot from USB for mfgtools&lt;BR /&gt;*** Warning - Use default environment for mfgtools&lt;BR /&gt;, using default environment&lt;/P&gt;&lt;P&gt;Run bootcmd_mfg: run mfgtool_args; if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else ${kboot} ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo Run fastboot ...; ${fb_cmd}; fi;&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;/P&gt;&lt;P&gt;## Checking Image at 83800000 ...&lt;BR /&gt;Unknown image format!&lt;BR /&gt;Run fastboot ...&lt;BR /&gt;auto usb 0&lt;BR /&gt;Failed to configure default pinctrl&lt;BR /&gt;Failed to initialize board for USB&lt;BR /&gt;Failed to configure default pinctrl&lt;BR /&gt;Failed to initialize board for USB&lt;BR /&gt;No USB device found&lt;BR /&gt;USB init failed: -19&lt;BR /&gt;u-boot=&amp;gt;&lt;/P&gt;Thank you very much for your answer&lt;BR /&gt;&lt;BR /&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Sun, 12 Apr 2026 11:26:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-successfully-program-the-eMMC-on-the-i-MX93EVK-using/m-p/2349760#M244861</guid>
      <dc:creator>weiyi</dc:creator>
      <dc:date>2026-04-12T11:26:56Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to successfully program the eMMC on the i.MX93EVK using UUU in Download Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-successfully-program-the-eMMC-on-the-i-MX93EVK-using/m-p/2349850#M244868</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/261595"&gt;@weiyi&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;在Windows下面烧写也会有这个错误吗？&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Mon, 13 Apr 2026 03:29:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-successfully-program-the-eMMC-on-the-i-MX93EVK-using/m-p/2349850#M244868</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2026-04-13T03:29:48Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to successfully program the eMMC on the i.MX93EVK using UUU in Download Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-successfully-program-the-eMMC-on-the-i-MX93EVK-using/m-p/2350133#M244878</link>
      <description>我已经通过SD卡进入Linux，随后dd写入flash wic镜像修复了这个问题。</description>
      <pubDate>Mon, 13 Apr 2026 11:32:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-successfully-program-the-eMMC-on-the-i-MX93EVK-using/m-p/2350133#M244878</guid>
      <dc:creator>weiyi</dc:creator>
      <dc:date>2026-04-13T11:32:54Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to successfully program the eMMC on the i.MX93EVK using UUU in Download Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-successfully-program-the-eMMC-on-the-i-MX93EVK-using/m-p/2405833#M246431</link>
      <description>&lt;P&gt;I had the very same issue with an FRDM-imx93. Flashing from Linux can be a solution, but if someone else faces the problem, the following worked for me.&lt;/P&gt;&lt;P&gt;When you get the U-Boot shell:&lt;/P&gt;&lt;P&gt;No USB device found USB init failed: -19 u-boot=&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;You can try:&lt;/P&gt;&lt;PRE&gt;=&amp;gt; usb stop
=&amp;gt; usb start
=&amp;gt; fastboot usb 0&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If it fails, unplug/replug (board side) only the USB dedicated to serial downloading and repeat those commands. At that point, USB should be discoverable by uuu, so uuu can proceed.&lt;BR /&gt;Note that uuu shall continue to run in the meantime (waiting for a USB device to appear).&lt;/P&gt;</description>
      <pubDate>Mon, 17 Aug 2026 16:37:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-successfully-program-the-eMMC-on-the-i-MX93EVK-using/m-p/2405833#M246431</guid>
      <dc:creator>gabriserra</dc:creator>
      <dc:date>2026-08-17T16:37:34Z</dc:date>
    </item>
  </channel>
</rss>