<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i2c problems during wakeup frum suspend</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i2c-problems-during-wakeup-frum-suspend/m-p/2402437#M246287</link>
    <description>&lt;P&gt;I use Kernel Version&amp;nbsp;6.6.23&lt;/P&gt;</description>
    <pubDate>Thu, 06 Aug 2026 09:02:39 GMT</pubDate>
    <dc:creator>RRD101</dc:creator>
    <dc:date>2026-08-06T09:02:39Z</dc:date>
    <item>
      <title>i2c problems during wakeup frum suspend</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i2c-problems-during-wakeup-frum-suspend/m-p/2402352#M246282</link>
      <description>&lt;P&gt;A question for the experts out there.&lt;BR /&gt;I have a circuit in which several push-button switches are connected to a GPIO expander. My current system is based on an IMX8MP, to which this GPIO expander is connected via I²C. This expander has an interrupt line to the IMX8MP. Often, when I put the system into suspend mode and press one of the push buttons (the expander is also marked as a wake-up source in the device tree), I receive this message hundreds or even thousands of times as soon as the system comes out of suspend: [ 117.113106] pca953x 3-0076: failed reading register. I know there was already a patch for a similar issue in the i2c-imx.c driver, and I’ve applied it. However, it isn’t having the desired effect. What can I do about this? P.S. It doesn’t happen all the time, but it can be reproduced relatively quickly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards R.&lt;/P&gt;</description>
      <pubDate>Thu, 06 Aug 2026 05:15:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i2c-problems-during-wakeup-frum-suspend/m-p/2402352#M246282</guid>
      <dc:creator>RRD101</dc:creator>
      <dc:date>2026-08-06T05:15:06Z</dc:date>
    </item>
    <item>
      <title>Re: i2c problems during wakeup frum suspend</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i2c-problems-during-wakeup-frum-suspend/m-p/2402410#M246286</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/115185"&gt;@RRD101&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Based on your description, it seems like you could try &lt;A href="https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git/commit/?id=3e38f946062b4845961ab86b726651b4457b2af8" target="_blank"&gt;this commit&lt;/A&gt;. Also, which kernel version are you using?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Thu, 06 Aug 2026 07:18:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i2c-problems-during-wakeup-frum-suspend/m-p/2402410#M246286</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2026-08-06T07:18:28Z</dc:date>
    </item>
    <item>
      <title>Re: i2c problems during wakeup frum suspend</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i2c-problems-during-wakeup-frum-suspend/m-p/2402437#M246287</link>
      <description>&lt;P&gt;I use Kernel Version&amp;nbsp;6.6.23&lt;/P&gt;</description>
      <pubDate>Thu, 06 Aug 2026 09:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i2c-problems-during-wakeup-frum-suspend/m-p/2402437#M246287</guid>
      <dc:creator>RRD101</dc:creator>
      <dc:date>2026-08-06T09:02:39Z</dc:date>
    </item>
  </channel>
</rss>