<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX8MP Heat Spreader Solution in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Heat-Spreader-Solution/m-p/2400912#M246229</link>
    <description>&lt;P class=""&gt;&lt;SPAN&gt;We are considering the following passive thermal solution for our i.MX 8M Plus–based infotainment application:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Aluminum heat spreader: 20 × 20 × 1.5 mm (up to 30 × 30 × 2 mm) &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;TIM: Henkel Bergquist Gap Filler TGF 2000&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;The aluminum plate will be used as a heat spreader on top of the i.MX 8M Plus.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Would this solution be sufficient for a typical infotainment workload? If not, could you recommend the appropriate heat-spreader size or any additional thermal requirements?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 31 Jul 2026 13:14:47 GMT</pubDate>
    <dc:creator>Wobaffet</dc:creator>
    <dc:date>2026-07-31T13:14:47Z</dc:date>
    <item>
      <title>i.MX8MP Heat Spreader Solution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Heat-Spreader-Solution/m-p/2400912#M246229</link>
      <description>&lt;P class=""&gt;&lt;SPAN&gt;We are considering the following passive thermal solution for our i.MX 8M Plus–based infotainment application:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Aluminum heat spreader: 20 × 20 × 1.5 mm (up to 30 × 30 × 2 mm) &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;TIM: Henkel Bergquist Gap Filler TGF 2000&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;The aluminum plate will be used as a heat spreader on top of the i.MX 8M Plus.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Would this solution be sufficient for a typical infotainment workload? If not, could you recommend the appropriate heat-spreader size or any additional thermal requirements?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 31 Jul 2026 13:14:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Heat-Spreader-Solution/m-p/2400912#M246229</guid>
      <dc:creator>Wobaffet</dc:creator>
      <dc:date>2026-07-31T13:14:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MP Heat Spreader Solution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Heat-Spreader-Solution/m-p/2400977#M246230</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206842"&gt;@Wobaffet&lt;/a&gt;,&lt;BR /&gt;Thank you for contacting NXP Support!&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;For this purpose, I recommend reviewing the &lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX8MPHDG" target="_self"&gt;i.MX8MP Hardware Design Guide,&lt;/A&gt; specifically Chapter 7.8, "Heat Sink Considerations", which provides detailed information and design recommendations for thermal management and heat sink implementation on the i.MX8MP.&lt;/P&gt;
&lt;P&gt;This chapter covers the key requirements and considerations needed to ensure proper thermal performance and reliable operation of the device.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Fri, 31 Jul 2026 17:31:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Heat-Spreader-Solution/m-p/2400977#M246230</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2026-07-31T17:31:35Z</dc:date>
    </item>
  </channel>
</rss>