<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Reducing Power Consumption by Disabling CPU/GPU/VPU on i.MX95 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Reducing-Power-Consumption-by-Disabling-CPU-GPU-VPU-on-i-MX95/m-p/2396955#M246059</link>
    <description>&lt;P class=""&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;We are looking for ways to reduce the overall power consumption of our i.MX95-based system.&lt;/P&gt;&lt;P&gt;Could you please help clarify the following questions?&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Is it possible to completely power down individual CPU cores when they are not required?&lt;/LI&gt;&lt;LI&gt;Is it possible to completely power down the GPU and VPU if our application does not use them?&lt;/LI&gt;&lt;LI&gt;If the CPU/ GPU / VPU is not required, is it possible to keep them disabled by default after boot to further reduce power consumption ?&amp;nbsp;(by device-tree ?)&lt;/LI&gt;&lt;LI&gt;Are there any recommended software configurations or reference documents for achieving the lowest possible power consumption?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Our BSP is based on Yocto 5.2 / Linux 6.12.x.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sean&lt;/P&gt;</description>
    <pubDate>Tue, 21 Jul 2026 01:33:09 GMT</pubDate>
    <dc:creator>SeanChuang</dc:creator>
    <dc:date>2026-07-21T01:33:09Z</dc:date>
    <item>
      <title>Reducing Power Consumption by Disabling CPU/GPU/VPU on i.MX95</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reducing-Power-Consumption-by-Disabling-CPU-GPU-VPU-on-i-MX95/m-p/2396955#M246059</link>
      <description>&lt;P class=""&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;We are looking for ways to reduce the overall power consumption of our i.MX95-based system.&lt;/P&gt;&lt;P&gt;Could you please help clarify the following questions?&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Is it possible to completely power down individual CPU cores when they are not required?&lt;/LI&gt;&lt;LI&gt;Is it possible to completely power down the GPU and VPU if our application does not use them?&lt;/LI&gt;&lt;LI&gt;If the CPU/ GPU / VPU is not required, is it possible to keep them disabled by default after boot to further reduce power consumption ?&amp;nbsp;(by device-tree ?)&lt;/LI&gt;&lt;LI&gt;Are there any recommended software configurations or reference documents for achieving the lowest possible power consumption?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Our BSP is based on Yocto 5.2 / Linux 6.12.x.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sean&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jul 2026 01:33:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reducing-Power-Consumption-by-Disabling-CPU-GPU-VPU-on-i-MX95/m-p/2396955#M246059</guid>
      <dc:creator>SeanChuang</dc:creator>
      <dc:date>2026-07-21T01:33:09Z</dc:date>
    </item>
    <item>
      <title>Re: Reducing Power Consumption by Disabling CPU/GPU/VPU on i.MX95</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reducing-Power-Consumption-by-Disabling-CPU-GPU-VPU-on-i-MX95/m-p/2398618#M246134</link>
      <description>&lt;P&gt;For your questions:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Is it possible to completely power down individual CPU cores when they are not required?&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;A:Yes, you can.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Is it possible to completely power down the GPU and VPU if our application does not use them?&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;A:Yes if not use them.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;If the CPU/ GPU / VPU is not required, is it possible to keep them disabled by default after boot to further reduce power consumption ?&amp;nbsp;(by device-tree ?)&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;A:Yes, For GPU/VPU-style platform devices, yes, the normal approach is to set the relevant device tree node status = "disabled"; so Linux does not register/probe that device.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Are there any recommended software configurations or reference documents for achieving the lowest possible power consumption?&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;A:We have the AN14449 — i.MX 95 Power Consumption Measurement : primary reference for measured low-power use cases, BCU procedure, DSM, Linux suspend, and BBSM.&lt;/P&gt;
&lt;P&gt;Any questions contact us freely&lt;/P&gt;
&lt;P&gt;Wish you have a nice day&lt;/P&gt;</description>
      <pubDate>Fri, 24 Jul 2026 08:18:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reducing-Power-Consumption-by-Disabling-CPU-GPU-VPU-on-i-MX95/m-p/2398618#M246134</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2026-07-24T08:18:12Z</dc:date>
    </item>
  </channel>
</rss>