<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Clarification Required: QSPI Flash Capacity Mismatch Between Datasheet and Actual Hardware</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Clarification-Required-QSPI-Flash-Capacity-Mismatch-Between/m-p/2396778#M246047</link>
    <description>&lt;P&gt;You are right, I will report it to related team, it is 256Mbit, that means 32MB.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 20 Jul 2026 12:02:01 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2026-07-20T12:02:01Z</dc:date>
    <item>
      <title>Clarification Required: QSPI Flash Capacity Mismatch Between Datasheet and Actual Hardware</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Clarification-Required-QSPI-Flash-Capacity-Mismatch-Between/m-p/2395278#M245995</link>
      <description>&lt;P&gt;Hello NXP Team,&lt;/P&gt;&lt;P&gt;I have purchased a board with the specified part number, and I noticed a discrepancy regarding the onboard QSPI flash capacity.&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="MCIMX6ULL-EVK" id="MCIMX6ULL-EVK"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The datasheet states that the board includes 256 MB QSPI flash. However, when I check the flash size from the operating system, it reports only 32 MB.&lt;/P&gt;&lt;P&gt;To verify this, I downloaded the design files and checked the BOM. I also looked up the same flash device part number on DigiKey and Mouser, and both list it as 256 Mbit flash memory, which corresponds to 32 MB, not 256 MB.&lt;/P&gt;&lt;P&gt;I purchased the board through the Element14 distributor.&lt;/P&gt;&lt;P&gt;Could you please clarify whether:&lt;/P&gt;&lt;P&gt;The datasheet contains a typo and should state 256 Mbit instead of 256 MB?&lt;BR /&gt;Or is there another explanation for why the datasheet and the actual hardware appear to use different storage classifications?&lt;/P&gt;&lt;P&gt;From my investigation, it appears that the installed flash device is 256 Mbit (32 MB) rather than 256 MB.&lt;/P&gt;&lt;P&gt;I would appreciate your confirmation.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jul 2026 09:03:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Clarification-Required-QSPI-Flash-Capacity-Mismatch-Between/m-p/2395278#M245995</guid>
      <dc:creator>AbhishekMakwana</dc:creator>
      <dc:date>2026-07-15T09:03:20Z</dc:date>
    </item>
    <item>
      <title>Re: Clarification Required: QSPI Flash Capacity Mismatch Between Datasheet and Actual Hardware</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Clarification-Required-QSPI-Flash-Capacity-Mismatch-Between/m-p/2396778#M246047</link>
      <description>&lt;P&gt;You are right, I will report it to related team, it is 256Mbit, that means 32MB.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jul 2026 12:02:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Clarification-Required-QSPI-Flash-Capacity-Mismatch-Between/m-p/2396778#M246047</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2026-07-20T12:02:01Z</dc:date>
    </item>
  </channel>
</rss>