<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: AP1302 MIPI CSI Streaming Issue on FRDM i.MX93</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/AP1302-MIPI-CSI-Streaming-Issue-on-FRDM-i-MX93/m-p/2394347#M245949</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;Please find my answers below for your reference.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1. Firmware Location&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I tried both the recommended firmware locations as well as each location individually. The camera probe is successful only when using &lt;STRONG&gt;ap1302_ar0144_single_fw.bin&lt;/STRONG&gt;.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx93evk:~# ls -la /lib/firmware/ap1302_ar0144_single_fw.bin
-rw-r--r-- 1 root root 80528 Aug  5 15:36 /lib/firmware/ap1302_ar0144_single_fw.bin

root@imx93evk:~# ls -la /lib/firmware/imx/camera/ap1302.fw
-rw-r--r-- 1 root root 80528 Aug  5 15:38 /lib/firmware/imx/camera/ap1302.fw&lt;/LI-CODE&gt;&lt;P&gt;The AP1302 is detected successfully during boot.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx93evk:~# dmesg | grep -i ap1302
...
[    9.962705] ap1302 2-003c: AP1302 revision 0.2.6 detected&lt;/LI-CODE&gt;&lt;P&gt;However, I do not see any firmware loading messages related to AP1302 in the kernel log.&lt;/P&gt;&lt;HR /&gt;&lt;P&gt;&lt;STRONG&gt;2. Software Environment&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am using the pre-built images provided for the &lt;STRONG&gt;FRDM i.MX93&lt;/STRONG&gt; board.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx93evk:~# cat /proc/device-tree/model
NXP FRDM-IMX93

root@imx93evk:~# cat /proc/cmdline
console=ttyLP0,115200 earlycon root=/dev/mmcblk0p2 rootwait rw&lt;/LI-CODE&gt;&lt;P&gt;The AP1302 is detected successfully, and the CSI/ISI devices are also present. I have attached the complete logs for your reference.&lt;/P&gt;&lt;HR /&gt;&lt;P&gt;&lt;STRONG&gt;3. Media Pipeline&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The media pipeline appears to be created correctly.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx93evk:~# ls /dev/media0
/dev/media0

root@imx93evk:~# ls /dev/video*
/dev/video0  /dev/video1&lt;/LI-CODE&gt;&lt;P&gt;The outputs from media-ctl show that the AP1302, CSI, and ISI entities are enabled. The complete media-ctl output is attached for your reference.&lt;/P&gt;&lt;HR /&gt;&lt;P&gt;&lt;STRONG&gt;4. Additional Information&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Please refer to the attached file &lt;STRONG&gt;fourth_point.txt&lt;/STRONG&gt; for the requested information.&lt;/P&gt;&lt;HR /&gt;&lt;P&gt;&lt;STRONG&gt;5. Streaming Failure&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I do not see any additional kernel messages when the streaming command fails.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx93evk:~# dmesg -c

root@imx93evk:~# v4l2-ctl -d /dev/video0 --stream-mmap=3 --stream-count=10
VIDIOC_STREAMON returned -1 (Broken pipe)

root@imx93evk:~# dmesg&lt;/LI-CODE&gt;&lt;P&gt;The dmesg output remains empty after the failure, so there are no additional kernel logs to help identify the root cause.&lt;/P&gt;&lt;P&gt;Since the AP1302 is detected successfully, the media graph is created correctly, and no kernel errors are reported during VIDIOC_STREAMON, could you please suggest what additional checks or debugging steps I should perform to identify why streaming fails with a &lt;STRONG&gt;"Broken pipe"&lt;/STRONG&gt; error?&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx93evk:~# v4l2-ctl --list-devices
mxc-isi-cap (platform:4ae40000.isi):
        /dev/video0
        /dev/video1
        /dev/media0

root@imx93evk:~# v4l2-ctl -d /dev/video0 --all
Driver Info:
        Driver name      : mxc-isi
        Card type        : mxc-isi-cap
        Bus info         : platform:4ae40000.isi
        Driver version   : 6.18.2
        Capabilities     : 0xa4201000
                Video Capture Multiplanar
                I/O MC
                Streaming
                Extended Pix Format
                Device Capabilities
        Device Caps      : 0x24201000
                Video Capture Multiplanar
                I/O MC
                Streaming
                Extended Pix Format
Media Driver Info:
        Driver name      : mxc-isi
        Model            : FSL Capture Media Device
        Serial           : 
        Bus info         : platform:4ae40000.isi
        Media version    : 6.18.2
        Hardware revision: 0x00000000 (0)
        Driver version   : 6.18.2
Interface Info:
        ID               : 0x0300000a
        Type             : V4L Video
Entity Info:
        ID               : 0x00000008 (8)
        Name             : mxc_isi.0.capture
        Function         : V4L2 I/O
        Pad 0x01000009   : 0: Sink
          Link 0x0200000c: from remote pad 0x1000007 of entity 'mxc_isi.0' (Video Pixel Formatter): Data, Enabled, Immutable
Priority: 2
Video input : 0 (mxc_isi.0.capture: ok)
Format Video Capture Multiplanar:
        Width/Height      : 1920/1080
        Pixel Format      : 'YUYV' (YUYV 4:2:2)
        Field             : None
        Number of planes  : 1
        Flags             : 
        Colorspace        : sRGB
        Transfer Function : sRGB
        YCbCr/HSV Encoding: ITU-R 601
        Quantization      : Limited Range
        Plane 0           :
           Bytes per Line : 3840
           Size Image     : 4147200

User Controls

                horizontal_flip 0x00980914 (bool)   : default=0 value=0 flags=0x00001000
                  vertical_flip 0x00980915 (bool)   : default=0 value=0 flags=0x00001000
                alpha_component 0x00980929 (int)    : min=0 max=255 step=1 default=0 value=0 flags=0x00001000
root@imx93evk:~# media-ctl -p
Media controller API version 6.18.2

Media device information
------------------------
driver          mxc-isi
model           FSL Capture Media Device
serial          
bus info        platform:4ae40000.isi
hw revision     0x0
driver version  6.18.2

Device topology
- entity 1: crossbar (3 pads, 3 links, 1 route)
            type V4L2 subdev subtype Unknown flags 0
            device node name /dev/v4l-subdev0
        routes:
                0/0 -&amp;gt; 2/0 [ACTIVE]
        pad0: SINK,MUST_CONNECT
                [stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
                &amp;lt;- "csidev-4ae00000.csi":1 [ENABLED,IMMUTABLE]
        pad1: SINK,MUST_CONNECT
                &amp;lt;- "mxc_isi.output":0 [ENABLED,IMMUTABLE]
        pad2: SOURCE
                [stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
                -&amp;gt; "mxc_isi.0":0 [ENABLED,IMMUTABLE]

- entity 5: mxc_isi.0 (2 pads, 2 links, 0 routes)
            type V4L2 subdev subtype Unknown flags 0
            device node name /dev/v4l-subdev1
        pad0: SINK
                [stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
                 compose.bounds:(0,0)/1920x1080
                 compose:(0,0)/1920x1080]
                &amp;lt;- "crossbar":2 [ENABLED,IMMUTABLE]
        pad1: SOURCE
                [stream:0 fmt:YUV8_1X24/1920x1080 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
                 crop.bounds:(0,0)/1920x1080
                 crop:(0,0)/1920x1080]
                -&amp;gt; "mxc_isi.0.capture":0 [ENABLED,IMMUTABLE]

- entity 8: mxc_isi.0.capture (1 pad, 1 link)
            type Node subtype V4L flags 0
            device node name /dev/video0
        pad0: SINK
                &amp;lt;- "mxc_isi.0":1 [ENABLED,IMMUTABLE]

- entity 16: mxc_isi.output (1 pad, 1 link)
             type Node subtype V4L flags 0
        pad0: SOURCE
                -&amp;gt; "crossbar":1 [ENABLED,IMMUTABLE]

- entity 23: csidev-4ae00000.csi (2 pads, 2 links, 1 route)
             type V4L2 subdev subtype Unknown flags 0
             device node name /dev/v4l-subdev2
        routes:
                0/0 -&amp;gt; 1/0 [ACTIVE]
        pad0: SINK
                [stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:smpte170m xfer:709 ycbcr:601 quantization:lim-range]
                &amp;lt;- "ap1302 2-003c":2 [ENABLED]
        pad1: SOURCE
                [stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:smpte170m xfer:709 ycbcr:601 quantization:lim-range]
                -&amp;gt; "crossbar":0 [ENABLED,IMMUTABLE]

- entity 28: ap1302 2-003c (3 pads, 2 links, 0 routes)
             type V4L2 subdev subtype Unknown flags 0
             device node name /dev/v4l-subdev4
        pad0: SINK
                [stream:0 fmt:SGRBG12_1X12/1280x800 field:none colorspace:srgb
                 crop.bounds:(0,0)/1280x800
                 crop:(0,0)/1280x800]
                &amp;lt;- "ar0144 0":0 [ENABLED,IMMUTABLE]
        pad1: SINK
                [stream:0 fmt:SGRBG12_1X12/1280x800 field:none colorspace:srgb
                 crop.bounds:(0,0)/1280x800
                 crop:(0,0)/1280x800]
        pad2: SOURCE
                [stream:0 fmt:UYYVYY8_0_5X24/4224x4092 field:none colorspace:srgb
                 crop.bounds:(0,0)/1280x800
                 crop:(0,0)/1280x800]
                -&amp;gt; "csidev-4ae00000.csi":0 [ENABLED]

- entity 32: ar0144 0 (1 pad, 1 link, 0 routes)
             type V4L2 subdev subtype Sensor flags 0
             device node name /dev/v4l-subdev3
        pad0: SOURCE
                [stream:0 fmt:SGRBG12_1X12/1280x800 field:none colorspace:srgb]
                -&amp;gt; "ap1302 2-003c":0 [ENABLED,IMMUTABLE]&lt;/LI-CODE&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Milav&lt;/P&gt;</description>
    <pubDate>Mon, 13 Jul 2026 10:09:39 GMT</pubDate>
    <dc:creator>milavsoni</dc:creator>
    <dc:date>2026-07-13T10:09:39Z</dc:date>
    <item>
      <title>AP1302 MIPI CSI Streaming Issue on FRDM i.MX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AP1302-MIPI-CSI-Streaming-Issue-on-FRDM-i-MX93/m-p/2394184#M245946</link>
      <description>&lt;P class=""&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I am using an &lt;/SPAN&gt;&lt;STRONG&gt;&lt;SPAN&gt;FRDM i.MX93&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN&gt; board with the &lt;/SPAN&gt;&lt;STRONG&gt;&lt;SPAN&gt;X-RPI-CAM-MIPI A1&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN&gt; camera module.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;The issue I am facing is that I am unable to capture the MIPI CSI stream from this setup.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I have placed the firmware binary &lt;/SPAN&gt;&lt;STRONG&gt;&lt;SPAN&gt;ap1302_60fps_ar0144_27M_2Lane_awb_tuning.bin&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN&gt; in the following location: "/lib/firmware"&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;During boot, I see that the AP1302 is detected successfully, but when I attempt to start video streaming, &lt;/SPAN&gt;&lt;STRONG&gt;&lt;SPAN&gt;VIDIOC_STREAMON&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN&gt; fails with a &lt;/SPAN&gt;&lt;STRONG&gt;&lt;SPAN&gt;"Broken pipe"&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN&gt; error.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Below are the relevant logs.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;STRONG&gt;&lt;SPAN&gt;Kernel log:&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx93evk:~# dmesg | grep ap1302
[    0.340980] /soc@0/bus@42000000/i2c@42530000/ap1302_mipi@3c: Fixed dependency cycle(s) with /soc@0/bus@42800000/csi@4ae00000
[    0.371014] /soc@0/bus@42800000/csi@4ae00000: Fixed dependency cycle(s) with /soc@0/bus@42000000/i2c@42530000/ap1302_mipi@3c
...
[   10.088832] ap1302 2-003c: AP1302 revision 0.2.6 detected&lt;/LI-CODE&gt;&lt;P class=""&gt;&lt;STRONG&gt;&lt;SPAN&gt;Streaming test:&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx93evk:~# v4l2-ctl -d /dev/video0 \
    --verbose \
    --stream-mmap=3 \
    --stream-count=10

VIDIOC_QUERYCAP: ok
VIDIOC_REQBUFS returned 0 (Success)
VIDIOC_CREATE_BUFS returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_G_FMT returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_STREAMON returned -1 (Broken pipe)&lt;/LI-CODE&gt;&lt;P class=""&gt;&lt;SPAN&gt;Could you please help me understand why &lt;/SPAN&gt;&lt;STRONG&gt;&lt;SPAN&gt;VIDIOC_STREAMON&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN&gt; is failing with a &lt;/SPAN&gt;&lt;STRONG&gt;&lt;SPAN&gt;"Broken pipe"&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN&gt; error?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Is there any additional configuration required for the AP1302 firmware, device tree, media pipeline, or sensor initialization before streaming can start successfully?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Furthermore, i am using "LF_v6.18.2-1.0.0_images_IMX93EVK" pre-built images for now.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Please let me know if you need any additional logs or information.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you for your support.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jul 2026 05:42:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AP1302-MIPI-CSI-Streaming-Issue-on-FRDM-i-MX93/m-p/2394184#M245946</guid>
      <dc:creator>milavsoni</dc:creator>
      <dc:date>2026-07-13T05:42:14Z</dc:date>
    </item>
    <item>
      <title>Re: AP1302 MIPI CSI Streaming Issue on FRDM i.MX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AP1302-MIPI-CSI-Streaming-Issue-on-FRDM-i-MX93/m-p/2394274#M245947</link>
      <description>&lt;P&gt;&lt;STRONG&gt;the AP1302 probe succeeding does not guarantee that the complete camera pipeline is configured and streaming.&lt;/STRONG&gt; On i.MX93, a VIDIOC_STREAMON returned -1 (Broken pipe) typically means that one of the media pipeline components (AP1302 → MIPI CSI-2 receiver → ISI capture path) failed to start or negotiate a valid stream. Your log only confirms that the AP1302 I²C device was detected:&lt;/P&gt;
&lt;P&gt;ap1302 2-003c: AP1302 revision 0.2.6 detected&lt;/P&gt;
&lt;P&gt;but it does &lt;STRONG&gt;not&lt;/STRONG&gt; confirm that:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;the firmware was loaded successfully,&lt;/LI&gt;
&lt;LI&gt;the correct DTB was used,&lt;/LI&gt;
&lt;LI&gt;the media graph was created,&lt;/LI&gt;
&lt;LI&gt;the CSI receiver is locked to incoming MIPI data,&lt;/LI&gt;
&lt;LI&gt;the AP1302 has been configured with a matching output format.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;STRONG&gt;First thing I would check: firmware location/name&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;For the FRDM-i.MX93 AP1302 support, NXP documentation indicates:&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;Download ap1302_60fps_ar0144_27M_2Lane_awb_tuning.bin&lt;/LI&gt;
&lt;LI&gt;Rename it to &lt;STRONG&gt;ap1302.fw&lt;/STRONG&gt;&lt;/LI&gt;
&lt;LI&gt;Place it in:&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;/lib/firmware/imx/camera/ap1302.fw&lt;/P&gt;
&lt;P&gt;not simply /lib/firmware.&lt;/P&gt;
&lt;P&gt;Please verify:&lt;/P&gt;
&lt;P&gt;ls -l /lib/firmware/imx/camera/ap1302.fw&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;and check boot log:&lt;/P&gt;
&lt;P&gt;dmesg | grep -i firmware&lt;/P&gt;
&lt;P&gt;dmesg | grep -i ap1302&lt;/P&gt;
&lt;P&gt;Look for messages such as:&lt;/P&gt;
&lt;P&gt;request firmware&lt;/P&gt;
&lt;P&gt;firmware loaded&lt;/P&gt;
&lt;P&gt;failed to load firmware&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Second check: are you using the correct DTB?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;The release notes indicate AP1302 support is associated with the i.MX93 EVK device tree support.&lt;/P&gt;
&lt;P&gt;Check:&lt;/P&gt;
&lt;P&gt;cat /proc/device-tree/model&lt;/P&gt;
&lt;P&gt;cat /proc/cmdline&lt;/P&gt;
&lt;P&gt;and determine the actual DTB being loaded.&lt;/P&gt;
&lt;P&gt;Also check:&lt;/P&gt;
&lt;P&gt;dmesg | grep -i ap1302&lt;/P&gt;
&lt;P&gt;dmesg | grep -i csi&lt;/P&gt;
&lt;P&gt;dmesg | grep -i isi&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Third check: verify media topology&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Before trying v4l2-ctl, verify that the media graph exists:&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Shell&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;media-ctl -p&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Show more lines&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;You should see entities similar to:&lt;/P&gt;
&lt;P&gt;ap1302&lt;/P&gt;
&lt;P&gt;csi&lt;/P&gt;
&lt;P&gt;isi&lt;/P&gt;
&lt;P&gt;videoX&lt;/P&gt;
&lt;P&gt;If /dev/media0 does not exist, the camera pipeline is not being created correctly. A very similar FRDM-i.MX93 AP1302 case showed:&lt;/P&gt;
&lt;P&gt;media-ctl -p&lt;/P&gt;
&lt;P&gt;Failed to enumerate /dev/media0&lt;/P&gt;
&lt;P&gt;which indicated the media pipeline was not instantiated.&lt;/P&gt;
&lt;P&gt;Please check:&lt;/P&gt;
&lt;P&gt;ls -l /dev/media*&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Fourth check: inspect the negotiated formats&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Run:&lt;/P&gt;
&lt;P&gt;v4l2-ctl --list-devices&lt;/P&gt;
&lt;P&gt;and&lt;/P&gt;
&lt;P&gt;v4l2-ctl -d /dev/video0 --all&lt;/P&gt;
&lt;P&gt;also:&lt;/P&gt;
&lt;P&gt;media-ctl -p&lt;/P&gt;
&lt;P&gt;The AP1302 firmware normally outputs processed YUV formats rather than RAW Bayer. Another common failure is:&lt;/P&gt;
&lt;P&gt;AP1302 outputs format A&lt;/P&gt;
&lt;P&gt;ISI configured for format B&lt;/P&gt;
&lt;P&gt;causing stream startup failure. A format mismatch often surfaces as STREAMON failure or CSI pipeline errors.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Fifth check: inspect CSI errors during STREAMON&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Open another terminal and monitor:&lt;/P&gt;
&lt;P&gt;dmesg -w&lt;/P&gt;
&lt;P&gt;then run:&lt;/P&gt;
&lt;P&gt;v4l2-ctl -d /dev/video0 \&lt;/P&gt;
&lt;P&gt;--stream-mmap=3 \&lt;/P&gt;
&lt;P&gt;--stream-count=10&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Look for messages such as:&lt;/P&gt;
&lt;P&gt;CSI timeout&lt;/P&gt;
&lt;P&gt;frame start timeout&lt;/P&gt;
&lt;P&gt;no data received&lt;/P&gt;
&lt;P&gt;FIFO overflow&lt;/P&gt;
&lt;P&gt;MIPI error&lt;/P&gt;
&lt;P&gt;link not enabled&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;These messages usually reveal the real reason behind the Broken pipe.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jul 2026 08:13:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AP1302-MIPI-CSI-Streaming-Issue-on-FRDM-i-MX93/m-p/2394274#M245947</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2026-07-13T08:13:38Z</dc:date>
    </item>
    <item>
      <title>Re: AP1302 MIPI CSI Streaming Issue on FRDM i.MX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AP1302-MIPI-CSI-Streaming-Issue-on-FRDM-i-MX93/m-p/2394347#M245949</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;Please find my answers below for your reference.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1. Firmware Location&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I tried both the recommended firmware locations as well as each location individually. The camera probe is successful only when using &lt;STRONG&gt;ap1302_ar0144_single_fw.bin&lt;/STRONG&gt;.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx93evk:~# ls -la /lib/firmware/ap1302_ar0144_single_fw.bin
-rw-r--r-- 1 root root 80528 Aug  5 15:36 /lib/firmware/ap1302_ar0144_single_fw.bin

root@imx93evk:~# ls -la /lib/firmware/imx/camera/ap1302.fw
-rw-r--r-- 1 root root 80528 Aug  5 15:38 /lib/firmware/imx/camera/ap1302.fw&lt;/LI-CODE&gt;&lt;P&gt;The AP1302 is detected successfully during boot.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx93evk:~# dmesg | grep -i ap1302
...
[    9.962705] ap1302 2-003c: AP1302 revision 0.2.6 detected&lt;/LI-CODE&gt;&lt;P&gt;However, I do not see any firmware loading messages related to AP1302 in the kernel log.&lt;/P&gt;&lt;HR /&gt;&lt;P&gt;&lt;STRONG&gt;2. Software Environment&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am using the pre-built images provided for the &lt;STRONG&gt;FRDM i.MX93&lt;/STRONG&gt; board.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx93evk:~# cat /proc/device-tree/model
NXP FRDM-IMX93

root@imx93evk:~# cat /proc/cmdline
console=ttyLP0,115200 earlycon root=/dev/mmcblk0p2 rootwait rw&lt;/LI-CODE&gt;&lt;P&gt;The AP1302 is detected successfully, and the CSI/ISI devices are also present. I have attached the complete logs for your reference.&lt;/P&gt;&lt;HR /&gt;&lt;P&gt;&lt;STRONG&gt;3. Media Pipeline&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The media pipeline appears to be created correctly.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx93evk:~# ls /dev/media0
/dev/media0

root@imx93evk:~# ls /dev/video*
/dev/video0  /dev/video1&lt;/LI-CODE&gt;&lt;P&gt;The outputs from media-ctl show that the AP1302, CSI, and ISI entities are enabled. The complete media-ctl output is attached for your reference.&lt;/P&gt;&lt;HR /&gt;&lt;P&gt;&lt;STRONG&gt;4. Additional Information&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Please refer to the attached file &lt;STRONG&gt;fourth_point.txt&lt;/STRONG&gt; for the requested information.&lt;/P&gt;&lt;HR /&gt;&lt;P&gt;&lt;STRONG&gt;5. Streaming Failure&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I do not see any additional kernel messages when the streaming command fails.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx93evk:~# dmesg -c

root@imx93evk:~# v4l2-ctl -d /dev/video0 --stream-mmap=3 --stream-count=10
VIDIOC_STREAMON returned -1 (Broken pipe)

root@imx93evk:~# dmesg&lt;/LI-CODE&gt;&lt;P&gt;The dmesg output remains empty after the failure, so there are no additional kernel logs to help identify the root cause.&lt;/P&gt;&lt;P&gt;Since the AP1302 is detected successfully, the media graph is created correctly, and no kernel errors are reported during VIDIOC_STREAMON, could you please suggest what additional checks or debugging steps I should perform to identify why streaming fails with a &lt;STRONG&gt;"Broken pipe"&lt;/STRONG&gt; error?&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx93evk:~# v4l2-ctl --list-devices
mxc-isi-cap (platform:4ae40000.isi):
        /dev/video0
        /dev/video1
        /dev/media0

root@imx93evk:~# v4l2-ctl -d /dev/video0 --all
Driver Info:
        Driver name      : mxc-isi
        Card type        : mxc-isi-cap
        Bus info         : platform:4ae40000.isi
        Driver version   : 6.18.2
        Capabilities     : 0xa4201000
                Video Capture Multiplanar
                I/O MC
                Streaming
                Extended Pix Format
                Device Capabilities
        Device Caps      : 0x24201000
                Video Capture Multiplanar
                I/O MC
                Streaming
                Extended Pix Format
Media Driver Info:
        Driver name      : mxc-isi
        Model            : FSL Capture Media Device
        Serial           : 
        Bus info         : platform:4ae40000.isi
        Media version    : 6.18.2
        Hardware revision: 0x00000000 (0)
        Driver version   : 6.18.2
Interface Info:
        ID               : 0x0300000a
        Type             : V4L Video
Entity Info:
        ID               : 0x00000008 (8)
        Name             : mxc_isi.0.capture
        Function         : V4L2 I/O
        Pad 0x01000009   : 0: Sink
          Link 0x0200000c: from remote pad 0x1000007 of entity 'mxc_isi.0' (Video Pixel Formatter): Data, Enabled, Immutable
Priority: 2
Video input : 0 (mxc_isi.0.capture: ok)
Format Video Capture Multiplanar:
        Width/Height      : 1920/1080
        Pixel Format      : 'YUYV' (YUYV 4:2:2)
        Field             : None
        Number of planes  : 1
        Flags             : 
        Colorspace        : sRGB
        Transfer Function : sRGB
        YCbCr/HSV Encoding: ITU-R 601
        Quantization      : Limited Range
        Plane 0           :
           Bytes per Line : 3840
           Size Image     : 4147200

User Controls

                horizontal_flip 0x00980914 (bool)   : default=0 value=0 flags=0x00001000
                  vertical_flip 0x00980915 (bool)   : default=0 value=0 flags=0x00001000
                alpha_component 0x00980929 (int)    : min=0 max=255 step=1 default=0 value=0 flags=0x00001000
root@imx93evk:~# media-ctl -p
Media controller API version 6.18.2

Media device information
------------------------
driver          mxc-isi
model           FSL Capture Media Device
serial          
bus info        platform:4ae40000.isi
hw revision     0x0
driver version  6.18.2

Device topology
- entity 1: crossbar (3 pads, 3 links, 1 route)
            type V4L2 subdev subtype Unknown flags 0
            device node name /dev/v4l-subdev0
        routes:
                0/0 -&amp;gt; 2/0 [ACTIVE]
        pad0: SINK,MUST_CONNECT
                [stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
                &amp;lt;- "csidev-4ae00000.csi":1 [ENABLED,IMMUTABLE]
        pad1: SINK,MUST_CONNECT
                &amp;lt;- "mxc_isi.output":0 [ENABLED,IMMUTABLE]
        pad2: SOURCE
                [stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
                -&amp;gt; "mxc_isi.0":0 [ENABLED,IMMUTABLE]

- entity 5: mxc_isi.0 (2 pads, 2 links, 0 routes)
            type V4L2 subdev subtype Unknown flags 0
            device node name /dev/v4l-subdev1
        pad0: SINK
                [stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
                 compose.bounds:(0,0)/1920x1080
                 compose:(0,0)/1920x1080]
                &amp;lt;- "crossbar":2 [ENABLED,IMMUTABLE]
        pad1: SOURCE
                [stream:0 fmt:YUV8_1X24/1920x1080 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
                 crop.bounds:(0,0)/1920x1080
                 crop:(0,0)/1920x1080]
                -&amp;gt; "mxc_isi.0.capture":0 [ENABLED,IMMUTABLE]

- entity 8: mxc_isi.0.capture (1 pad, 1 link)
            type Node subtype V4L flags 0
            device node name /dev/video0
        pad0: SINK
                &amp;lt;- "mxc_isi.0":1 [ENABLED,IMMUTABLE]

- entity 16: mxc_isi.output (1 pad, 1 link)
             type Node subtype V4L flags 0
        pad0: SOURCE
                -&amp;gt; "crossbar":1 [ENABLED,IMMUTABLE]

- entity 23: csidev-4ae00000.csi (2 pads, 2 links, 1 route)
             type V4L2 subdev subtype Unknown flags 0
             device node name /dev/v4l-subdev2
        routes:
                0/0 -&amp;gt; 1/0 [ACTIVE]
        pad0: SINK
                [stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:smpte170m xfer:709 ycbcr:601 quantization:lim-range]
                &amp;lt;- "ap1302 2-003c":2 [ENABLED]
        pad1: SOURCE
                [stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:smpte170m xfer:709 ycbcr:601 quantization:lim-range]
                -&amp;gt; "crossbar":0 [ENABLED,IMMUTABLE]

- entity 28: ap1302 2-003c (3 pads, 2 links, 0 routes)
             type V4L2 subdev subtype Unknown flags 0
             device node name /dev/v4l-subdev4
        pad0: SINK
                [stream:0 fmt:SGRBG12_1X12/1280x800 field:none colorspace:srgb
                 crop.bounds:(0,0)/1280x800
                 crop:(0,0)/1280x800]
                &amp;lt;- "ar0144 0":0 [ENABLED,IMMUTABLE]
        pad1: SINK
                [stream:0 fmt:SGRBG12_1X12/1280x800 field:none colorspace:srgb
                 crop.bounds:(0,0)/1280x800
                 crop:(0,0)/1280x800]
        pad2: SOURCE
                [stream:0 fmt:UYYVYY8_0_5X24/4224x4092 field:none colorspace:srgb
                 crop.bounds:(0,0)/1280x800
                 crop:(0,0)/1280x800]
                -&amp;gt; "csidev-4ae00000.csi":0 [ENABLED]

- entity 32: ar0144 0 (1 pad, 1 link, 0 routes)
             type V4L2 subdev subtype Sensor flags 0
             device node name /dev/v4l-subdev3
        pad0: SOURCE
                [stream:0 fmt:SGRBG12_1X12/1280x800 field:none colorspace:srgb]
                -&amp;gt; "ap1302 2-003c":0 [ENABLED,IMMUTABLE]&lt;/LI-CODE&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Milav&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jul 2026 10:09:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AP1302-MIPI-CSI-Streaming-Issue-on-FRDM-i-MX93/m-p/2394347#M245949</guid>
      <dc:creator>milavsoni</dc:creator>
      <dc:date>2026-07-13T10:09:39Z</dc:date>
    </item>
    <item>
      <title>Re: AP1302 MIPI CSI Streaming Issue on FRDM i.MX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AP1302-MIPI-CSI-Streaming-Issue-on-FRDM-i-MX93/m-p/2394672#M245964</link>
      <description>&lt;P&gt;Discussing with the AE team.&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jul 2026 06:35:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AP1302-MIPI-CSI-Streaming-Issue-on-FRDM-i-MX93/m-p/2394672#M245964</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2026-07-14T06:35:19Z</dc:date>
    </item>
    <item>
      <title>Re: AP1302 MIPI CSI Streaming Issue on FRDM i.MX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AP1302-MIPI-CSI-Streaming-Issue-on-FRDM-i-MX93/m-p/2395793#M246017</link>
      <description>&lt;P&gt;It's required to set up the pipeline using the following commands before capturing.&lt;/P&gt;
&lt;P&gt;$ media-ctl -l "'ap1302 2-003c':2 -&amp;gt; 'csidev-4ae00000.csi':0&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class="error"&gt;[1]&lt;/SPAN&gt;"&lt;BR /&gt;$ media-ctl -V "'ap1302 2-003c':0&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class="error"&gt;[fmt: UYVY8_1X16/1280x800 field:none]&lt;/SPAN&gt;"&lt;BR /&gt;$ media-ctl -V "'ap1302 2-003c':2&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class="error"&gt;[fmt: UYVY8_1X16/1280x800 field:none]&lt;/SPAN&gt;"&lt;BR /&gt;$ media-ctl -V "'ar0144 0':0&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class="error"&gt;[fmt: UYVY8_1X16/1280x800 field:none]&lt;/SPAN&gt;"&lt;BR /&gt;$ media-ctl -V "'csidev-4ae00000.csi':1&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class="error"&gt;[fmt: UYVY8_1X16/1280x800 field:none]&lt;/SPAN&gt;"&lt;BR /&gt;$ media-ctl -V "'crossbar':2&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class="error"&gt;[fmt: UYVY8_1X16/1280x800 field:none]&lt;/SPAN&gt;"&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jul 2026 07:58:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AP1302-MIPI-CSI-Streaming-Issue-on-FRDM-i-MX93/m-p/2395793#M246017</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2026-07-16T07:58:33Z</dc:date>
    </item>
  </channel>
</rss>