<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6Q U-BooT in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-U-BooT/m-p/2392214#M245911</link>
    <description>&lt;P&gt;Working bootloader version&lt;BR /&gt;U-Boot 2018.03 (Apr 22 2021 - 04:17:10 -0400)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6Q rev1.3 996 MHz (running at 792 MHz)&lt;BR /&gt;CPU: Automotive temperature grade (-40C to 125C) at 30C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: Freescale i.MX6 Quad SABER Smart Device Board&lt;BR /&gt;Board: MX6-SabreSD&lt;BR /&gt;Watchdog enabled&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x21&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... Card did not respond to voltage&lt;/P&gt;&lt;P&gt;My board is a reference board with SabreSD&lt;BR /&gt;I have all the schematics and data&lt;BR /&gt;I'm not good at this kind of task, but I'd like to update the firmware to try out the new features.&lt;/P&gt;</description>
    <pubDate>Wed, 08 Jul 2026 10:12:21 GMT</pubDate>
    <dc:creator>CAT5000</dc:creator>
    <dc:date>2026-07-08T10:12:21Z</dc:date>
    <item>
      <title>IMX6Q U-BooT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-U-BooT/m-p/2391497#M245891</link>
      <description>&lt;P&gt;Hi, I have a custom camera with an IMX6q processor.&lt;BR /&gt;I have working firmware on an old bootloader and an old kernel.&lt;BR /&gt;I need to update the bootloader and kernel.&lt;BR /&gt;But I can't get past the kernel loading stage.&lt;BR /&gt;The UART log is always empty.&lt;BR /&gt;Please help.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jul 2026 08:50:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-U-BooT/m-p/2391497#M245891</guid>
      <dc:creator>CAT5000</dc:creator>
      <dc:date>2026-07-07T08:50:39Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q U-BooT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-U-BooT/m-p/2391772#M245899</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/264456"&gt;@CAT5000&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing very well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please specify the current BSP version and the new one.&lt;/P&gt;
&lt;P&gt;Also, your Software changes related to the UART where is defined for Console.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jul 2026 17:01:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-U-BooT/m-p/2391772#M245899</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2026-07-07T17:01:20Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q U-BooT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-U-BooT/m-p/2392214#M245911</link>
      <description>&lt;P&gt;Working bootloader version&lt;BR /&gt;U-Boot 2018.03 (Apr 22 2021 - 04:17:10 -0400)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6Q rev1.3 996 MHz (running at 792 MHz)&lt;BR /&gt;CPU: Automotive temperature grade (-40C to 125C) at 30C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: Freescale i.MX6 Quad SABER Smart Device Board&lt;BR /&gt;Board: MX6-SabreSD&lt;BR /&gt;Watchdog enabled&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x21&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... Card did not respond to voltage&lt;/P&gt;&lt;P&gt;My board is a reference board with SabreSD&lt;BR /&gt;I have all the schematics and data&lt;BR /&gt;I'm not good at this kind of task, but I'd like to update the firmware to try out the new features.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Jul 2026 10:12:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-U-BooT/m-p/2392214#M245911</guid>
      <dc:creator>CAT5000</dc:creator>
      <dc:date>2026-07-08T10:12:21Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q U-BooT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-U-BooT/m-p/2392508#M245915</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Actually, we have a guide for porting our processors to the last BSP version.&lt;/P&gt;
&lt;P&gt;Please take a look to the&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/user-guide/UG10165.pdf" target="_self"&gt;UG10165&lt;/A&gt; (i.MX Porting Guide).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There are described the changes that you need to do in U-boot.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also, if you have the Sabre board, you can simply download the last version Pre-compiled image from&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_self"&gt;Embedded Linux for i.MX Applications Processors&lt;/A&gt; and flash to your board.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Jul 2026 18:19:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-U-BooT/m-p/2392508#M245915</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2026-07-08T18:19:37Z</dc:date>
    </item>
  </channel>
</rss>