<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックFRDM-IMX95: No Serial Output when Booting from SD Card (Pre-installed eMMC Boot Works Perfectly</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-IMX95-No-Serial-Output-when-Booting-from-SD-Card-Pre/m-p/2391680#M245894</link>
    <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I am mechanical and electrical engineering background, and this is my first time diving deep into complex System-on-Chips (SoCs) and embedded Operating Systems.&lt;/P&gt;&lt;P&gt;For my project, I am using the FRDM-IMX95 development board. My ultimate goal is to run two operating systems in parallel using an IPC (Inter-Process Communication) framework.&lt;/P&gt;&lt;P&gt;The board arrived with a pre-installed Linux image on the internal eMMC. This works flawlessly out of the box, and I get full serial output logs in my terminal monitor program.&lt;/P&gt;&lt;P&gt;Now, I am trying to follow the official &lt;I&gt;Getting Started Guide&lt;/I&gt; to flash the standard Linux BSP image onto a microSD card using UUU (Universal Update Utility) on a Windows host machine.&lt;/P&gt;&lt;P&gt;According to the Windows command prompt, the UUU flashing process completes with a "SUCCESS" status. I used the following standard command layout: &lt;EM&gt;".\uuu.exe -b sd_all imx-boot-imx95-15x15-lpddr4x-frdm-sd.bin-flash_all imx-image-full-imx95evk.wic"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;The Problem: After successful flashing, I turn off the board and configure the physical boot switches for SD Boot Mode by setting SW1 [1:2] to 11 (ON / ON). When I power the board back on, the serial monitor remains completely blank. There is absolutely no text output or hardware initialization visible.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;Do I have a fundamental misunderstanding of how the boot chain works here? According to the &lt;I&gt;i.MX Linux User's Guide&lt;/I&gt;, the .wic image contains all four essential pieces, including the bootloader image (U-Boot). Shouldn't I at least see the initial U-Boot SPL sequence appearing on my serial monitor, since the basic hardware configuration blocks should be read from the card?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any insights, common pitfalls for beginners on this specific FRDM variant, or hidden switch requirements would be highly appreciated!&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
    <pubDate>Tue, 07 Jul 2026 13:40:40 GMT</pubDate>
    <dc:creator>Magnus98</dc:creator>
    <dc:date>2026-07-07T13:40:40Z</dc:date>
    <item>
      <title>FRDM-IMX95: No Serial Output when Booting from SD Card (Pre-installed eMMC Boot Works Perfectly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-IMX95-No-Serial-Output-when-Booting-from-SD-Card-Pre/m-p/2391680#M245894</link>
      <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I am mechanical and electrical engineering background, and this is my first time diving deep into complex System-on-Chips (SoCs) and embedded Operating Systems.&lt;/P&gt;&lt;P&gt;For my project, I am using the FRDM-IMX95 development board. My ultimate goal is to run two operating systems in parallel using an IPC (Inter-Process Communication) framework.&lt;/P&gt;&lt;P&gt;The board arrived with a pre-installed Linux image on the internal eMMC. This works flawlessly out of the box, and I get full serial output logs in my terminal monitor program.&lt;/P&gt;&lt;P&gt;Now, I am trying to follow the official &lt;I&gt;Getting Started Guide&lt;/I&gt; to flash the standard Linux BSP image onto a microSD card using UUU (Universal Update Utility) on a Windows host machine.&lt;/P&gt;&lt;P&gt;According to the Windows command prompt, the UUU flashing process completes with a "SUCCESS" status. I used the following standard command layout: &lt;EM&gt;".\uuu.exe -b sd_all imx-boot-imx95-15x15-lpddr4x-frdm-sd.bin-flash_all imx-image-full-imx95evk.wic"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;The Problem: After successful flashing, I turn off the board and configure the physical boot switches for SD Boot Mode by setting SW1 [1:2] to 11 (ON / ON). When I power the board back on, the serial monitor remains completely blank. There is absolutely no text output or hardware initialization visible.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;Do I have a fundamental misunderstanding of how the boot chain works here? According to the &lt;I&gt;i.MX Linux User's Guide&lt;/I&gt;, the .wic image contains all four essential pieces, including the bootloader image (U-Boot). Shouldn't I at least see the initial U-Boot SPL sequence appearing on my serial monitor, since the basic hardware configuration blocks should be read from the card?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any insights, common pitfalls for beginners on this specific FRDM variant, or hidden switch requirements would be highly appreciated!&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jul 2026 13:40:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FRDM-IMX95-No-Serial-Output-when-Booting-from-SD-Card-Pre/m-p/2391680#M245894</guid>
      <dc:creator>Magnus98</dc:creator>
      <dc:date>2026-07-07T13:40:40Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-IMX95: No Serial Output when Booting from SD Card (Pre-installed eMMC Boot Works Perfectly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-IMX95-No-Serial-Output-when-Booting-from-SD-Card-Pre/m-p/2393417#M245933</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I'm testing on my side to share the exact steps for you, I will update soon.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 10 Jul 2026 05:18:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FRDM-IMX95-No-Serial-Output-when-Booting-from-SD-Card-Pre/m-p/2393417#M245933</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2026-07-10T05:18:20Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-IMX95: No Serial Output when Booting from SD Card (Pre-installed eMMC Boot Works Perfectly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-IMX95-No-Serial-Output-when-Booting-from-SD-Card-Pre/m-p/2395724#M246009</link>
      <description>&lt;P&gt;Thank you for looking into this and testing it on your end! I appreciate the help and look forward to your update.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jul 2026 06:25:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FRDM-IMX95-No-Serial-Output-when-Booting-from-SD-Card-Pre/m-p/2395724#M246009</guid>
      <dc:creator>Magnus98</dc:creator>
      <dc:date>2026-07-16T06:25:59Z</dc:date>
    </item>
  </channel>
</rss>