<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックTouch Input Configuration for Multiple Displays in AAOS 15 on i.MX8QM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Touch-Input-Configuration-for-Multiple-Displays-in-AAOS-15-on-i/m-p/2386438#M245770</link>
    <description>&lt;P&gt;Hi Team,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;I am using 10.1-inch HDMI LCD(E) touchscreen displays with the i.MX8QM board. I need guidance on how to properly connect these displays to the board and configure the touch input for each display. Specifically, I would like to understand which ports/interfaces on the board should be used to connect the touch input (USB). Additionally, I need help in correctly mapping each touch input to its corresponding display in the Android Automotive system.&lt;BR /&gt;&lt;BR /&gt;Thanks &amp;amp; Regards&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Thu, 25 Jun 2026 13:10:05 GMT</pubDate>
    <dc:creator>harshi03</dc:creator>
    <dc:date>2026-06-25T13:10:05Z</dc:date>
    <item>
      <title>Touch Input Configuration for Multiple Displays in AAOS 15 on i.MX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Touch-Input-Configuration-for-Multiple-Displays-in-AAOS-15-on-i/m-p/2386438#M245770</link>
      <description>&lt;P&gt;Hi Team,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;I am using 10.1-inch HDMI LCD(E) touchscreen displays with the i.MX8QM board. I need guidance on how to properly connect these displays to the board and configure the touch input for each display. Specifically, I would like to understand which ports/interfaces on the board should be used to connect the touch input (USB). Additionally, I need help in correctly mapping each touch input to its corresponding display in the Android Automotive system.&lt;BR /&gt;&lt;BR /&gt;Thanks &amp;amp; Regards&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 25 Jun 2026 13:10:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Touch-Input-Configuration-for-Multiple-Displays-in-AAOS-15-on-i/m-p/2386438#M245770</guid>
      <dc:creator>harshi03</dc:creator>
      <dc:date>2026-06-25T13:10:05Z</dc:date>
    </item>
    <item>
      <title>Re: Touch Input Configuration for Multiple Displays in AAOS 15 on i.MX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Touch-Input-Configuration-for-Multiple-Displays-in-AAOS-15-on-i/m-p/2386600#M245777</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;i.MX 8QuadMax, support up to 4 displays:&lt;/P&gt;
&lt;P&gt;Any combination of 2-4 displays of the following 4 displays: HDMI_TX, LVDS0_CH0, LVDS1_CH0, MIPI_DSI1.&lt;/P&gt;
&lt;P&gt;Any combination of 2-4 displays of the following 4 displays: LVDS0_CH0, LVDS1_CH0, MIPI_DSI0, MIPI_DSI1.&lt;/P&gt;
&lt;P&gt;Regarding the input configuration, I suggest you take a look in section&amp;nbsp;8.3.3.1 Binding the display port with the input port of&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/user-guide/UG10176.pdf" target="_self"&gt;Android Automotive User's Guide&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jun 2026 23:06:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Touch-Input-Configuration-for-Multiple-Displays-in-AAOS-15-on-i/m-p/2386600#M245777</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2026-06-25T23:06:53Z</dc:date>
    </item>
    <item>
      <title>Re: Touch Input Configuration for Multiple Displays in AAOS 15 on i.MX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Touch-Input-Configuration-for-Multiple-Displays-in-AAOS-15-on-i/m-p/2395734#M246011</link>
      <description>&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jul 2026 06:40:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Touch-Input-Configuration-for-Multiple-Displays-in-AAOS-15-on-i/m-p/2395734#M246011</guid>
      <dc:creator>harshi03</dc:creator>
      <dc:date>2026-07-16T06:40:47Z</dc:date>
    </item>
  </channel>
</rss>