<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: FRDM-MX95 AAOS 16</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX95-AAOS-16/m-p/2378346#M245564</link>
    <description>Hello Flyn,&lt;BR /&gt;&lt;BR /&gt;I am also looking for an Android image or source package compatible with the FRDM-i.MX95. Have you found anything suitable?</description>
    <pubDate>Mon, 08 Jun 2026 12:34:08 GMT</pubDate>
    <dc:creator>saajid</dc:creator>
    <dc:date>2026-06-08T12:34:08Z</dc:date>
    <item>
      <title>FRDM-MX95 AAOS 16</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX95-AAOS-16/m-p/2372071#M245382</link>
      <description>&lt;P&gt;Will Android AAOS 16 image from nxp install on the FRDM-MX95?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Secondarily, can an m.2 hard drive be installed in the slot?&lt;/P&gt;</description>
      <pubDate>Wed, 27 May 2026 23:34:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX95-AAOS-16/m-p/2372071#M245382</guid>
      <dc:creator>FlynHawaiian</dc:creator>
      <dc:date>2026-05-27T23:34:30Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-MX95 AAOS 16</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX95-AAOS-16/m-p/2372899#M245413</link>
      <description>&lt;P&gt;&lt;SPAN&gt;NXP documentation supports Android 16 and AAOS on i.MX 95 EVK/Verdin boards—not FRDM-IMX95， for the Android 16 BSP have the source code for the FRDM-95, but we have not rest it by now. A&lt;/SPAN&gt;&lt;SPAN&gt;nd the FRDM-IMX95 does include an M.2 Key-M slot intended for AI cards and SSDs.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 29 May 2026 08:03:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX95-AAOS-16/m-p/2372899#M245413</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2026-05-29T08:03:52Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-MX95 AAOS 16</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX95-AAOS-16/m-p/2373254#M245424</link>
      <description>&lt;P&gt;1) Is it possible I can build an android 16 image, as you say the source code for the frdm is there. &amp;nbsp;&lt;/P&gt;&lt;P&gt;2) Is there a particular reason that AAOS 16 couldn't be run on the FRDM-MX95? &amp;nbsp;Since the processor is a&amp;nbsp;MIMX9596XVTXNAC, it has full features and the only difference is the memory speed. &amp;nbsp;The MX95EVK uses the&amp;nbsp;MIMX9596AVZXNAC. &amp;nbsp;&lt;/P&gt;&lt;P&gt;Since both processors are full function processors I can't imagine there being a reason that AAOS nor Android shouldn't be able to be installed on the FRDM-mx95 board. &amp;nbsp;Could you shed some light on the reasoning?&lt;/P&gt;</description>
      <pubDate>Fri, 29 May 2026 22:05:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX95-AAOS-16/m-p/2373254#M245424</guid>
      <dc:creator>FlynHawaiian</dc:creator>
      <dc:date>2026-05-29T22:05:16Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-MX95 AAOS 16</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX95-AAOS-16/m-p/2378346#M245564</link>
      <description>Hello Flyn,&lt;BR /&gt;&lt;BR /&gt;I am also looking for an Android image or source package compatible with the FRDM-i.MX95. Have you found anything suitable?</description>
      <pubDate>Mon, 08 Jun 2026 12:34:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX95-AAOS-16/m-p/2378346#M245564</guid>
      <dc:creator>saajid</dc:creator>
      <dc:date>2026-06-08T12:34:08Z</dc:date>
    </item>
  </channel>
</rss>