<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX93 uuu libusb error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX93-uuu-libusb-error/m-p/2373245#M245423</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260022"&gt;@jamesfowkes&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;As I understand, you are using a custom board. Could you please confirm this?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Have you ported our software to match the hardware on your board by following our &lt;A href="https://www.nxp.com/docs/en/user-guide/UG10165.pdf" target="_self"&gt;porting guide&lt;/A&gt;?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Additionally, could you try using the latest version of the &lt;A href="https://github.com/nxp-imx/mfgtools/releases/tag/uuu_1.5.243" target="_self"&gt;UUU tool&lt;/A&gt;?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Have you completed DDR training and generated the corresponding timing files for your hardware?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Chavira&lt;/P&gt;</description>
    <pubDate>Fri, 29 May 2026 21:13:10 GMT</pubDate>
    <dc:creator>Chavira</dc:creator>
    <dc:date>2026-05-29T21:13:10Z</dc:date>
    <item>
      <title>IMX93 uuu libusb error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX93-uuu-libusb-error/m-p/2373101#M245420</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am having issues using &lt;FONT face="courier new,courier"&gt;uuu&lt;/FONT&gt; to flash an IMX93 (MIMX9352CVVXMAB).&lt;/P&gt;&lt;P&gt;I am using &lt;FONT face="courier new,courier"&gt;Ubuntu 24.04.4&lt;/FONT&gt; and uuu version:&lt;/P&gt;&lt;PRE&gt;&lt;FONT face="courier new,courier"&gt;uuu (Universal Update Utility) for nxp imx chips -- lib1.5.141&lt;/FONT&gt;&lt;/PRE&gt;&lt;P&gt;I can successfully flash the MCU on an IMX93EVK so I am confident that the laptop and software are not the issue.&lt;/P&gt;&lt;P&gt;The boot pins on the MCU are set to &lt;FONT face="courier new,courier"&gt;0001&lt;/FONT&gt; and the MCU is detected when powered.&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;dmesg&lt;/FONT&gt; output:&lt;/P&gt;&lt;PRE&gt;[15894.841580] usb 3-2: new high-speed USB device number 44 using xhci_hcd&lt;BR /&gt;[15894.966279] usb 3-2: New USB device found, idVendor=1fc9, idProduct=014e, bcdDevice= 0.01&lt;BR /&gt;[15894.966293] usb 3-2: New USB device strings: Mfr=1, Product=2, SerialNumber=0&lt;BR /&gt;[15894.966297] usb 3-2: Product: OO Blank 93&lt;BR /&gt;[15894.966300] usb 3-2: Manufacturer: NXP SemiConductor Inc &lt;BR /&gt;[15894.969654] hid-generic 0003:1FC9:014E.0011: hiddev0,hidraw4: USB HID v1.10 Device [NXP SemiConductor Inc OO Blank 93] on usb-0000:00:14.0-2/input0&lt;/PRE&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;uuu -lsusb&lt;/FONT&gt; output:&lt;/P&gt;&lt;PRE&gt;james@laptop:~$ uuu -lsusb&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- lib1.5.141&lt;BR /&gt;&lt;BR /&gt;Connected Known USB Devices&lt;BR /&gt;Path Chip Pro   Vid    Pid    BcdVersion&lt;BR /&gt;==================================================&lt;BR /&gt;3:2  MX93 SDPS: 0x1FC9 0x014E 0x0001&lt;/PRE&gt;&lt;P&gt;But when I try and flash the MCU:&lt;/P&gt;&lt;PRE&gt;james@laptop:~$ uuu -v -V -b emmc_all imx-boot-imx93-sd.bin-flash_singleboot image-dev-imx93.rootfs-20260521113620.wic.zst &lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- lib1.5.141&lt;BR /&gt;&lt;BR /&gt;Build in config:&lt;BR /&gt;Pctl Chip Vid Pid BcdVersion&lt;BR /&gt;==================================================&lt;BR /&gt;SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]&lt;BR /&gt;SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]&lt;BR /&gt;SDPS: MX8DXL 0x1fc9 0x0147&lt;BR /&gt;SDPS: MX28 0x15a2 0x004f&lt;BR /&gt;SDPS: MX815 0x1fc9 0x013e&lt;BR /&gt;SDPS: MX865 0x1fc9 0x0146&lt;BR /&gt;SDPS: MX8ULP 0x1fc9 0x014a&lt;BR /&gt;SDPS: MX8ULP 0x1fc9 0x014b&lt;BR /&gt;SDPS: MX93 0x1fc9 0x014e&lt;BR /&gt;SDPS: MX95 0x1fc9 0x015d&lt;BR /&gt;SDP: MX7D 0x15a2 0x0076&lt;BR /&gt;SDP: MX6Q 0x15a2 0x0054&lt;BR /&gt;SDP: MX6D 0x15a2 0x0061&lt;BR /&gt;SDP: MX6SL 0x15a2 0x0063&lt;BR /&gt;SDP: MX6SX 0x15a2 0x0071&lt;BR /&gt;SDP: MX6UL 0x15a2 0x007d&lt;BR /&gt;SDP: MX6ULL 0x15a2 0x0080&lt;BR /&gt;SDP: MX6SLL 0x1fc9 0x0128&lt;BR /&gt;SDP: MX7ULP 0x1fc9 0x0126&lt;BR /&gt;SDP: MXRT106X 0x1fc9 0x0135&lt;BR /&gt;SDP: MX8MM 0x1fc9 0x0134&lt;BR /&gt;SDP: MX8MQ 0x1fc9 0x012b&lt;BR /&gt;SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]&lt;BR /&gt;SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]&lt;BR /&gt;SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998]&lt;BR /&gt;SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]&lt;BR /&gt;SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]&lt;BR /&gt;SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]&lt;BR /&gt;FBK: 0x066f 0x9afe&lt;BR /&gt;FBK: 0x066f 0x9bff&lt;BR /&gt;FBK: 0x1fc9 0x0153&lt;BR /&gt;FB: 0x0525 0xa4a5&lt;BR /&gt;FB: 0x18d1 0x0d02&lt;BR /&gt;FB: 0x3016 0x0001&lt;BR /&gt;FB: 0x1fc9 0x0152&lt;BR /&gt;FB: 0x0483 0x0afb&lt;BR /&gt;&lt;BR /&gt;Run built-in script:&lt;BR /&gt;&lt;BR /&gt;uuu_version 1.4.149&lt;BR /&gt;&lt;BR /&gt;# @_flash.bin | bootloader, which can extract from wic image&lt;BR /&gt;# @_image [_flash.bin] | wic image burn to emmc.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ&lt;BR /&gt;SDP: boot -f imx-boot-imx93-sd.bin-flash_singleboot -scanlimited 0x800000&lt;BR /&gt;&lt;BR /&gt;# This command will be run when ROM support stream mode&lt;BR /&gt;# i.MX8QXP, i.MX8QM&lt;BR /&gt;SDPS: boot -scanterm -f imx-boot-imx93-sd.bin-flash_singleboot -scanlimited 0x800000&lt;BR /&gt;&lt;BR /&gt;# These commands will be run when use SPL and will be skipped if no spl&lt;BR /&gt;# SDPU will be deprecated. please use SDPV instead of SDPU&lt;BR /&gt;# {&lt;BR /&gt;SDPU: delay 1000&lt;BR /&gt;SDPU: write -f imx-boot-imx93-sd.bin-flash_singleboot -offset 0x57c00&lt;BR /&gt;SDPU: jump -scanlimited 0x800000&lt;BR /&gt;# }&lt;BR /&gt;&lt;BR /&gt;# These commands will be run when use SPL and will be skipped if no spl&lt;BR /&gt;# if (SPL support SDPV)&lt;BR /&gt;# {&lt;BR /&gt;SDPV: delay 1000&lt;BR /&gt;SDPV: write -f imx-boot-imx93-sd.bin-flash_singleboot -skipspl -scanterm -scanlimited 0x800000&lt;BR /&gt;SDPV: jump -scanlimited 0x800000&lt;BR /&gt;# }&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;FB: ucmd setenv fastboot_dev mmc&lt;BR /&gt;FB: ucmd setenv mmcdev ${emmc_dev}&lt;BR /&gt;FB: ucmd mmc dev ${emmc_dev}&lt;BR /&gt;FB: flash -raw2sparse all image-dev-imx93.rootfs-20260521113620.wic.zst/*&lt;BR /&gt;FB: flash -scanterm -scanlimited 0x800000 bootloader imx-boot-imx93-sd.bin-flash_singleboot&lt;BR /&gt;FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;&lt;BR /&gt;FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0&lt;BR /&gt;FB: done&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Wait for Known USB Device Appear...&lt;BR /&gt;New USB Device Attached at 3:2&lt;BR /&gt;3:2&amp;gt;Start Cmd:SDPS: boot -scanterm -f imx-boot-imx93-sd.bin-flash_singleboot -scanlimited 0x800000&lt;BR /&gt;3:2&amp;gt;Fail HID(W):LIBUSB_ERROR_IO(0.114s)&lt;/PRE&gt;&lt;P&gt;This error sometimes also appears as a &lt;FONT face="courier new,courier"&gt;LIBUSB_ERROR_TIMEOUT.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;I have read through all the existing threads I can find about libusb errors but none have helped me.&lt;/P&gt;&lt;P&gt;Any suggestions or advice are appreciated.&lt;/P&gt;</description>
      <pubDate>Fri, 29 May 2026 14:01:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX93-uuu-libusb-error/m-p/2373101#M245420</guid>
      <dc:creator>jamesfowkes</dc:creator>
      <dc:date>2026-05-29T14:01:10Z</dc:date>
    </item>
    <item>
      <title>Re: IMX93 uuu libusb error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX93-uuu-libusb-error/m-p/2373245#M245423</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260022"&gt;@jamesfowkes&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;As I understand, you are using a custom board. Could you please confirm this?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Have you ported our software to match the hardware on your board by following our &lt;A href="https://www.nxp.com/docs/en/user-guide/UG10165.pdf" target="_self"&gt;porting guide&lt;/A&gt;?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Additionally, could you try using the latest version of the &lt;A href="https://github.com/nxp-imx/mfgtools/releases/tag/uuu_1.5.243" target="_self"&gt;UUU tool&lt;/A&gt;?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Have you completed DDR training and generated the corresponding timing files for your hardware?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Fri, 29 May 2026 21:13:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX93-uuu-libusb-error/m-p/2373245#M245423</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2026-05-29T21:13:10Z</dc:date>
    </item>
    <item>
      <title>Re: IMX93 uuu libusb error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX93-uuu-libusb-error/m-p/2380139#M245629</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yes we are using a custom board.&lt;/P&gt;&lt;P&gt;I have used the latest version of `uuu`, there is no change in behaviour.&lt;/P&gt;&lt;P&gt;We can successfully boot images and run from an SD card so the issue is isolated specifically to the USB boot.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jun 2026 11:02:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX93-uuu-libusb-error/m-p/2380139#M245629</guid>
      <dc:creator>jamesfowkes</dc:creator>
      <dc:date>2026-06-11T11:02:58Z</dc:date>
    </item>
  </channel>
</rss>