<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Support for Ox03C10 Camera in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Support-for-Ox03C10-Camera/m-p/2370640#M245338</link>
    <description>&lt;P&gt;refer to the guide,&amp;nbsp;OX03C10 does have embedded data which in the top lines, for more detailed of this, you should refer to the camera data sheet&lt;/P&gt;
&lt;P&gt;for imx95,&amp;nbsp;HDR combining of 2 exposures, for the frame rate set, you can set in the libcamera or gstreamer user space level&lt;/P&gt;</description>
    <pubDate>Mon, 25 May 2026 06:42:58 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2026-05-25T06:42:58Z</dc:date>
    <item>
      <title>Support for Ox03C10 Camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Support-for-Ox03C10-Camera/m-p/2369143#M245302</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I am evaluating the ox03c10 camera with imx95-19*19-evk.&lt;BR /&gt;I have the 360 SVS setup with me. 4 mx95mbcam along with SerDes, but I am using only 1 camera from that setup.&lt;BR /&gt;EVK Setup Details:&amp;nbsp;Linux imx95-19x19-lpddr5-evk 6.12.20-lts-next-gdfaf2136deb2-dirty #1 SMP PREEMPT Wed May 13 05:19:25 UTC 2026 aarch64 GNU/Linux&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;As per my understanding, the existing sensor driver in the imx95 kernel src supports 3 exposure HDR(HDR4 Raw 16bit pwl with 1920*1280@30 fps).&lt;BR /&gt;I wanted to run it with dual exposure HDR(HDR3 Raw 16bit pwl with 1920*1280@60 fps).&lt;BR /&gt;&lt;BR /&gt;I have a few queries regarding the architecture and the flow:&lt;/P&gt;&lt;P&gt;1. Why are 2 lines of embedded sent along with the actual data? Is it required every time for all the diffrent configuration which I wanted to try?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Rathorepioneer_0-1779341714030.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/386306i66B7E120F0B51971/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Rathorepioneer_0-1779341714030.png" alt="Rathorepioneer_0-1779341714030.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Rathorepioneer_0-1779341714030.png&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;2. Can you provide the register configuration to change fps from 30 to 60? Does it also need any changes in SerDes?&lt;BR /&gt;3. What are the changes required to achieve HDR3?&lt;BR /&gt;4. Why does the existing sensor setup have flickering effects, idealy since HDR4 is running the default, it should be able to do LFM.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 21 May 2026 05:44:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Support-for-Ox03C10-Camera/m-p/2369143#M245302</guid>
      <dc:creator>Rathore-pioneer</dc:creator>
      <dc:date>2026-05-21T05:44:38Z</dc:date>
    </item>
    <item>
      <title>Re: Support for Ox03C10 Camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Support-for-Ox03C10-Camera/m-p/2370640#M245338</link>
      <description>&lt;P&gt;refer to the guide,&amp;nbsp;OX03C10 does have embedded data which in the top lines, for more detailed of this, you should refer to the camera data sheet&lt;/P&gt;
&lt;P&gt;for imx95,&amp;nbsp;HDR combining of 2 exposures, for the frame rate set, you can set in the libcamera or gstreamer user space level&lt;/P&gt;</description>
      <pubDate>Mon, 25 May 2026 06:42:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Support-for-Ox03C10-Camera/m-p/2370640#M245338</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2026-05-25T06:42:58Z</dc:date>
    </item>
    <item>
      <title>Re: Support for Ox03C10 Camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Support-for-Ox03C10-Camera/m-p/2371084#M245349</link>
      <description>Which guide needs to be referred to? I have a camera datasheet reference, but what is configured in the existing driver? Why am I getting too many flicker effects?&lt;BR /&gt;</description>
      <pubDate>Tue, 26 May 2026 06:45:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Support-for-Ox03C10-Camera/m-p/2371084#M245349</guid>
      <dc:creator>Rathore-pioneer</dc:creator>
      <dc:date>2026-05-26T06:45:53Z</dc:date>
    </item>
  </channel>
</rss>