<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: RT1062 SAI MCLK input as master</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RT1062-SAI-MCLK-input-as-master/m-p/2370370#M245325</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262883"&gt;@mojolabs&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I have provided an answer on the latest post you did here:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1062-SAI-MCLK-input-as-master/td-p/2369672#" target="_blank"&gt;RT1062 SAI MCLK input as master - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I will continue supporting you on that post if needed!&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
    <pubDate>Fri, 22 May 2026 21:27:18 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2026-05-22T21:27:18Z</dc:date>
    <item>
      <title>RT1062 SAI MCLK input as master</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1062-SAI-MCLK-input-as-master/m-p/2366982#M245267</link>
      <description>&lt;P&gt;I'm attempting to use SAI1 on the RT1062 as an I2S master for transmit while using MCLK as an input from external clock source on the 1060 EVKB.&amp;nbsp;I have SAI1 on the RT1062 working as an I2S master using MCLK generated from the internal PLL, and can see the MCLK output on pin 1 of J23, which is signal GPIO_AD_B1_09, as well as BCLK, etc on the same header.&lt;/P&gt;&lt;P&gt;I'm understanding from this thread:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/SAI1-MCLK1-source-select/m-p/1435023" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/SAI1-MCLK1-source-select/m-p/1435023&lt;/A&gt;&lt;/P&gt;&lt;P&gt;That I can use that same pin as MCLK input. I'm changing these register fields (p326-327 in RM):&lt;/P&gt;&lt;P&gt;- SAI1_MCLK1_SEL in IOMUXC_GPR_GPR1 - change from 000 to 011 to select MCLK pin&lt;/P&gt;&lt;P&gt;- SAI1_MCLK1_DIR in IOMUXC_GPR_GPR1 - change from 1 to 0 to select MCLK as an input&lt;/P&gt;&lt;P&gt;And,&amp;nbsp;IOMUXC_SW_MUX_CTL_PAD_GPIO_AD_B1_09 is set to 3 in both cases, selecting AD_B1_09 to the MCLK function.&lt;/P&gt;&lt;P&gt;When I do this, and provide an external clock signal to pin 1 on of J23, I do not see I2S output however - no BCLK generation, etc.&lt;/P&gt;&lt;P&gt;Is there another register change that needs to happen to select MCLK as an input for I2S master transmission?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 18 May 2026 14:56:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1062-SAI-MCLK-input-as-master/m-p/2366982#M245267</guid>
      <dc:creator>mojolabs</dc:creator>
      <dc:date>2026-05-18T14:56:53Z</dc:date>
    </item>
    <item>
      <title>Re: RT1062 SAI MCLK input as master</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1062-SAI-MCLK-input-as-master/m-p/2370370#M245325</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262883"&gt;@mojolabs&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I have provided an answer on the latest post you did here:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1062-SAI-MCLK-input-as-master/td-p/2369672#" target="_blank"&gt;RT1062 SAI MCLK input as master - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I will continue supporting you on that post if needed!&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Fri, 22 May 2026 21:27:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1062-SAI-MCLK-input-as-master/m-p/2370370#M245325</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2026-05-22T21:27:18Z</dc:date>
    </item>
  </channel>
</rss>