<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX8MP galcore_deamon Undefined instruction</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-galcore-deamon-Undefined-instruction/m-p/2365905#M245247</link>
    <description>The yocto version is scarthgap6.6.23. I did not make any modifications to the linux-imx_6.6.bb file, nor did I modify the galcore related drivers. I only modified the dts file of the kernel. So it should be the standard Linux kernel.Sometimes the error occurs in other functions, and dma_fence_signal is just one of them.&lt;BR /&gt;&lt;BR /&gt;## zcat /proc/config.gz | grep PREEMPT&lt;BR /&gt;CONFIG_PREEMPT_BUILD=y&lt;BR /&gt;# CONFIG_PREEMPT_NONE is not set&lt;BR /&gt;# CONFIG_PREEMPT_VOLUNTARY is not set&lt;BR /&gt;CONFIG_PREEMPT=y&lt;BR /&gt;CONFIG_PREEMPT_COUNT=y&lt;BR /&gt;CONFIG_PREEMPTION=y&lt;BR /&gt;# CONFIG_PREEMPT_DYNAMIC is not set&lt;BR /&gt;CONFIG_PREEMPT_RCU=y&lt;BR /&gt;CONFIG_HAVE_PREEMPT_DYNAMIC=y&lt;BR /&gt;CONFIG_HAVE_PREEMPT_DYNAMIC_KEY=y&lt;BR /&gt;CONFIG_PREEMPT_NOTIFIERS=y&lt;BR /&gt;# CONFIG_DEBUG_PREEMPT is not set</description>
    <pubDate>Fri, 15 May 2026 05:54:14 GMT</pubDate>
    <dc:creator>James33</dc:creator>
    <dc:date>2026-05-15T05:54:14Z</dc:date>
    <item>
      <title>IMX8MP galcore_deamon Undefined instruction</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-galcore-deamon-Undefined-instruction/m-p/2364422#M245213</link>
      <description>&lt;P&gt;Dear NXP Technical Support Team,&lt;/P&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;BOARD: IMX8MP&lt;BR /&gt;Yocto: scarthgap 6.6.23&lt;/P&gt;&lt;P&gt;On the i.MX8mp development board, I encountered this error.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;## imx8mp-lpddr4-evk kernel: Internal error: Oops - Undefined instruction: 0000000002000000 [#1] PREEMPT SMP 
## imx8mp-lpddr4-evk kernel: Modules linked in: fsl_jr_uio caam_jr caamkeyblob_desc caamhash_desc caamalg_desc crypto_engine authenc libdes crct10dif_ce polyval_ce polyval_generic snd_soc_fsl_asoc_card dw_hdmi_cec snd_soc_fsl_sai snd_soc_fsl_micfil snd_soc_fsl_xcvr imx8_media_dev(C) snd_soc_imx_audmux snd_soc_fsl_aud2htx snd_soc_fsl_easrc snd_soc_fsl_utils snd_soc_fsl_asrc imx_pcm_dma rtc_ds1307 snd_soc_wm8962 caam secvio error imx_dsp_rproc xt_conntrack nf_conntrack nf_defrag_ipv4 iptable_filter fuse 
## imx8mp-lpddr4-evk kernel: CPU: 3 PID: 79 Comm: galcore_deamon/ Tainted: G         C         6.6.23-lts-next-dirty #1 
## imx8mp-lpddr4-evk kernel: Hardware name: YTX FT Release Distro (DT) 
## imx8mp-lpddr4-evk kernel: pstate: 60000005 (nZCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--) 
## imx8mp-lpddr4-evk kernel: pc : dma_fence_signal+0x58/0x64
## imx8mp-lpddr4-evk kernel: lr : gckOS_Signal+0x180/0x244
## imx8mp-lpddr4-evk kernel: sp : ffff800082a6bd00
	
## imx8mp-lpddr4-evk kernel: x29: ffff800082a6bd10 x28: 0000000000000000 x27: ffff800082a6be10 
## imx8mp-lpddr4-evk kernel: x26: 0000000000000000 x25: ffff800081b3c008 x24: ffff000026b7f3c4 
## imx8mp-lpddr4-evk kernel: x23: ffff0000d1b6c1e0 x22: ffff0000d0d64044 x21: 0000000000000000 
## imx8mp-lpddr4-evk kernel: x20: ffff0000d0d64048 x19: ffff000026b7f3c0 x18: 0000000000000000 
## imx8mp-lpddr4-evk kernel: x17: 0000000000000000 x16: 0000000000000000 x15: 0000ffff8db25538 
## imx8mp-lpddr4-evk kernel: x14: 0000000000000000 x13: 0000000000000209 x12: 0000000000000002 
## imx8mp-lpddr4-evk kernel: x11: 0000000000000040 x10: ffff0000d0d64050 x9 : ffff0000d0d64048 
## imx8mp-lpddr4-evk kernel: x8 : ffff000006433b78 x7 : 0000000000000000 x6 : 000002a5fe056003 
## imx8mp-lpddr4-evk kernel: x5 : 00ffffffffffffff x4 : ffff0000d1b6c210 x3 : 0000000000000000 
## imx8mp-lpddr4-evk kernel: x2 : 0000000000000000 x1 : ffff0000d02b6740 x0 : 0000000000000000 
## imx8mp-lpddr4-evk kernel: Call trace: 
## imx8mp-lpddr4-evk kernel:  dma_fence_signal+0x58/0x64 
## imx8mp-lpddr4-evk kernel:  gckOS_UserSignal+0x7c/0xb0 
## imx8mp-lpddr4-evk kernel:  gckEVENT_Notify+0x21c/0x410 
## imx8mp-lpddr4-evk kernel:  gckHARDWARE_Notify+0x68/0xc8 
## imx8mp-lpddr4-evk kernel:  gckKERNEL_Notify+0x20/0x2c 
## imx8mp-lpddr4-evk kernel:  threadRoutine+0x1c/0x78 
## imx8mp-lpddr4-evk kernel:  kthread+0x110/0x114 
## imx8mp-lpddr4-evk kernel:  ret_from_fork+0x10/0x20 
## imx8mp-lpddr4-evk kernel: Code: 2a1303e0 a94153f3 a8c27bfd d50323bf (d65f03c0)  
## imx8mp-lpddr4-evk kernel: ---[ end trace 0000000000000000 ]---&lt;/LI-CODE&gt;&lt;P&gt;According to "dma_fence_signal+0x58/0x64", I checked the "dma_fence_signal" function and found that the instruction corresponding to the 0x58 position is the "ret" instruction.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;file path: imx8mp-xwayland/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source/drivers/dma-buf/dma-fence.c

int dma_fence_signal(struct dma_fence *fence)
{
	unsigned long flags;
	int ret;
	bool tmp;

	if (!fence)
		return -EINVAL;

	tmp = dma_fence_begin_signalling();

	spin_lock_irqsave(fence-&amp;gt;lock, flags);
	ret = dma_fence_signal_timestamp_locked(fence, ktime_get());
	spin_unlock_irqrestore(fence-&amp;gt;lock, flags);

	dma_fence_end_signalling(tmp);

	return ret;
}
EXPORT_SYMBOL(dma_fence_signal);&lt;/LI-CODE&gt;&lt;LI-CODE lang="markup"&gt;## aarch64-linux-gnu-objdump -r -d vmlinux | grep -A 30 \&amp;lt;dma_fence_signal\&amp;gt;:
ffff8000809bcfe8 &amp;lt;dma_fence_signal&amp;gt;:
ffff8000809bcfe8:	d503233f 	paciasp
ffff8000809bcfec:	a9be7bfd 	stp	x29, x30, [sp, #-32]!
ffff8000809bcff0:	910003fd 	mov	x29, sp
ffff8000809bcff4:	a90153f3 	stp	x19, x20, [sp, #16]
ffff8000809bcff8:	b4000260 	cbz	x0, ffff8000809bd044 &amp;lt;dma_fence_signal+0x5c&amp;gt;
ffff8000809bcffc:	aa0003f3 	mov	x19, x0
ffff8000809bd000:	f9400000 	ldr	x0, [x0]
ffff8000809bd004:	942b4fed 	bl	ffff800081490fb8 &amp;lt;_raw_spin_lock_irqsave&amp;gt;
ffff8000809bd008:	aa0003f4 	mov	x20, x0
ffff8000809bd00c:	97dd9d70 	bl	ffff8000801245cc &amp;lt;ktime_get&amp;gt;
ffff8000809bd010:	aa0003e1 	mov	x1, x0
ffff8000809bd014:	aa1303e0 	mov	x0, x19
ffff8000809bd018:	97ffff6e 	bl	ffff8000809bcdd0 &amp;lt;dma_fence_signal_timestamp_locked&amp;gt;
ffff8000809bd01c:	2a0003e2 	mov	w2, w0
ffff8000809bd020:	aa1403e1 	mov	x1, x20
ffff8000809bd024:	f9400260 	ldr	x0, [x19]
ffff8000809bd028:	2a0203f3 	mov	w19, w2
ffff8000809bd02c:	942b4eb5 	bl	ffff800081490b00 &amp;lt;_raw_spin_unlock_irqrestore&amp;gt;
ffff8000809bd030:	2a1303e0 	mov	w0, w19
ffff8000809bd034:	a94153f3 	ldp	x19, x20, [sp, #16]
ffff8000809bd038:	a8c27bfd 	ldp	x29, x30, [sp], #32
ffff8000809bd03c:	d50323bf 	autiasp
ffff8000809bd040:	d65f03c0 	ret
ffff8000809bd044:	128002b3 	mov	w19, #0xffffffea            	// #-22
ffff8000809bd048:	17fffffa 	b	ffff8000809bd030 &amp;lt;dma_fence_signal+0x48&amp;gt;&lt;/LI-CODE&gt;&lt;P&gt;I would like to know why the "ret" instruction is causing the problem? And what should I do to avoid this error?&amp;nbsp;This is an occasional occurrence. I don't yet know what kind of action caused this problem to happen. I am unable to manually reproduce this issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 May 2026 02:01:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-galcore-deamon-Undefined-instruction/m-p/2364422#M245213</guid>
      <dc:creator>James33</dc:creator>
      <dc:date>2026-05-13T02:01:03Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP galcore_deamon Undefined instruction</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-galcore-deamon-Undefined-instruction/m-p/2365848#M245243</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/255264"&gt;@James33&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Are you using the standard Linux kernel or PREEMPT Linux?&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Fri, 15 May 2026 02:51:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-galcore-deamon-Undefined-instruction/m-p/2365848#M245243</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2026-05-15T02:51:29Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP galcore_deamon Undefined instruction</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-galcore-deamon-Undefined-instruction/m-p/2365905#M245247</link>
      <description>The yocto version is scarthgap6.6.23. I did not make any modifications to the linux-imx_6.6.bb file, nor did I modify the galcore related drivers. I only modified the dts file of the kernel. So it should be the standard Linux kernel.Sometimes the error occurs in other functions, and dma_fence_signal is just one of them.&lt;BR /&gt;&lt;BR /&gt;## zcat /proc/config.gz | grep PREEMPT&lt;BR /&gt;CONFIG_PREEMPT_BUILD=y&lt;BR /&gt;# CONFIG_PREEMPT_NONE is not set&lt;BR /&gt;# CONFIG_PREEMPT_VOLUNTARY is not set&lt;BR /&gt;CONFIG_PREEMPT=y&lt;BR /&gt;CONFIG_PREEMPT_COUNT=y&lt;BR /&gt;CONFIG_PREEMPTION=y&lt;BR /&gt;# CONFIG_PREEMPT_DYNAMIC is not set&lt;BR /&gt;CONFIG_PREEMPT_RCU=y&lt;BR /&gt;CONFIG_HAVE_PREEMPT_DYNAMIC=y&lt;BR /&gt;CONFIG_HAVE_PREEMPT_DYNAMIC_KEY=y&lt;BR /&gt;CONFIG_PREEMPT_NOTIFIERS=y&lt;BR /&gt;# CONFIG_DEBUG_PREEMPT is not set</description>
      <pubDate>Fri, 15 May 2026 05:54:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-galcore-deamon-Undefined-instruction/m-p/2365905#M245247</guid>
      <dc:creator>James33</dc:creator>
      <dc:date>2026-05-15T05:54:14Z</dc:date>
    </item>
  </channel>
</rss>