<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: linux-imx: include/uapi/linux/ipu.h redefines standard integer types in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/linux-imx-include-uapi-linux-ipu-h-redefines-standard-integer/m-p/2362321#M245143</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247585"&gt;@ernest_tdx&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;We have a similar patch in our lf-6.18 branch scheduled for Q2 2026 Release. Can you please test it and see if it fixes your issue?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 08 May 2026 07:13:17 GMT</pubDate>
    <dc:creator>dbaluta</dc:creator>
    <dc:date>2026-05-08T07:13:17Z</dc:date>
    <item>
      <title>linux-imx: include/uapi/linux/ipu.h redefines standard integer types</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/linux-imx-include-uapi-linux-ipu-h-redefines-standard-integer/m-p/2359396#M245072</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using the Toradex BSP master branch to build for the Verdin iMX8MM. This BSP uses the meta-freescale layer to support the NXP SoCs. There, things are being updated to follow NXP BSP 6.18.2.&amp;nbsp; In particular, imx-gst1.0-plugin is now at version "MM_04.10.03_2512_L6.18.2", and linux-imx and linux-imx-headers are now at lf-6.18.y.&lt;/P&gt;&lt;P&gt;When building&amp;nbsp;imx-gst1.0-plugin with Yocto/OE for the verdin-imx8mm, I noticed the following build error:&lt;BR /&gt;MACHINE=verdin-imx8mm bitbake imx-gst1.0-plugin:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;  | In file included from ../sources/imx-gst1.0-plugin-4.10.3+git/libs/v4l2_core/gstimxv4l2.c:29:
  | /workdir/oe/tmp/work/armv8a-mx8mm-tdx-linux/imx-gst1.0-plugin/4.10.3+git/recipe-sysroot/usr/include/imx/linux/ipu.h:42:17: error: two or more data types in declaration specifiers
  |    42 | #define uint8_t unsigned char
  |       |                 ^~~~~~~~
  | /workdir/oe/tmp/work/armv8a-mx8mm-tdx-linux/imx-gst1.0-plugin/4.10.3+git/recipe-sysroot/usr/include/imx/linux/ipu.h:42:26: error: two or more data types in declaration specifiers
  |    42 | #define uint8_t unsigned char
  |       |                          ^~~~
  | /workdir/oe/tmp/work/armv8a-mx8mm-tdx-linux/imx-gst1.0-plugin/4.10.3+git/recipe-sysroot/usr/include/imx/linux/ipu.h:41:18: error: two or more data types in declaration specifiers
  |    41 | #define uint16_t unsigned short
  |       |                  ^~~~~~~~
  | /workdir/oe/tmp/work/armv8a-mx8mm-tdx-linux/imx-gst1.0-plugin/4.10.3+git/recipe-sysroot/usr/include/imx/linux/ipu.h:41:27: error: two or more data types in declaration specifiers
  |    41 | #define uint16_t unsigned short
  |       |                           ^~~~~
  | /workdir/oe/tmp/work/armv8a-mx8mm-tdx-linux/imx-gst1.0-plugin/4.10.3+git/recipe-sysroot/usr/include/imx/linux/ipu.h:40:18: error: two or more data types in declaration specifiers
  |    40 | #define uint32_t unsigned int
  |       |                  ^~~~~~~~
  | /workdir/oe/tmp/work/armv8a-mx8mm-tdx-linux/imx-gst1.0-plugin/4.10.3+git/recipe-sysroot/usr/include/imx/linux/ipu.h:40:27: error: two or more data types in declaration specifiers
  |    40 | #define uint32_t unsigned int
  |       |                           ^~~

[...]

  | ninja: build stopped: subcommand failed.
  | INFO: autodetecting backend as ninja
  | INFO: calculating backend command to run: /workdir/oe/tmp/work/armv8a-mx8mm-tdx-linux/imx-gst1.0-plugin/4.10.3+git/recipe-sysroot-native/usr/bin/ninja -j 64 -v
  | WARNING: exit code 1 from a shell command.
  NOTE: recipe imx-gst1.0-plugin-4.10.3+git-r0: task do_compile: Failed
  ERROR: Task (/workdir/oe/build/../layers/meta-freescale/recipes-multimedia/gstreamer/imx-gst1.0-plugin_git.bb:do_compile) failed with exit code '1'
  NOTE: recipe gstreamer1.0-plugins-bad-1.26.6.imx-r0: task do_package: Succeeded
  NOTE: Tasks Summary: Attempted 10003 tasks of which 8796 didn't need to be rerun and 1 failed.
  NOTE: Writing buildhistory
  NOTE: Writing buildhistory took: 6 seconds
  
  Summary: 1 task failed:
    /workdir/oe/build/../layers/meta-freescale/recipes-multimedia/gstreamer/imx-gst1.0-plugin_git.bb:do_compile
      log: /workdir/oe/tmp/work/armv8a-mx8mm-tdx-linux/imx-gst1.0-plugin/4.10.3+git/temp/log.do_compile.827805
  Summary: There was 1 WARNING message.
  Summary: There was 1 ERROR message, returning a non-zero exit code.&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;This happens because "include/imx/linux/ipu.h" is redefining types that are already set as a typedef in "linux/types.h", which is included by ipu.h. It is probably pure chance that this error was not triggered by a userspace program consuming this header before, due to a different include order.&lt;BR /&gt;&lt;BR /&gt;The solution seems relatively straightforward to me: remove the macro defines of uint*_t, which already exist anyways. My assumption is these just remained from some historical growth but there should be no reason for them in a Linux context.&lt;BR /&gt;&lt;BR /&gt;I've attached a patch with what I believe is a decent solution, on top of lf-6.18.y, which fixes my build problems. Any feedback or the integration of this patch would certainly be appreciated.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Ernest - Toradex&lt;/P&gt;</description>
      <pubDate>Thu, 30 Apr 2026 15:30:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/linux-imx-include-uapi-linux-ipu-h-redefines-standard-integer/m-p/2359396#M245072</guid>
      <dc:creator>ernest_tdx</dc:creator>
      <dc:date>2026-04-30T15:30:54Z</dc:date>
    </item>
    <item>
      <title>Re: linux-imx: include/uapi/linux/ipu.h redefines standard integer types</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/linux-imx-include-uapi-linux-ipu-h-redefines-standard-integer/m-p/2362321#M245143</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247585"&gt;@ernest_tdx&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;We have a similar patch in our lf-6.18 branch scheduled for Q2 2026 Release. Can you please test it and see if it fixes your issue?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 08 May 2026 07:13:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/linux-imx-include-uapi-linux-ipu-h-redefines-standard-integer/m-p/2362321#M245143</guid>
      <dc:creator>dbaluta</dc:creator>
      <dc:date>2026-05-08T07:13:17Z</dc:date>
    </item>
    <item>
      <title>Re: linux-imx: include/uapi/linux/ipu.h redefines standard integer types</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/linux-imx-include-uapi-linux-ipu-h-redefines-standard-integer/m-p/2362388#M245146</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/161047"&gt;@dbaluta&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;The patch you attached seems reasonable as well, I double checked and can confirm this patch also solves the issues.&lt;/P&gt;&lt;P&gt;I really appreciate NXP taking a look at the patches submitted here. If we can ever get a way to find such patches before a major release, that would of course be very helpful for us in backporting them &lt;LI-EMOJI id="lia_winking-face" title=":winking_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;Thanks and kind regards,&lt;/P&gt;&lt;P&gt;Ernest&lt;/P&gt;</description>
      <pubDate>Fri, 08 May 2026 08:59:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/linux-imx-include-uapi-linux-ipu-h-redefines-standard-integer/m-p/2362388#M245146</guid>
      <dc:creator>ernest_tdx</dc:creator>
      <dc:date>2026-05-08T08:59:46Z</dc:date>
    </item>
  </channel>
</rss>