<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx35_sdio_timeout</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx35-sdio-timeout/m-p/256176#M24514</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using imx35 board and wince 6 on that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;inserted sdio card and started to download one file from internet (around 100mb).while downloding the sdio driver gets timeout and not responding.Then only one way is rebooting the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the log file of sdio debugging is&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Call NdisMQueryInformationComplete With FAILURE&lt;/P&gt;&lt;P&gt;GetCmdFromQueueToExecute()&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; command timeout (0x1f) ********&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;:HCR_HOST_INT_STATUS_REGISTER (0x0)*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HCR_HOST_INT_MASK_REGISTER (0x3)*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;UPLOAD_HOST_INT_STATUS_RDY (0x1)*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[TT] INT NO upload status (int:0x0, mask:0x3)&lt;/P&gt;&lt;P&gt;MISC - Command TIME OUT !!&lt;/P&gt;&lt;P&gt;Call NdisMQueryInformationComplete With FAILURE&lt;/P&gt;&lt;P&gt;GetCmdFromQueueToExecute()&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;command timeout (0x6) ********&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HCR_HOST_INT_STATUS_REGISTER (0x0)*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HCR_HOST_INT_MASK_REGISTER (0x3)*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;UPLOAD_HOST_INT_STATUS_RDY (0x1)*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[TT] INT NO upload status (int:0x0, mask:0x3)&lt;/P&gt;&lt;P&gt;MISC - Command TIME OUT !!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what will be the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Apr 2013 11:59:21 GMT</pubDate>
    <dc:creator>nancy</dc:creator>
    <dc:date>2013-04-08T11:59:21Z</dc:date>
    <item>
      <title>imx35_sdio_timeout</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx35-sdio-timeout/m-p/256176#M24514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using imx35 board and wince 6 on that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;inserted sdio card and started to download one file from internet (around 100mb).while downloding the sdio driver gets timeout and not responding.Then only one way is rebooting the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the log file of sdio debugging is&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Call NdisMQueryInformationComplete With FAILURE&lt;/P&gt;&lt;P&gt;GetCmdFromQueueToExecute()&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; command timeout (0x1f) ********&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;:HCR_HOST_INT_STATUS_REGISTER (0x0)*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HCR_HOST_INT_MASK_REGISTER (0x3)*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;UPLOAD_HOST_INT_STATUS_RDY (0x1)*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[TT] INT NO upload status (int:0x0, mask:0x3)&lt;/P&gt;&lt;P&gt;MISC - Command TIME OUT !!&lt;/P&gt;&lt;P&gt;Call NdisMQueryInformationComplete With FAILURE&lt;/P&gt;&lt;P&gt;GetCmdFromQueueToExecute()&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;command timeout (0x6) ********&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HCR_HOST_INT_STATUS_REGISTER (0x0)*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HCR_HOST_INT_MASK_REGISTER (0x3)*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;UPLOAD_HOST_INT_STATUS_RDY (0x1)*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[TT] INT NO upload status (int:0x0, mask:0x3)&lt;/P&gt;&lt;P&gt;MISC - Command TIME OUT !!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what will be the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2013 11:59:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx35-sdio-timeout/m-p/256176#M24514</guid>
      <dc:creator>nancy</dc:creator>
      <dc:date>2013-04-08T11:59:21Z</dc:date>
    </item>
    <item>
      <title>Re: imx35_sdio_timeout</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx35-sdio-timeout/m-p/256177#M24515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Deactivated user can you help on this case?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Apr 2013 16:40:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx35-sdio-timeout/m-p/256177#M24515</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2013-04-19T16:40:05Z</dc:date>
    </item>
  </channel>
</rss>