<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.mx8M Plus Pin function of B11</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8M-Plus-Pin-function-of-B11/m-p/2358606#M245054</link>
    <description>&lt;P&gt;Hello NXP Team,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We are designing a Hardware platform using the&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;MIMX8ML6NKZACVB&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;Processor.&amp;nbsp;We require a USB ID pin function for the Host and Slave control of USB devices. There is no separate pin in the SOC pinout.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In EVK Schematics, it is mentioned that pin B11 should not be considered for the USB ID function&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Melshia_0-1777456557078.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/383992iFE0F99DDBF1D3CC3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Melshia_0-1777456557078.png" alt="Melshia_0-1777456557078.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But in the Config tool of i.mx8M plus (&lt;STRONG&gt;MIMX8ML6NKZACVB), this B11 pin is configured as a USB ID function.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Melshia_0-1777466433833.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/384004i03A17E240ADE76F7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Melshia_0-1777466433833.png" alt="Melshia_0-1777466433833.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Could you please confirm which I need to consider for this B11 pin function?&lt;/P&gt;</description>
    <pubDate>Wed, 29 Apr 2026 12:41:55 GMT</pubDate>
    <dc:creator>Melshia</dc:creator>
    <dc:date>2026-04-29T12:41:55Z</dc:date>
    <item>
      <title>i.mx8M Plus Pin function of B11</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8M-Plus-Pin-function-of-B11/m-p/2358606#M245054</link>
      <description>&lt;P&gt;Hello NXP Team,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We are designing a Hardware platform using the&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;MIMX8ML6NKZACVB&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;Processor.&amp;nbsp;We require a USB ID pin function for the Host and Slave control of USB devices. There is no separate pin in the SOC pinout.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In EVK Schematics, it is mentioned that pin B11 should not be considered for the USB ID function&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Melshia_0-1777456557078.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/383992iFE0F99DDBF1D3CC3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Melshia_0-1777456557078.png" alt="Melshia_0-1777456557078.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But in the Config tool of i.mx8M plus (&lt;STRONG&gt;MIMX8ML6NKZACVB), this B11 pin is configured as a USB ID function.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Melshia_0-1777466433833.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/384004i03A17E240ADE76F7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Melshia_0-1777466433833.png" alt="Melshia_0-1777466433833.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Could you please confirm which I need to consider for this B11 pin function?&lt;/P&gt;</description>
      <pubDate>Wed, 29 Apr 2026 12:41:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx8M-Plus-Pin-function-of-B11/m-p/2358606#M245054</guid>
      <dc:creator>Melshia</dc:creator>
      <dc:date>2026-04-29T12:41:55Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx8M Plus Pin function of B11</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8M-Plus-Pin-function-of-B11/m-p/2360835#M245112</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;USB1_DNU should be left floating since it doesn't work as USB1_ID.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;To use this function, a GPIO pin should be used and configured. If USB_DNU signal is connected as USB1_ID will not work.&lt;/P&gt;
&lt;P&gt;Please follow the recommendation of the Note.&lt;/P&gt;</description>
      <pubDate>Wed, 06 May 2026 05:11:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx8M-Plus-Pin-function-of-B11/m-p/2360835#M245112</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2026-05-06T05:11:37Z</dc:date>
    </item>
  </channel>
</rss>