<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RTSP Camera Streaming Failure for 2K/Above Full HD Resolution on NXP i.MX8M Plus FRDM (4GB RAM) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RTSP-Camera-Streaming-Failure-for-2K-Above-Full-HD-Resolution-on/m-p/2353565#M244935</link>
    <description>&lt;P&gt;&lt;FONT color="#000000"&gt;The RTSP camera streaming pipeline using GStreamer on the&lt;STRONG&gt; i.MX8M Plus FRDM board (4GB RAM) &lt;/STRONG&gt;fails when processing high-resolution video streams (2K or above Full HD).&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;The system successfully initializes the pipeline and establishes an RTSP connection. However, during playback, the pipeline terminates with the following errors:&lt;/FONT&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;Internal data stream error&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;streaming stopped, reason not-negotiated (-4)&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;Could not write to resource (Received end-of-file)&lt;/FONT&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;This issue is observed specifically with high-resolution (≥2K) H.265 streams, indicating that the platform is unable to negotiate or sustain the required decoding pipeline.&lt;/FONT&gt;&lt;/P&gt;&lt;H3&gt;&lt;FONT color="#000000"&gt;Key Observations:&lt;/FONT&gt;&lt;/H3&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;GStreamer pipeline works for lower resolutions (e.g., 1080p)&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;Failure occurs during caps negotiation or decoder stage&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;Hardware decoder (v4l2h265dec) likely hitting limitations&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;System is running:&lt;/FONT&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;Linux Kernel: 6.6.x (scarthgap)&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;Yocto-based NXP BSP&lt;/FONT&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;Board configuration: i.MX8M Plus FRDM with 4GB RAM&lt;/FONT&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
    <pubDate>Mon, 20 Apr 2026 08:16:18 GMT</pubDate>
    <dc:creator>Kaustubhnaik45</dc:creator>
    <dc:date>2026-04-20T08:16:18Z</dc:date>
    <item>
      <title>RTSP Camera Streaming Failure for 2K/Above Full HD Resolution on NXP i.MX8M Plus FRDM (4GB RAM)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTSP-Camera-Streaming-Failure-for-2K-Above-Full-HD-Resolution-on/m-p/2353565#M244935</link>
      <description>&lt;P&gt;&lt;FONT color="#000000"&gt;The RTSP camera streaming pipeline using GStreamer on the&lt;STRONG&gt; i.MX8M Plus FRDM board (4GB RAM) &lt;/STRONG&gt;fails when processing high-resolution video streams (2K or above Full HD).&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;The system successfully initializes the pipeline and establishes an RTSP connection. However, during playback, the pipeline terminates with the following errors:&lt;/FONT&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;Internal data stream error&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;streaming stopped, reason not-negotiated (-4)&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;Could not write to resource (Received end-of-file)&lt;/FONT&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;This issue is observed specifically with high-resolution (≥2K) H.265 streams, indicating that the platform is unable to negotiate or sustain the required decoding pipeline.&lt;/FONT&gt;&lt;/P&gt;&lt;H3&gt;&lt;FONT color="#000000"&gt;Key Observations:&lt;/FONT&gt;&lt;/H3&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;GStreamer pipeline works for lower resolutions (e.g., 1080p)&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;Failure occurs during caps negotiation or decoder stage&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;Hardware decoder (v4l2h265dec) likely hitting limitations&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;System is running:&lt;/FONT&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;Linux Kernel: 6.6.x (scarthgap)&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;Yocto-based NXP BSP&lt;/FONT&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT color="#000000"&gt;Board configuration: i.MX8M Plus FRDM with 4GB RAM&lt;/FONT&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Mon, 20 Apr 2026 08:16:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTSP-Camera-Streaming-Failure-for-2K-Above-Full-HD-Resolution-on/m-p/2353565#M244935</guid>
      <dc:creator>Kaustubhnaik45</dc:creator>
      <dc:date>2026-04-20T08:16:18Z</dc:date>
    </item>
    <item>
      <title>Re: RTSP Camera Streaming Failure for 2K/Above Full HD Resolution on NXP i.MX8M Plus FRDM (4GB RAM)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTSP-Camera-Streaming-Failure-for-2K-Above-Full-HD-Resolution-on/m-p/2356679#M245016</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;This issue is regarding the encoding/decoding operations for H.265 2K frames, i.MX 8M Plus supports only 1080p as seen in the documentation.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JosephAtNXP_0-1777309761873.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/383716iC298EDE5C6DA8C46/image-size/large?v=v2&amp;amp;px=999" role="button" title="JosephAtNXP_0-1777309761873.png" alt="JosephAtNXP_0-1777309761873.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JosephAtNXP_0-1777309761873.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 27 Apr 2026 17:09:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTSP-Camera-Streaming-Failure-for-2K-Above-Full-HD-Resolution-on/m-p/2356679#M245016</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2026-04-27T17:09:33Z</dc:date>
    </item>
    <item>
      <title>Re: RTSP Camera Streaming Failure for 2K/Above Full HD Resolution on NXP i.MX8M Plus FRDM (4GB RAM)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTSP-Camera-Streaming-Failure-for-2K-Above-Full-HD-Resolution-on/m-p/2357091#M245035</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;First of all, thank you for your reply.&lt;/P&gt;&lt;P&gt;Based on your clarification that the i.MX 8M Plus supports only up to 1080p . I would like to ask if you could suggest any alternative&amp;nbsp;suitable processors or development boards&amp;nbsp; that supports &lt;STRONG&gt;2K (1440p) RTSP streaming&lt;/STRONG&gt;, particularly .&lt;/P&gt;&lt;P&gt;Thank you in advance for your guidance.&lt;/P&gt;</description>
      <pubDate>Tue, 28 Apr 2026 08:55:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTSP-Camera-Streaming-Failure-for-2K-Above-Full-HD-Resolution-on/m-p/2357091#M245035</guid>
      <dc:creator>Kaustubhnaik45</dc:creator>
      <dc:date>2026-04-28T08:55:55Z</dc:date>
    </item>
    <item>
      <title>Re: RTSP Camera Streaming Failure for 2K/Above Full HD Resolution on NXP i.MX8M Plus FRDM (4GB RAM)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTSP-Camera-Streaming-Failure-for-2K-Above-Full-HD-Resolution-on/m-p/2360169#M245093</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/261887"&gt;@Kaustubhnaik45&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please refer to&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/reference-manual/IMX95RM.pdf" target="_self"&gt;i.MX 95 Reference Manual&lt;/A&gt;,&lt;/P&gt;
&lt;P&gt;The VPU domain consists of a H.264/H.265 VPU codec, a motion JPEG encoder, and a motion JPEG decoder for image and video compression applications.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JosephAtNXP_0-1777917598467.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/384276i915CD5463401D9BF/image-size/large?v=v2&amp;amp;px=999" role="button" title="JosephAtNXP_0-1777917598467.png" alt="JosephAtNXP_0-1777917598467.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JosephAtNXP_0-1777917598467.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 04 May 2026 18:00:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTSP-Camera-Streaming-Failure-for-2K-Above-Full-HD-Resolution-on/m-p/2360169#M245093</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2026-05-04T18:00:12Z</dc:date>
    </item>
    <item>
      <title>Re: RTSP Camera Streaming Failure for 2K/Above Full HD Resolution on NXP i.MX8M Plus FRDM (4GB RAM)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTSP-Camera-Streaming-Failure-for-2K-Above-Full-HD-Resolution-on/m-p/2374283#M245435</link>
      <description>Hi,&lt;BR /&gt;&lt;BR /&gt;Thanks for confirming that i.MX 8MPlus supports H.265 up to 1080p@60fps.&lt;BR /&gt;&lt;BR /&gt;Could you please clarify whether the device can decode a 2560×1440 (1440p) H.265 stream at a very low frame rate (e.g., 5 fps)?&lt;BR /&gt;&lt;BR /&gt;Is the 1080p limit a hard resolution limitation of the VPU hardware ?</description>
      <pubDate>Mon, 01 Jun 2026 07:18:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTSP-Camera-Streaming-Failure-for-2K-Above-Full-HD-Resolution-on/m-p/2374283#M245435</guid>
      <dc:creator>Kaustubhnaik45</dc:creator>
      <dc:date>2026-06-01T07:18:58Z</dc:date>
    </item>
  </channel>
</rss>