<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 i.MX8MM – Kernel logo support with DRM / GKI (fb/simplefb issue)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-Kernel-logo-support-with-DRM-GKI-fb-simplefb-issue/m-p/2350106#M244876</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on i.MX8MM (Android 12, kernel 5.15, GKI) and trying to implement a kernel-level logo.&lt;/P&gt;&lt;P&gt;Since FBDEV is not supported in Android 12, I attempted to enable&lt;BR /&gt;CONFIG_FB=y&lt;BR /&gt;CONFIG_FB_EFI=y&lt;BR /&gt;CONFIG_LOGO=y&lt;BR /&gt;and use a framebuffer/simplefb-based approach. However, I am facing the following issues:&lt;/P&gt;&lt;P&gt;* Kernel crashes when adding the framebuffer node&lt;BR /&gt;* simplefb/simpledrm is not working as expected&lt;BR /&gt;* Display drivers (LCDIF + MIPI DSI) are built as GKI modules&lt;/P&gt;&lt;P&gt;Because of this, I am unable to display any logo during the kernel phase.&lt;/P&gt;&lt;P&gt;I also tried to retain the U-Boot logo during the kernel transition by disabling video shutdown (video_link_shut_down), as suggested in some references. However, the display still goes blank (white/black) before the Android boot animation starts.&lt;/P&gt;&lt;P&gt;I have attached a video for reference.&lt;/P&gt;&lt;P&gt;**Platform details:**&lt;/P&gt;&lt;P&gt;* SoC: i.MX8MM&lt;BR /&gt;* Display pipeline: LCDIF + MIPI DSI (ili9881c panel)&lt;BR /&gt;* Display driver: DRM/KMS (no FBDEV)&lt;BR /&gt;* Kernel: 5.15 (Android GKI)&lt;/P&gt;&lt;P&gt;**Questions:**&lt;/P&gt;&lt;P&gt;1. What is the recommended approach to implement a kernel logo using DRM (without FBDEV)?&lt;BR /&gt;2. Does NXP BSP support simplefb/simpledrm for Android 12?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Mon, 13 Apr 2026 10:44:16 GMT</pubDate>
    <dc:creator>Santhrupthi_123</dc:creator>
    <dc:date>2026-04-13T10:44:16Z</dc:date>
    <item>
      <title>i.MX8MM – Kernel logo support with DRM / GKI (fb/simplefb issue)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-Kernel-logo-support-with-DRM-GKI-fb-simplefb-issue/m-p/2350106#M244876</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on i.MX8MM (Android 12, kernel 5.15, GKI) and trying to implement a kernel-level logo.&lt;/P&gt;&lt;P&gt;Since FBDEV is not supported in Android 12, I attempted to enable&lt;BR /&gt;CONFIG_FB=y&lt;BR /&gt;CONFIG_FB_EFI=y&lt;BR /&gt;CONFIG_LOGO=y&lt;BR /&gt;and use a framebuffer/simplefb-based approach. However, I am facing the following issues:&lt;/P&gt;&lt;P&gt;* Kernel crashes when adding the framebuffer node&lt;BR /&gt;* simplefb/simpledrm is not working as expected&lt;BR /&gt;* Display drivers (LCDIF + MIPI DSI) are built as GKI modules&lt;/P&gt;&lt;P&gt;Because of this, I am unable to display any logo during the kernel phase.&lt;/P&gt;&lt;P&gt;I also tried to retain the U-Boot logo during the kernel transition by disabling video shutdown (video_link_shut_down), as suggested in some references. However, the display still goes blank (white/black) before the Android boot animation starts.&lt;/P&gt;&lt;P&gt;I have attached a video for reference.&lt;/P&gt;&lt;P&gt;**Platform details:**&lt;/P&gt;&lt;P&gt;* SoC: i.MX8MM&lt;BR /&gt;* Display pipeline: LCDIF + MIPI DSI (ili9881c panel)&lt;BR /&gt;* Display driver: DRM/KMS (no FBDEV)&lt;BR /&gt;* Kernel: 5.15 (Android GKI)&lt;/P&gt;&lt;P&gt;**Questions:**&lt;/P&gt;&lt;P&gt;1. What is the recommended approach to implement a kernel logo using DRM (without FBDEV)?&lt;BR /&gt;2. Does NXP BSP support simplefb/simpledrm for Android 12?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Apr 2026 10:44:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-Kernel-logo-support-with-DRM-GKI-fb-simplefb-issue/m-p/2350106#M244876</guid>
      <dc:creator>Santhrupthi_123</dc:creator>
      <dc:date>2026-04-13T10:44:16Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MM – Kernel logo support with DRM / GKI (fb/simplefb issue)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-Kernel-logo-support-with-DRM-GKI-fb-simplefb-issue/m-p/2354397#M244957</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Please note that Android 12 + GKI + DRM/KMS does not support a classic kernel logo, if you want to have an image early on boot you may use Uboot bootloader logo, using a bmp image.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Apr 2026 00:14:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-Kernel-logo-support-with-DRM-GKI-fb-simplefb-issue/m-p/2354397#M244957</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2026-04-22T00:14:16Z</dc:date>
    </item>
  </channel>
</rss>