<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX95 2D GPU</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX95-2D-GPU/m-p/2349828#M244867</link>
    <description>&lt;P&gt;There is no VGLite or related support for i.MX95, or other MPU. Also no plan for support that.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;I checked the latest SDK(2603), there is g2d+DPU demo. That means the 2d GPU and display has been enabled. For i.MX MPU, 2D GPU is supported by G2D lib.&lt;/P&gt;
&lt;P&gt;And you can check the&amp;nbsp;SDK_26_03_00_IMX95LPD5EVK-19\middleware\g2d_dpu\cm7, the g2d lib is released by "libg2d.a", no opensource.&lt;/P&gt;</description>
    <pubDate>Mon, 13 Apr 2026 02:41:11 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2026-04-13T02:41:11Z</dc:date>
    <item>
      <title>iMX95 2D GPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX95-2D-GPU/m-p/2348250#M244834</link>
      <description>&lt;P&gt;I've been reading that the i.MX95 will have a dedicated 2D GPU that can be used by the M7 core.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Will the bare metal VGLite driver provided by NXP support the 2D GPU in the i.MX95?&lt;/P&gt;&lt;P&gt;I see there are lots of examples for using the VGLite driver for the RT line or processors.&amp;nbsp; Would these apply and work for the M7 and 2D GPU in the i.MX95?&lt;/P&gt;&lt;P&gt;Is the driver for the 2D GPU completely open source, meaning no pre-compiled libraries are required?&lt;/P&gt;</description>
      <pubDate>Thu, 09 Apr 2026 10:15:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX95-2D-GPU/m-p/2348250#M244834</guid>
      <dc:creator>mrudy</dc:creator>
      <dc:date>2026-04-09T10:15:40Z</dc:date>
    </item>
    <item>
      <title>Re: iMX95 2D GPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX95-2D-GPU/m-p/2349828#M244867</link>
      <description>&lt;P&gt;There is no VGLite or related support for i.MX95, or other MPU. Also no plan for support that.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;I checked the latest SDK(2603), there is g2d+DPU demo. That means the 2d GPU and display has been enabled. For i.MX MPU, 2D GPU is supported by G2D lib.&lt;/P&gt;
&lt;P&gt;And you can check the&amp;nbsp;SDK_26_03_00_IMX95LPD5EVK-19\middleware\g2d_dpu\cm7, the g2d lib is released by "libg2d.a", no opensource.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Apr 2026 02:41:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX95-2D-GPU/m-p/2349828#M244867</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2026-04-13T02:41:11Z</dc:date>
    </item>
  </channel>
</rss>