<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX95: Compilation error with bitbake.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX95-Compilation-error-with-bitbake/m-p/2346841#M244813</link>
    <description>&lt;P&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Wed, 08 Apr 2026 08:46:02 GMT</pubDate>
    <dc:creator>danielsan-77</dc:creator>
    <dc:date>2026-04-08T08:46:02Z</dc:date>
    <item>
      <title>iMX95: Compilation error with bitbake.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX95-Compilation-error-with-bitbake/m-p/2346316#M244796</link>
      <description>&lt;P&gt;I want to compile from the source code, but I get errors when compiling it for the iMx95. I am working with a computer with Ubuntu 18.04. To do this I follow the steps of I have followed the steps of &lt;A href="https://dev.variscite.com/dart-mx95/mx95-yocto-walnascar-6.12.49_2.2.0-v1.0/yocto-build-release/" target="_blank"&gt;https://dev.variscite.com/dart-mx95/mx95-yocto-walnascar-6.12.49_2.2.0-v1.0/yocto-build-release/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Specifically, when launching the "bitbake fsl-image-gui-chromium" I get this error:&lt;/P&gt;&lt;P&gt;ERROR: OE-core's config sanity checker detected a potential misconfiguration.&lt;BR /&gt;Either fix the cause of this error or at your own risk disable the checker (see sanity.conf).&lt;BR /&gt;Following is the list of potential problems / advisories:&lt;/P&gt;&lt;P&gt;Fetcher failure for URL: '&lt;A href="https://www.yoctoproject.org/connectivity.html" target="_blank"&gt;https://www.yoctoproject.org/connectivity.html&lt;/A&gt;'. URL doesn't work.&lt;BR /&gt;Please ensure your host's network is configured correctly.&lt;BR /&gt;Please ensure CONNECTIVITY_CHECK_URIS is correct and specified URIs are available.&lt;BR /&gt;If your ISP or network is blocking the above URL,&lt;BR /&gt;try with another domain name, for example by setting:&lt;BR /&gt;CONNECTIVITY_CHECK_URIS = "&lt;A href="https://www.example.com/" target="_blank"&gt;https://www.example.com/&lt;/A&gt;" You could also set BB_NO_NETWORK = "1" to disable network&lt;BR /&gt;access if all required sources are on local disk.&lt;BR /&gt;Summary: There was 1 ERROR message, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;I have also tried other previous versions, but the same thing happens.&lt;/P&gt;&lt;P&gt;The same error occurs if I launch other bitbakes.&lt;/P&gt;&lt;P&gt;All the best,&lt;BR /&gt;Daniel.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Apr 2026 11:53:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX95-Compilation-error-with-bitbake/m-p/2346316#M244796</guid>
      <dc:creator>danielsan-77</dc:creator>
      <dc:date>2026-04-07T11:53:05Z</dc:date>
    </item>
    <item>
      <title>Re: iMX95: Compilation error with bitbake.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX95-Compilation-error-with-bitbake/m-p/2346545#M244805</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I suggest you check directly with Variscite since our BSP is built&amp;nbsp;and requirements are different.&lt;/P&gt;
&lt;P&gt;Please check if this is a known issue in the recipe or if you have some kind of firewall issue since you have fetch errors.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Apr 2026 20:47:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX95-Compilation-error-with-bitbake/m-p/2346545#M244805</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2026-04-07T20:47:40Z</dc:date>
    </item>
    <item>
      <title>Re: iMX95: Compilation error with bitbake.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX95-Compilation-error-with-bitbake/m-p/2346841#M244813</link>
      <description>&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 08 Apr 2026 08:46:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX95-Compilation-error-with-bitbake/m-p/2346841#M244813</guid>
      <dc:creator>danielsan-77</dc:creator>
      <dc:date>2026-04-08T08:46:02Z</dc:date>
    </item>
  </channel>
</rss>