<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Config Tools for i.MX 26.03: Which uboot version is recomonded for the ddr3lConfig Tools v26.03 DDR3 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-26-03-Which-uboot-version-is-recomonded/m-p/2343691#M244725</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using &lt;STRONG&gt;Config Tools for i.MX v26.03&lt;/STRONG&gt; to train DDR3L on a custom i.MX8MM board.&lt;/P&gt;&lt;P&gt;The DDR training completes successfully using the tool, and I have generated the ddr3l_timing.c file.&lt;/P&gt;&lt;P&gt;I built U-Boot using &lt;STRONG&gt;2019.04&lt;/STRONG&gt;, and from the logs it shows that:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;DDR initialization is completed&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;DDR configuration is applied&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;DDR calibration/training is successful&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;However, when I download the U-Boot proper image into DDR (RAM), I observe that memory contains repeated pattern values (as seen in logs), indicating that DDR write is not working correctly.&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;--- SDP CMD RX --- &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;Raw: 0b 0b 40 20 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;Jumping to header at 0x40200000 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;Header Tag is not an IMX image &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;Memory dump at 0000000040200000: &lt;/FONT&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;0x40200000: 20 20 75 75 59 59 c7 c7 8b 8b 07 07 f4 f4 d5 d5 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;0x40200010: ae ae 3d 3d ef ef 27 27 68 68 b0 b0 1a 1a f4 f4 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;0x40200020: 20 20 75 75 59 59 c7 c7 8b 8b 07 07 f4 f4 d5 d5 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;0x40200030: ae ae 3d 3d ef ef 27 27 68 68 b0 b0 1a 1a f4 f4 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;0x40200040: 20 20 75 75 59 59 c7 c7 8b 8b 07 07 f4 f4 d5 d5&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;I also tried building with &lt;STRONG&gt;U-Boot 2023.04&lt;/STRONG&gt;, but I am facing a different issue:&lt;/P&gt;&lt;P&gt;&lt;FONT face="batang,apple gothic"&gt;U-Boot SPL 2023.04-dirty (Apr 01 2026 - 16:03:20 +0530)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;CPU freq: 1200 MHz&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;PMIC: PCA9450AA configured for DDR3L (1.5V) and custom rails&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;DDRINFO: start DRAM init&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;DDRINFO: DRAM rate 344069MTS&lt;BR /&gt;&lt;BR /&gt;&lt;/FONT&gt;At this point, the system gets stuck and does not proceed further.&lt;/P&gt;&lt;P&gt;So my questions are:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Which U-Boot version is recommended when using Config Tools v26.03 for DDR3L?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is the generated ddr3l_timing.c compatible with U-Boot 2019.04, or is a newer version required?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Could this issue (successful training but DDR write failure) be due to a mismatch between tool version and U-Boot version?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Wed, 01 Apr 2026 13:11:52 GMT</pubDate>
    <dc:creator>suraj02</dc:creator>
    <dc:date>2026-04-01T13:11:52Z</dc:date>
    <item>
      <title>Config Tools for i.MX 26.03: Which uboot version is recomonded for the ddr3lConfig Tools v26.03 DDR3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-26-03-Which-uboot-version-is-recomonded/m-p/2343691#M244725</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using &lt;STRONG&gt;Config Tools for i.MX v26.03&lt;/STRONG&gt; to train DDR3L on a custom i.MX8MM board.&lt;/P&gt;&lt;P&gt;The DDR training completes successfully using the tool, and I have generated the ddr3l_timing.c file.&lt;/P&gt;&lt;P&gt;I built U-Boot using &lt;STRONG&gt;2019.04&lt;/STRONG&gt;, and from the logs it shows that:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;DDR initialization is completed&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;DDR configuration is applied&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;DDR calibration/training is successful&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;However, when I download the U-Boot proper image into DDR (RAM), I observe that memory contains repeated pattern values (as seen in logs), indicating that DDR write is not working correctly.&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;--- SDP CMD RX --- &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;Raw: 0b 0b 40 20 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;Jumping to header at 0x40200000 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;Header Tag is not an IMX image &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;Memory dump at 0000000040200000: &lt;/FONT&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;0x40200000: 20 20 75 75 59 59 c7 c7 8b 8b 07 07 f4 f4 d5 d5 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;0x40200010: ae ae 3d 3d ef ef 27 27 68 68 b0 b0 1a 1a f4 f4 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;0x40200020: 20 20 75 75 59 59 c7 c7 8b 8b 07 07 f4 f4 d5 d5 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;0x40200030: ae ae 3d 3d ef ef 27 27 68 68 b0 b0 1a 1a f4 f4 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;0x40200040: 20 20 75 75 59 59 c7 c7 8b 8b 07 07 f4 f4 d5 d5&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;I also tried building with &lt;STRONG&gt;U-Boot 2023.04&lt;/STRONG&gt;, but I am facing a different issue:&lt;/P&gt;&lt;P&gt;&lt;FONT face="batang,apple gothic"&gt;U-Boot SPL 2023.04-dirty (Apr 01 2026 - 16:03:20 +0530)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;CPU freq: 1200 MHz&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;PMIC: PCA9450AA configured for DDR3L (1.5V) and custom rails&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;DDRINFO: start DRAM init&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="batang,apple gothic"&gt;DDRINFO: DRAM rate 344069MTS&lt;BR /&gt;&lt;BR /&gt;&lt;/FONT&gt;At this point, the system gets stuck and does not proceed further.&lt;/P&gt;&lt;P&gt;So my questions are:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Which U-Boot version is recommended when using Config Tools v26.03 for DDR3L?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is the generated ddr3l_timing.c compatible with U-Boot 2019.04, or is a newer version required?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Could this issue (successful training but DDR write failure) be due to a mismatch between tool version and U-Boot version?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 01 Apr 2026 13:11:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-26-03-Which-uboot-version-is-recomonded/m-p/2343691#M244725</guid>
      <dc:creator>suraj02</dc:creator>
      <dc:date>2026-04-01T13:11:52Z</dc:date>
    </item>
    <item>
      <title>Re: Config Tools for i.MX 26.03: Which uboot version is recomonded for the ddr3lConfig Tools v26.03</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-26-03-Which-uboot-version-is-recomonded/m-p/2343827#M244731</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;They don't relate that closely, probably you could compare the generated code against the functions in the other boards configs. You could share it and we could compare it.&lt;/P&gt;
&lt;P&gt;Most of the time it's related to the DDR config and bringup rather than U-boot version. I would suggest double-checking it.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 01 Apr 2026 19:52:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Config-Tools-for-i-MX-26-03-Which-uboot-version-is-recomonded/m-p/2343827#M244731</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2026-04-01T19:52:57Z</dc:date>
    </item>
  </channel>
</rss>