<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RPI-CAM-MIPI and i.MX93FRDM issues on BSP6.12.49 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RPI-CAM-MIPI-and-i-MX93FRDM-issues-on-BSP6-12-49/m-p/2337420#M244599</link>
    <description>&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;My understanding is that to run 6.1.3.1.3, I placed /lib/firmware/ap1302_ar0144_single_fw.bin and executed the following.&lt;/P&gt;&lt;P&gt;media-ctl -V "'ap1302 2-003c':2 [fmt:UYVY8_1X16/1920x1080 field:none]"&lt;BR /&gt;media-ctl -V "'csidev-4ae00000.csi':0 [fmt:UYVY8_1X16/1920x1080 field:none]"&lt;BR /&gt;media-ctl -V "'csidev-4ae00000.csi':1 [fmt:UYVY8_1X16/1920x1080 field:none]"&lt;BR /&gt;media-ctl -V "'crossbar':0 [fmt:UYVY8_1X16/1920x1080 field:none]"&lt;BR /&gt;media-ctl -V "'crossbar':2 [fmt:UYVY8_1X16/1920x1080 field:none]"&lt;BR /&gt;media-ctl -V "'mxc_isi.0':1 [fmt:YUV8_1X24/1920x1080 field:none]"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I then tried to display the video using this command, and although no errors occurred, the camera image did not appear on the screen.&lt;BR /&gt;gst-launch-1.0 v4l2src device=/dev/video0 ! "video/x-raw,format=YUY2,width=1920,height=1080,framerate=30/1" ! videoconvert ! autovideosink&lt;/P&gt;&lt;P&gt;Are there any plans to revise the procedure (4.3) for displaying camera images in UM11933 for the latest BSP?&lt;/P&gt;</description>
    <pubDate>Mon, 23 Mar 2026 08:39:00 GMT</pubDate>
    <dc:creator>Ryo_Aoki</dc:creator>
    <dc:date>2026-03-23T08:39:00Z</dc:date>
    <item>
      <title>RPI-CAM-MIPI and i.MX93FRDM issues on BSP6.12.49</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RPI-CAM-MIPI-and-i-MX93FRDM-issues-on-BSP6-12-49/m-p/2334353#M244537</link>
      <description>&lt;P&gt;Hi NXP.&lt;/P&gt;&lt;P&gt;I'm trying to run RPI-CAM-MIPI on an i.MX93FRDM, but I'm having trouble getting it to work with the latest BSP 6.12.49.&lt;BR /&gt;With the BSP6.6.36 image, setting it up according to UM11933 allowed RPI-CAM-MIPI to work without any problems and display video.&lt;BR /&gt;However, with BSP6.12.49, even if I follow the same setup procedure and run the same commands, the video does not display.&lt;/P&gt;&lt;P&gt;If you find out the cause of this phenomenon or how to fix it, please let me know.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;log:&lt;BR /&gt;root@imx93-11x11-lpddr4x-frdm:~# gst-launch-1.0 -v v4l2src device=/dev/video0 ! ""video/x-raw,format=YUY2,width=1280,height=800"" ! queue ! waylandsink&lt;BR /&gt;Setting pipeline to PAUSED ...&lt;BR /&gt;Pipeline is live and does not need PREROLL ...&lt;BR /&gt;Pipeline is PREROLLED ...&lt;BR /&gt;Setting pipeline to PLAYING ...&lt;BR /&gt;New clock: GstSystemClock&lt;BR /&gt;/GstPipeline:pipeline0/GstV4l2Src:v4l2src0.GstPad:src: caps = video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709&lt;BR /&gt;/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:src: caps = video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709&lt;BR /&gt;/GstPipeline:pipeline0/GstQueue:queue0.GstPad:sink: caps = video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709&lt;BR /&gt;/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:sink: caps = video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709&lt;BR /&gt;/GstPipeline:pipeline0/GstQueue:queue0.GstPad:src: caps = video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709&lt;BR /&gt;/GstPipeline:pipeline0/GstWaylandSink:waylandsink0.GstPad:sink: caps = video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709&lt;BR /&gt;ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Failed to allocate required memory.&lt;BR /&gt;Additional debug info:&lt;BR /&gt;/usr/src/debug/gstreamer1.0-plugins-good/1.26.6.imx/sys/v4l2/gstv4l2src.c(957): gst_v4l2src_decide_allocation (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:&lt;BR /&gt;Buffer pool activation failed&lt;BR /&gt;Execution ended after 0:00:00.017016750&lt;BR /&gt;Setting pipeline to NULL ...&lt;BR /&gt;ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Internal data stream error.&lt;BR /&gt;Additional debug info:&lt;BR /&gt;/usr/src/debug/gstreamer1.0/1.26.6.imx/libs/gst/base/gstbasesrc.c(3187): gst_base_src_loop (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:&lt;BR /&gt;streaming stopped, reason not-negotiated (-4)&lt;BR /&gt;Freeing pipeline ...&lt;BR /&gt;root@imx93-11x11-lpddr4x-frdm:~#"&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Additional information:&lt;BR /&gt;UM11933 specifies that ap1302.fw should be placed in /lib/firmware/imx/camera.&lt;BR /&gt;However, when I tried the same thing with BPS 6.12.49, I got the following error:&lt;BR /&gt;$ dmesg | grep -E 'ap1302|mx8-img-md'&lt;BR /&gt;[ 11.642956] ap1302 2-003c: Direct firmware load for ap1302_ar0144_single_fw.bin failed with error -2&lt;BR /&gt;[ 11.642979] ap1302 2-003c: Falling back to sysfs fallback for: ap1302_ar0144_single_fw.bin&lt;/P&gt;&lt;P&gt;This error can be avoided by placing ap1302_ar0144_single_fw.bin in /lib/firmware, but this does not resolve the issue of the video not displaying.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Mar 2026 01:56:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RPI-CAM-MIPI-and-i-MX93FRDM-issues-on-BSP6-12-49/m-p/2334353#M244537</guid>
      <dc:creator>Ryo_Aoki</dc:creator>
      <dc:date>2026-03-18T01:56:06Z</dc:date>
    </item>
    <item>
      <title>Re: RPI-CAM-MIPI and i.MX93FRDM issues on BSP6.12.49</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RPI-CAM-MIPI-and-i-MX93FRDM-issues-on-BSP6-12-49/m-p/2334437#M244539</link>
      <description>&lt;P&gt;for the 6.12 bsp, you need to use media-ctl to create a link ,pls refer to the chapter&amp;nbsp;6.1.3.1.3 AP1302/AR0144 of reference manual&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/reference-manual/RM00293.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/reference-manual/RM00293.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Mar 2026 05:32:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RPI-CAM-MIPI-and-i-MX93FRDM-issues-on-BSP6-12-49/m-p/2334437#M244539</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2026-03-18T05:32:18Z</dc:date>
    </item>
    <item>
      <title>Re: RPI-CAM-MIPI and i.MX93FRDM issues on BSP6.12.49</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RPI-CAM-MIPI-and-i-MX93FRDM-issues-on-BSP6-12-49/m-p/2337420#M244599</link>
      <description>&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;My understanding is that to run 6.1.3.1.3, I placed /lib/firmware/ap1302_ar0144_single_fw.bin and executed the following.&lt;/P&gt;&lt;P&gt;media-ctl -V "'ap1302 2-003c':2 [fmt:UYVY8_1X16/1920x1080 field:none]"&lt;BR /&gt;media-ctl -V "'csidev-4ae00000.csi':0 [fmt:UYVY8_1X16/1920x1080 field:none]"&lt;BR /&gt;media-ctl -V "'csidev-4ae00000.csi':1 [fmt:UYVY8_1X16/1920x1080 field:none]"&lt;BR /&gt;media-ctl -V "'crossbar':0 [fmt:UYVY8_1X16/1920x1080 field:none]"&lt;BR /&gt;media-ctl -V "'crossbar':2 [fmt:UYVY8_1X16/1920x1080 field:none]"&lt;BR /&gt;media-ctl -V "'mxc_isi.0':1 [fmt:YUV8_1X24/1920x1080 field:none]"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I then tried to display the video using this command, and although no errors occurred, the camera image did not appear on the screen.&lt;BR /&gt;gst-launch-1.0 v4l2src device=/dev/video0 ! "video/x-raw,format=YUY2,width=1920,height=1080,framerate=30/1" ! videoconvert ! autovideosink&lt;/P&gt;&lt;P&gt;Are there any plans to revise the procedure (4.3) for displaying camera images in UM11933 for the latest BSP?&lt;/P&gt;</description>
      <pubDate>Mon, 23 Mar 2026 08:39:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RPI-CAM-MIPI-and-i-MX93FRDM-issues-on-BSP6-12-49/m-p/2337420#M244599</guid>
      <dc:creator>Ryo_Aoki</dc:creator>
      <dc:date>2026-03-23T08:39:00Z</dc:date>
    </item>
    <item>
      <title>Re: RPI-CAM-MIPI and i.MX93FRDM issues on BSP6.12.49</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RPI-CAM-MIPI-and-i-MX93FRDM-issues-on-BSP6-12-49/m-p/2338884#M244626</link>
      <description>&lt;P&gt;you can refer my document for this topic&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/ov5640-support-on-i-mx93-with-6-12-20-bsp/ta-p/2129317" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/ov5640-support-on-i-mx93-with-6-12-20-bsp/ta-p/2129317&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Mar 2026 01:47:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RPI-CAM-MIPI-and-i-MX93FRDM-issues-on-BSP6-12-49/m-p/2338884#M244626</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2026-03-25T01:47:12Z</dc:date>
    </item>
  </channel>
</rss>