<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX93 RS485 half duplex without Rx enable gpio in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-RS485-half-duplex-without-Rx-enable-gpio/m-p/2336399#M244576</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using the i.MX93 with RS485 on Linux, but the hardware doesn't have a separate gpio for controlling the transceiver's receive enable pin, so the hardware echos anything that is transmitted.&lt;/P&gt;&lt;P&gt;On a Raspberry Pi, the pl011 driver handles this by disabling the uart's receive enable when transmitting and the SER_RS485_RX_DURING_TX flag is not set.&lt;/P&gt;&lt;P&gt;I tried to implement the same for the lpuart, but it looks like lpuart32_tx_empty() returns non-zero whilst there is still data in the fifo.&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;P&gt;Thanks, Phil&lt;/P&gt;</description>
    <pubDate>Fri, 20 Mar 2026 07:57:29 GMT</pubDate>
    <dc:creator>phil331</dc:creator>
    <dc:date>2026-03-20T07:57:29Z</dc:date>
    <item>
      <title>i.MX93 RS485 half duplex without Rx enable gpio</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-RS485-half-duplex-without-Rx-enable-gpio/m-p/2336399#M244576</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using the i.MX93 with RS485 on Linux, but the hardware doesn't have a separate gpio for controlling the transceiver's receive enable pin, so the hardware echos anything that is transmitted.&lt;/P&gt;&lt;P&gt;On a Raspberry Pi, the pl011 driver handles this by disabling the uart's receive enable when transmitting and the SER_RS485_RX_DURING_TX flag is not set.&lt;/P&gt;&lt;P&gt;I tried to implement the same for the lpuart, but it looks like lpuart32_tx_empty() returns non-zero whilst there is still data in the fifo.&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;P&gt;Thanks, Phil&lt;/P&gt;</description>
      <pubDate>Fri, 20 Mar 2026 07:57:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-RS485-half-duplex-without-Rx-enable-gpio/m-p/2336399#M244576</guid>
      <dc:creator>phil331</dc:creator>
      <dc:date>2026-03-20T07:57:29Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 RS485 half duplex without Rx enable gpio</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-RS485-half-duplex-without-Rx-enable-gpio/m-p/2336574#M244581</link>
      <description>&lt;P&gt;I've mailed to you pls check&lt;/P&gt;</description>
      <pubDate>Fri, 20 Mar 2026 09:55:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-RS485-half-duplex-without-Rx-enable-gpio/m-p/2336574#M244581</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2026-03-20T09:55:05Z</dc:date>
    </item>
  </channel>
</rss>