<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: How do I specify the debug UART for the MIMX8ML8CVNKZAB?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-specify-the-debug-UART-for-the-MIMX8ML8CVNKZAB/m-p/2333209#M244497</link>
    <description>&lt;P&gt;I apologize for the late reply. Thank you for your answer; it was very helpful.&lt;/P&gt;&lt;P&gt;I was able to establish a UART connection by specifying the Debug UART port in the i.MX8MP (865) DDR Controller Configuration Spreadsheet (MX8M_Plus_DDR4_RPA_v10.xlsx).&lt;/P&gt;&lt;P&gt;I referred to the following link for MX8M_Plus_DDR4_RPA_v10.xlsx:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8MPlus-m865S-DDR-Register-Programming-Aids-RPA/ta-p/1235352" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8MPlus-m865S-DDR-Register-Programming-Aids-RPA/ta-p/1235352&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 16 Mar 2026 04:01:56 GMT</pubDate>
    <dc:creator>TK141</dc:creator>
    <dc:date>2026-03-16T04:01:56Z</dc:date>
    <item>
      <title>How do I specify the debug UART for the MIMX8ML8CVNKZAB?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-specify-the-debug-UART-for-the-MIMX8ML8CVNKZAB/m-p/2327654#M244345</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;I have finished designing a board featuring the MIMX8ML8CVNKZAB and two DDR4 (8GBit 512M x 16) buses. I am preparing to build the board and will soon receive the assembled board.&lt;/P&gt;&lt;P&gt;While preparing to check the communication between the SoC and the DDR, I came across the following comment in the mscale_ddr_tool_v3.31&lt;BR /&gt;MSCALE_DDR_Tool_User_Guide.pdf document:&lt;/P&gt;&lt;P&gt;1. Connect the target board to the PC host.&lt;/P&gt;&lt;P&gt;Connect a UART cable from the host computer to the MX8MSCALE debug UART.&lt;/P&gt;&lt;P&gt;Regarding the debug UART, this SoC has UART1 through UART4. Is there a designated port when using the debug UART? If so, do you know how to specify it?&lt;/P&gt;</description>
      <pubDate>Fri, 06 Mar 2026 08:49:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-specify-the-debug-UART-for-the-MIMX8ML8CVNKZAB/m-p/2327654#M244345</guid>
      <dc:creator>TK141</dc:creator>
      <dc:date>2026-03-06T08:49:10Z</dc:date>
    </item>
    <item>
      <title>Re: How do I specify the debug UART for the MIMX8ML8CVNKZAB?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-specify-the-debug-UART-for-the-MIMX8ML8CVNKZAB/m-p/2328748#M244377</link>
      <description>&lt;P&gt;Default debug UART on common i.MX8M Plus platforms&lt;/P&gt;
&lt;P&gt;A53 uses uart2 as debug port and M7 uses uart4 as debug port.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You may choose any of the four UARTs (UART1–UART4) as the debug UART,&amp;nbsp;as long as:&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;You routed that UART's TX/RX pins to a connector (or a USB‑serial IC), and&lt;/LI&gt;
&lt;LI&gt;You configure:&lt;/LI&gt;
&lt;UL&gt;
&lt;LI&gt;ATF (BL31 early output)&lt;/LI&gt;
&lt;LI&gt;U‑Boot stdout-path&lt;/LI&gt;
&lt;LI&gt;Linux Device Tree (chosen { stdout-path = &amp;amp;uartX; })&lt;/LI&gt;
&lt;/UL&gt;
&lt;/OL&gt;
&lt;P&gt;Please refer to the following link.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NXP-Tech-Blog/How-to-Change-i-MX8MM-evk-Linux-Debug-UART/ba-p/1243938?attachment-id=111447" target="_blank"&gt;https://community.nxp.com/t5/NXP-Tech-Blog/How-to-Change-i-MX8MM-evk-Linux-Debug-UART/ba-p/1243938?attachment-id=111447&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 09 Mar 2026 08:39:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-specify-the-debug-UART-for-the-MIMX8ML8CVNKZAB/m-p/2328748#M244377</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2026-03-09T08:39:15Z</dc:date>
    </item>
    <item>
      <title>Re: How do I specify the debug UART for the MIMX8ML8CVNKZAB?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-specify-the-debug-UART-for-the-MIMX8ML8CVNKZAB/m-p/2333209#M244497</link>
      <description>&lt;P&gt;I apologize for the late reply. Thank you for your answer; it was very helpful.&lt;/P&gt;&lt;P&gt;I was able to establish a UART connection by specifying the Debug UART port in the i.MX8MP (865) DDR Controller Configuration Spreadsheet (MX8M_Plus_DDR4_RPA_v10.xlsx).&lt;/P&gt;&lt;P&gt;I referred to the following link for MX8M_Plus_DDR4_RPA_v10.xlsx:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8MPlus-m865S-DDR-Register-Programming-Aids-RPA/ta-p/1235352" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8MPlus-m865S-DDR-Register-Programming-Aids-RPA/ta-p/1235352&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 16 Mar 2026 04:01:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-specify-the-debug-UART-for-the-MIMX8ML8CVNKZAB/m-p/2333209#M244497</guid>
      <dc:creator>TK141</dc:creator>
      <dc:date>2026-03-16T04:01:56Z</dc:date>
    </item>
  </channel>
</rss>