<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMX8QM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX8QM/m-p/2333125#M244490</link>
    <description>&lt;P&gt;Subject: Jailhouse Hypervisor support on i.MX8QM with latest kernel&lt;/P&gt;&lt;P&gt;Hello NXP Team,&lt;/P&gt;&lt;P&gt;We are planning to use the MCIMX8QM SoC (i.MX8 QuadMax) for our project.&lt;/P&gt;&lt;P&gt;Our target architecture is:&lt;/P&gt;&lt;P&gt;- Hypervisor as the base layer&lt;/P&gt;&lt;P&gt;- Android running as one guest OS&lt;/P&gt;&lt;P&gt;- FreeRTOS running as another guest OS&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are evaluating hypervisor solutions for this platform.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would like to clarify the following:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Is Jailhouse hypervisor supported on the latest i.MX8QM BSP and kernel versions (for example Linux 5.15 or newer)?&lt;/P&gt;&lt;P&gt;2. If Jailhouse is not supported in the latest BSP, is there any recommended hypervisor from NXP for this architecture?&lt;/P&gt;&lt;P&gt;3. Does NXP provide any reference design or documentation for running Android + FreeRTOS on top of a hypervisor on i.MX8QM?&lt;/P&gt;&lt;P&gt;Our goal is to run:&lt;/P&gt;&lt;P&gt;- Android on A-core cluster&lt;/P&gt;&lt;P&gt;- FreeRTOS as another isolated guest&lt;/P&gt;&lt;P&gt;Any guidance or recommended approach from NXP would be very helpful.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Sun, 15 Mar 2026 15:01:12 GMT</pubDate>
    <dc:creator>Shivu_Guru_24</dc:creator>
    <dc:date>2026-03-15T15:01:12Z</dc:date>
    <item>
      <title>MX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8QM/m-p/2333125#M244490</link>
      <description>&lt;P&gt;Subject: Jailhouse Hypervisor support on i.MX8QM with latest kernel&lt;/P&gt;&lt;P&gt;Hello NXP Team,&lt;/P&gt;&lt;P&gt;We are planning to use the MCIMX8QM SoC (i.MX8 QuadMax) for our project.&lt;/P&gt;&lt;P&gt;Our target architecture is:&lt;/P&gt;&lt;P&gt;- Hypervisor as the base layer&lt;/P&gt;&lt;P&gt;- Android running as one guest OS&lt;/P&gt;&lt;P&gt;- FreeRTOS running as another guest OS&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are evaluating hypervisor solutions for this platform.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would like to clarify the following:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Is Jailhouse hypervisor supported on the latest i.MX8QM BSP and kernel versions (for example Linux 5.15 or newer)?&lt;/P&gt;&lt;P&gt;2. If Jailhouse is not supported in the latest BSP, is there any recommended hypervisor from NXP for this architecture?&lt;/P&gt;&lt;P&gt;3. Does NXP provide any reference design or documentation for running Android + FreeRTOS on top of a hypervisor on i.MX8QM?&lt;/P&gt;&lt;P&gt;Our goal is to run:&lt;/P&gt;&lt;P&gt;- Android on A-core cluster&lt;/P&gt;&lt;P&gt;- FreeRTOS as another isolated guest&lt;/P&gt;&lt;P&gt;Any guidance or recommended approach from NXP would be very helpful.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Sun, 15 Mar 2026 15:01:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8QM/m-p/2333125#M244490</guid>
      <dc:creator>Shivu_Guru_24</dc:creator>
      <dc:date>2026-03-15T15:01:12Z</dc:date>
    </item>
    <item>
      <title>Re: MX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8QM/m-p/2333739#M244518</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260363"&gt;@Shivu_Guru_24&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. Is Jailhouse hypervisor supported on the latest i.MX8QM BSP and kernel versions (for example Linux 5.15 or newer)?&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;&amp;gt;&amp;gt;&amp;gt;Not, we do not support&amp;nbsp;hypervisor supported in our BSP code.&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;2. If Jailhouse is not supported in the latest BSP, is there any recommended hypervisor from NXP for this architecture?&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;&amp;gt;&amp;gt;&amp;gt;No, we do not have plan to support&amp;nbsp;hypervisor on i.MX8QM.&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;3. Does NXP provide any reference design or documentation for running Android + FreeRTOS on top of a hypervisor on i.MX8QM?&lt;/P&gt;
&lt;P&gt;Our goal is to run:&lt;/P&gt;
&lt;P&gt;- Android on A-core cluster&lt;/P&gt;
&lt;P&gt;- FreeRTOS as another isolated guest&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;&amp;gt;&amp;gt;&amp;gt;The i.MX Jailhouse source code can be accessed at&amp;nbsp;&lt;A href="https://github.com/nxp-imx/imx-jailhouse" target="_blank"&gt;https://github.com/nxp-imx/imx-jailhous&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;If you intend to run Android, significant customization and porting work will be required by yourself. We do not support it now.&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
      <pubDate>Tue, 17 Mar 2026 03:00:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8QM/m-p/2333739#M244518</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2026-03-17T03:00:56Z</dc:date>
    </item>
  </channel>
</rss>