<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Input spec for XTALI pin when using external clock source in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255956#M24445</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jamesbone"&gt;jamesbone&lt;/A&gt; can you continue with the&amp;nbsp; follow up on this case?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Nov 2013 16:14:09 GMT</pubDate>
    <dc:creator>karina_valencia</dc:creator>
    <dc:date>2013-11-21T16:14:09Z</dc:date>
    <item>
      <title>Input spec for XTALI pin when using external clock source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255951#M24440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Forum,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wish to drive the XTALI pin of the iMX6 with an external clock source. The data sheet states that this is an acceptable thing to do and provides the DC input specifications in section 4.6.1 on page 37 (iMX6 Dual/Quad for Consumer data sheet rev 2.3). One problem is that the Vih value is specified only in terms of NVCC_PLL_OUT. Whilst it is suggested that this is nominally 1.1V, I cannot find a complete specification for NVCC_PLL_OUT. For example, what is the tolerance on this value?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A second problem is that the spec provided for Vih is not very generous and it would be very difficult to strictly meet this spec. The max value is given as equal to NVCC_PLL_OUT. In the Absolute Maximum Ratings (section 4.1.1 on page 19) it suggests that input voltages may exceed the corresponding supply voltage by up to 300mV - is that acceptable for the XTALI input?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using a potential divider and aiming for a nominal swing of 1.1V, I can provide a clock with the following characteristics:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Max DC high: 1150mV&lt;/P&gt;&lt;P&gt;Min DC high: 1050mV&lt;/P&gt;&lt;P&gt;Max positive overshoot: 1200mV for 500ps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Min DC low: 0mV&lt;/P&gt;&lt;P&gt;Max DC low: 10mV&lt;/P&gt;&lt;P&gt;Max negative overshoot: -90mV for 500ps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this acceptable for the XTALI input? Do I need to reduce the high level voltage a little?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Gavin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Nov 2013 17:57:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255951#M24440</guid>
      <dc:creator>gavinjones</dc:creator>
      <dc:date>2013-11-04T17:57:26Z</dc:date>
    </item>
    <item>
      <title>Re: Input spec for XTALI pin when using external clock source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255952#M24441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;NVCC_PLL_OUT it is basically generated by an internal LDO of the i.MX6, ( LDO_1P1).LDO_1P1 - The LDO_1P1 linearly regulates down a higher supply voltage&lt;/P&gt;&lt;P&gt;(2.8V-3.3V from VDD_HIGH_IN) to produce a nominal 1.1V output voltage. This regulator supplies digital portions of USB PHYs, PLLs, and the internal 24MHz oscillator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;VDD_HIGH_IN&amp;nbsp; oscilates between -0.3v - 3.6v&amp;nbsp; but the Regulator it is 1.1v with a aprox 80% of swing.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Nov 2013 18:30:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255952#M24441</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2013-11-08T18:30:41Z</dc:date>
    </item>
    <item>
      <title>Re: Input spec for XTALI pin when using external clock source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255953#M24442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi James,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply but sadly I do not understand it. You say that VDD_HIGH_IN oscillates - this is a power rail and any oscillation would surely be very bad. The oscillator I was referring to in my question is an external crystal oscillator that is feeding the 24MHz clock into the XTALI pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To answer the first part of my question, please can you tell me the minimum and maximum values (accounting for variation due to silicon process, temperature, load regulation, etc) for the NVCC_PLL_OUT output?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Gavin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Nov 2013 20:11:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255953#M24442</guid>
      <dc:creator>gavinjones</dc:creator>
      <dc:date>2013-11-08T20:11:28Z</dc:date>
    </item>
    <item>
      <title>Re: Input spec for XTALI pin when using external clock source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255954#M24443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Oh sorry if my communication skills confuse you,&amp;nbsp; VDD_HIGH_IN it is the power supply of the oscillator. not that oscillates&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Nov 2013 17:54:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255954#M24443</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2013-11-15T17:54:15Z</dc:date>
    </item>
    <item>
      <title>Re: Input spec for XTALI pin when using external clock source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255955#M24444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, thanks for the clarification.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Returning to my question, in order to obtain a complete input specification for the XTALI pin, I need to know the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the minimum and maximum values (accounting for variation due to silicon process, temperature, load regulation, etc) for the NVCC_PLL_OUT output?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Nov 2013 18:59:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255955#M24444</guid>
      <dc:creator>gavinjones</dc:creator>
      <dc:date>2013-11-15T18:59:06Z</dc:date>
    </item>
    <item>
      <title>Re: Input spec for XTALI pin when using external clock source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255956#M24445</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jamesbone"&gt;jamesbone&lt;/A&gt; can you continue with the&amp;nbsp; follow up on this case?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2013 16:14:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255956#M24445</guid>
      <dc:creator>karina_valencia</dc:creator>
      <dc:date>2013-11-21T16:14:09Z</dc:date>
    </item>
    <item>
      <title>Re: Input spec for XTALI pin when using external clock source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255957#M24446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately we do not have such detail information of the XTAL spec. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2013 16:39:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255957#M24446</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2013-11-21T16:39:18Z</dc:date>
    </item>
    <item>
      <title>Re: Input spec for XTALI pin when using external clock source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255958#M24447</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, thanks James.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Given that Freescale are unable to provide an input specification for the XTALI pin, perhaps the assertion that an external clock is supported should be removed from the documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Gavin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2013 17:21:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Input-spec-for-XTALI-pin-when-using-external-clock-source/m-p/255958#M24447</guid>
      <dc:creator>gavinjones</dc:creator>
      <dc:date>2013-11-21T17:21:55Z</dc:date>
    </item>
  </channel>
</rss>