<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Configuring P11 Expansion Connector Pin as GPIO on FRDM-IMX93 (VS Code)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-P11-Expansion-Connector-Pin-as-GPIO-on-FRDM-IMX93-VS/m-p/2329156#M244397</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;Correct, any pin from P11 connector can be used as GPIO, for your reference, you can either download Config Tools for i.MX or review &lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.12.y/arch/arm64/boot/dts/freescale/imx93-pinfunc.h#L33-L246" target="_self"&gt;pin-func.h&lt;/A&gt;; for alternate functions of each pin.&lt;/P&gt;
&lt;P&gt;For pin usage, review &lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.12.y/arch/arm64/boot/dts/freescale/imx93-11x11-frdm.dts" target="_self"&gt;imx93-11x11-frdm.dts&lt;/A&gt;, most of the pins including GPIO_IO02 are not reserved to use, if you find a pin used you can modify DTS accordingly so you can use it in Cortex-M.&lt;/P&gt;
&lt;P&gt;For config, you are correct, you can add&amp;nbsp;IOMUXC_PAD_FSEL1,&amp;nbsp;IOMUXC_PAD_PD_MASK, etc. when needed.&lt;/P&gt;
&lt;P&gt;This is a sample code for using a GPIO in i.MX 93.&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;int main(void)
{
    /* Define the init structure for the output LED pin*/
    rgpio_pin_config_t led_config = {
        kRGPIO_DigitalOutput,
        0,
    };

    /* Board pin, clock, debug console init */
    BOARD_InitHardware();

    /* Print a note to terminal. */
    PRINTF("\r\n RGPIO Driver example\r\n");
    PRINTF("\r\n The LED is taking turns to shine.\r\n");

    /* Init output LED GPIO. */
    RGPIO_PinInit(BOARD_LED_RGPIO, BOARD_LED_RGPIO_PIN, &amp;amp;led_config);

    while (1)
    {
        SDK_DelayAtLeastUs(1000000U, SystemCoreClock);
        RGPIO_PortToggle(BOARD_LED_RGPIO, 1u &amp;lt;&amp;lt; BOARD_LED_RGPIO_PIN);
    }
}&lt;/LI-CODE&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Mon, 09 Mar 2026 17:02:15 GMT</pubDate>
    <dc:creator>JosephAtNXP</dc:creator>
    <dc:date>2026-03-09T17:02:15Z</dc:date>
    <item>
      <title>Configuring P11 Expansion Connector Pin as GPIO on FRDM-IMX93 (VS Code)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-P11-Expansion-Connector-Pin-as-GPIO-on-FRDM-IMX93-VS/m-p/2328168#M244357</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working with the FRDM-IMX93 development board using VS Code with the MCUXpresso SDK. I need to configure one of the pins from the P11 (40-pin expansion connector) as a GPIO to control the START pin of an external ADS1235 ADC.&lt;/P&gt;&lt;P&gt;My plan was to connect the START pin of the ADC to P11 header pin 3.&lt;/P&gt;&lt;P&gt;In the code, I defined the START pin as follows:&lt;/P&gt;&lt;PRE&gt;&lt;SPAN class=""&gt;/* START pin control */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;#define ADS1235_START_GPIO GPIO2&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;#define ADS1235_START_PIN 2U&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;I also configured the pin in the IOMUX like this:&lt;/P&gt;&lt;PRE&gt;&lt;SPAN class=""&gt;void&lt;/SPAN&gt; &lt;SPAN class=""&gt;BOARD_InitUserPins&lt;/SPAN&gt;(&lt;SPAN class=""&gt;void&lt;/SPAN&gt;)&lt;BR /&gt;{&lt;BR /&gt;&lt;SPAN class=""&gt;/* Configure GPIO_IO02 as GPIO2_IO02 (ADS1235 START pin) */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;IOMUXC_SetPinMux&lt;/SPAN&gt;(&lt;SPAN class=""&gt;IOMUXC_PAD_GPIO_IO02__GPIO2_IO02&lt;/SPAN&gt;, &lt;SPAN class=""&gt;0U&lt;/SPAN&gt;);&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;IOMUXC_SetPinConfig&lt;/SPAN&gt;(&lt;BR /&gt;&lt;SPAN class=""&gt;IOMUXC_PAD_GPIO_IO02__GPIO2_IO02&lt;/SPAN&gt;,&lt;BR /&gt;&lt;SPAN class=""&gt;IOMUXC_PAD_DSE&lt;/SPAN&gt;(&lt;SPAN class=""&gt;15U&lt;/SPAN&gt;) &lt;SPAN class=""&gt;/* Drive strength */&lt;/SPAN&gt;&lt;BR /&gt; );&lt;BR /&gt;}&lt;/PRE&gt;&lt;P&gt;From the FRDM-IMX93 schematic, P11 header pin 3 appears to correspond to GPIO2_IO02 (shown as GPIO_2 in the board documentation).&lt;/P&gt;&lt;P&gt;However, when testing in main.c, I tried writing logic 1 and 0 to this GPIO and then reading the pin state back. The read value always returns 0, regardless of what I write. Because of this, I suspect there may be an issue with my GPIO/IOMUX configuration or that the pin may not actually be available as a free GPIO.&lt;/P&gt;&lt;P&gt;My questions are:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Can P11 pin 3 (GPIO2_IO02) be configured as a general-purpose GPIO for controlling the ADS1235 START signal?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;If this pin is not available or is reserved for another function on the FRDM-IMX93 board, could someone suggest a free GPIO pin on the P11 expansion connector that I could use instead?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;What would be the correct GPIO and IOMUX configuration for such a pin in MCUXpresso?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Any guidance on properly configuring GPIO pins from the P11 expansion header on the FRDM-IMX93 would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Shanmugapriya&lt;/P&gt;</description>
      <pubDate>Sat, 07 Mar 2026 07:58:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configuring-P11-Expansion-Connector-Pin-as-GPIO-on-FRDM-IMX93-VS/m-p/2328168#M244357</guid>
      <dc:creator>Shanmugapriya</dc:creator>
      <dc:date>2026-03-07T07:58:10Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring P11 Expansion Connector Pin as GPIO on FRDM-IMX93 (VS Code)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-P11-Expansion-Connector-Pin-as-GPIO-on-FRDM-IMX93-VS/m-p/2329156#M244397</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;Correct, any pin from P11 connector can be used as GPIO, for your reference, you can either download Config Tools for i.MX or review &lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.12.y/arch/arm64/boot/dts/freescale/imx93-pinfunc.h#L33-L246" target="_self"&gt;pin-func.h&lt;/A&gt;; for alternate functions of each pin.&lt;/P&gt;
&lt;P&gt;For pin usage, review &lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.12.y/arch/arm64/boot/dts/freescale/imx93-11x11-frdm.dts" target="_self"&gt;imx93-11x11-frdm.dts&lt;/A&gt;, most of the pins including GPIO_IO02 are not reserved to use, if you find a pin used you can modify DTS accordingly so you can use it in Cortex-M.&lt;/P&gt;
&lt;P&gt;For config, you are correct, you can add&amp;nbsp;IOMUXC_PAD_FSEL1,&amp;nbsp;IOMUXC_PAD_PD_MASK, etc. when needed.&lt;/P&gt;
&lt;P&gt;This is a sample code for using a GPIO in i.MX 93.&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;int main(void)
{
    /* Define the init structure for the output LED pin*/
    rgpio_pin_config_t led_config = {
        kRGPIO_DigitalOutput,
        0,
    };

    /* Board pin, clock, debug console init */
    BOARD_InitHardware();

    /* Print a note to terminal. */
    PRINTF("\r\n RGPIO Driver example\r\n");
    PRINTF("\r\n The LED is taking turns to shine.\r\n");

    /* Init output LED GPIO. */
    RGPIO_PinInit(BOARD_LED_RGPIO, BOARD_LED_RGPIO_PIN, &amp;amp;led_config);

    while (1)
    {
        SDK_DelayAtLeastUs(1000000U, SystemCoreClock);
        RGPIO_PortToggle(BOARD_LED_RGPIO, 1u &amp;lt;&amp;lt; BOARD_LED_RGPIO_PIN);
    }
}&lt;/LI-CODE&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 09 Mar 2026 17:02:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configuring-P11-Expansion-Connector-Pin-as-GPIO-on-FRDM-IMX93-VS/m-p/2329156#M244397</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2026-03-09T17:02:15Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring P11 Expansion Connector Pin as GPIO on FRDM-IMX93 (VS Code)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-P11-Expansion-Connector-Pin-as-GPIO-on-FRDM-IMX93-VS/m-p/2331110#M244449</link>
      <description>&lt;DIV class=""&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;I reviewed the pin-func.h file and the device tree from the shared link. The pin GPIO2, which corresponds to header pin 3 on the expansion connector, appears to be free and is configured as a GPIO by default.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since this pin is defined in pin-func.h but not present in the device tree, I confirmed that Linux is not currently using it and that it should be available.&lt;/P&gt;&lt;P&gt;I configured this pin and attempted to write values 1 and 0, then read them back. However, the output always returns 0.&lt;/P&gt;&lt;P&gt;For your reference, I have attached the board configuration settings, the main.c code, and the output I am observing.&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#ifndef&lt;/SPAN&gt;&lt;SPAN&gt; _BOARD_USER_PINS_H_&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#define&lt;/SPAN&gt; &lt;SPAN&gt;_BOARD_USER_PINS_H_&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;/* --------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;* ADS1235 START pin mapping on FRDM‑i.MX93&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;* Pad &amp;nbsp;: GPIO_IO02&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;* GPIO : GPIO2_IO02&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;* --------------------------------------------------------------------------*/&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#define&lt;/SPAN&gt; &lt;SPAN&gt;ADS1235_START_GPIO&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;GPIO2&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#define&lt;/SPAN&gt; &lt;SPAN&gt;ADS1235_START_PIN&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;2U&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;void&lt;/SPAN&gt; &lt;SPAN&gt;BOARD_ConfigUserPins&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;void&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;void&lt;/SPAN&gt; &lt;SPAN&gt;BOARD_InitUserPins&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;void&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;#endif&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#include&lt;/SPAN&gt; &lt;SPAN&gt;"fsl_iomuxc.h"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#include&lt;/SPAN&gt; &lt;SPAN&gt;"board_user_pins.h"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#include&lt;/SPAN&gt; &lt;SPAN&gt;"fsl_rgpio.h"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;/*&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;* Configure user-specific pins that are NOT part of SDK pin tool&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;*/&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;void&lt;/SPAN&gt; &lt;SPAN&gt;BOARD_ConfigUserPins&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;void&lt;/SPAN&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; /* Configure GPIO_IO02 as GPIO2_IO02 (ADS1235 START pin) */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;IOMUXC_SetPinMux&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;IOMUXC_PAD_GPIO_IO02__GPIO2_IO02&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0U&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;IOMUXC_SetPinConfig&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;IOMUXC_PAD_GPIO_IO02__GPIO2_IO02&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;IOMUXC_PAD_DSE&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;15U&lt;/SPAN&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; /* Drive strength */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; );&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;/*&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;* Initialize user-specific pins that are NOT part of SDK pin tool&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;*/&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;void&lt;/SPAN&gt; &lt;SPAN&gt;BOARD_InitUserPins&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;void&lt;/SPAN&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;rgpio_pin_config_t&lt;/SPAN&gt; &lt;SPAN&gt;cfg&lt;/SPAN&gt; &lt;SPAN&gt;=&lt;/SPAN&gt;&lt;SPAN&gt; {&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; .&lt;/SPAN&gt;&lt;SPAN&gt;pinDirection&lt;/SPAN&gt; &lt;SPAN&gt;=&lt;/SPAN&gt; &lt;SPAN&gt;kRGPIO_DigitalOutput&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; .&lt;/SPAN&gt;&lt;SPAN&gt;outputLogic&lt;/SPAN&gt; &lt;SPAN&gt;=&lt;/SPAN&gt; &lt;SPAN&gt;0U&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;/* idle LOW */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; };&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;RGPIO_PinInit&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;ADS1235_START_GPIO&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;ADS1235_START_PIN&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;&amp;amp;&lt;/SPAN&gt;&lt;SPAN&gt;cfg&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;/*&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;* Copyright 2017 NXP&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;* All rights reserved.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;*&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;* SPDX-License-Identifier: BSD-3-Clause&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;*/&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;#include&lt;/SPAN&gt; &lt;SPAN&gt;"fsl_device_registers.h"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#include&lt;/SPAN&gt; &lt;SPAN&gt;"fsl_debug_console.h"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#include&lt;/SPAN&gt; &lt;SPAN&gt;"fsl_lpspi.h"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#include&lt;/SPAN&gt; &lt;SPAN&gt;"board.h"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#include&lt;/SPAN&gt; &lt;SPAN&gt;"app.h"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#include&lt;/SPAN&gt; &lt;SPAN&gt;"pin_mux.h"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#include&lt;/SPAN&gt; &lt;SPAN&gt;"clock_config.h"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#include&lt;/SPAN&gt; &lt;SPAN&gt;"fsl_rgpio.h"&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;// For DRDY if needed&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#include&lt;/SPAN&gt; &lt;SPAN&gt;"ads1235.h"&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;//ADS1235&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#include&lt;/SPAN&gt; &lt;SPAN&gt;"spi3.h"&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;//SPI3&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#include&lt;/SPAN&gt; &lt;SPAN&gt;"board_user_pins.h"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#include&lt;/SPAN&gt; &lt;SPAN&gt;"weighing.h"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;/*******************************************************************************&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;* Definitions&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;******************************************************************************/&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#define&lt;/SPAN&gt; &lt;SPAN&gt;TRANSFER_SIZE&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;3U&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; &amp;nbsp; /*! Transfer dataSize */ &amp;nbsp; &amp;nbsp; &amp;nbsp; //ADS1235 is a 24-bit ADC so 3 bytes&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#define&lt;/SPAN&gt; &lt;SPAN&gt;TRANSFER_BAUDRATE&lt;/SPAN&gt; &lt;SPAN&gt;500000U&lt;/SPAN&gt;&lt;SPAN&gt; /*! Transfer baudrate - 500k */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;/* SPI3 instance */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#define&lt;/SPAN&gt; &lt;SPAN&gt;EXAMPLE_LPSPI_MASTER_BASEADDR&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;LPSPI3&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#define&lt;/SPAN&gt; &lt;SPAN&gt;EXAMPLE_LPSPI_MASTER_PCS_FOR_INIT&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;kLPSPI_Pcs0&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;#define&lt;/SPAN&gt; &lt;SPAN&gt;EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER&lt;/SPAN&gt; &lt;SPAN&gt;kLPSPI_MasterPcs0&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;/*******************************************************************************&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;* Variables&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;******************************************************************************/&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;uint8_t&lt;/SPAN&gt; &lt;SPAN&gt;adcTxCmd&lt;/SPAN&gt;&lt;SPAN&gt;[&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;];&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;uint8_t&lt;/SPAN&gt; &lt;SPAN&gt;adcRxData&lt;/SPAN&gt;&lt;SPAN&gt;[&lt;/SPAN&gt;&lt;SPAN&gt;TRANSFER_SIZE&lt;/SPAN&gt;&lt;SPAN&gt;] &lt;/SPAN&gt;&lt;SPAN&gt;=&lt;/SPAN&gt;&lt;SPAN&gt; {&lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;};&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;uint8_t&lt;/SPAN&gt; &lt;SPAN&gt;masterRxData&lt;/SPAN&gt;&lt;SPAN&gt;[&lt;/SPAN&gt;&lt;SPAN&gt;TRANSFER_SIZE&lt;/SPAN&gt;&lt;SPAN&gt;] &lt;/SPAN&gt;&lt;SPAN&gt;=&lt;/SPAN&gt;&lt;SPAN&gt; {&lt;/SPAN&gt;&lt;SPAN&gt;0U&lt;/SPAN&gt;&lt;SPAN&gt;};&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;uint8_t&lt;/SPAN&gt; &lt;SPAN&gt;masterTxData&lt;/SPAN&gt;&lt;SPAN&gt;[&lt;/SPAN&gt;&lt;SPAN&gt;TRANSFER_SIZE&lt;/SPAN&gt;&lt;SPAN&gt;] &lt;/SPAN&gt;&lt;SPAN&gt;=&lt;/SPAN&gt;&lt;SPAN&gt; {&lt;/SPAN&gt;&lt;SPAN&gt;0U&lt;/SPAN&gt;&lt;SPAN&gt;};&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;/*******************************************************************************&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;* Main &lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;******************************************************************************/&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;int&lt;/SPAN&gt; &lt;SPAN&gt;main&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;void&lt;/SPAN&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;BOARD_InitBootPins&lt;/SPAN&gt;&lt;SPAN&gt;();&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; /* Initialize board pins */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;BOARD_InitBootClocks&lt;/SPAN&gt;&lt;SPAN&gt;();&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; /* Initialize clocks */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;BOARD_InitDebugConsole&lt;/SPAN&gt;&lt;SPAN&gt;();&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; /* Initialize debug UART */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;PRINTF&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;SPAN&gt;\r\n&lt;/SPAN&gt;&lt;SPAN&gt;ADS1235 SPI Test&lt;/SPAN&gt;&lt;SPAN&gt;\r\n&lt;/SPAN&gt;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;CLOCK_EnableClock&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;kCLOCK_Gpio1&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;BOARD_ConfigUserPins&lt;/SPAN&gt;&lt;SPAN&gt;();&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;BOARD_InitUserPins&lt;/SPAN&gt;&lt;SPAN&gt;();&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;SPI3_Init&lt;/SPAN&gt;&lt;SPAN&gt;();&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; &amp;nbsp; &amp;nbsp;// Your SPI init&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;uint8_t&lt;/SPAN&gt; &lt;SPAN&gt;tx&lt;/SPAN&gt;&lt;SPAN&gt;[&lt;/SPAN&gt;&lt;SPAN&gt;3&lt;/SPAN&gt;&lt;SPAN&gt;] &lt;/SPAN&gt;&lt;SPAN&gt;=&lt;/SPAN&gt;&lt;SPAN&gt; {&lt;/SPAN&gt;&lt;SPAN&gt;0xAA&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;SPAN&gt;0x55&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;SPAN&gt;0xFF&lt;/SPAN&gt;&lt;SPAN&gt;};&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;uint8_t&lt;/SPAN&gt; &lt;SPAN&gt;rx&lt;/SPAN&gt;&lt;SPAN&gt;[&lt;/SPAN&gt;&lt;SPAN&gt;3&lt;/SPAN&gt;&lt;SPAN&gt;] &lt;/SPAN&gt;&lt;SPAN&gt;=&lt;/SPAN&gt;&lt;SPAN&gt; {&lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;};&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;lpspi_transfer_t&lt;/SPAN&gt; &lt;SPAN&gt;transfer&lt;/SPAN&gt;&lt;SPAN&gt;;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;transfer&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;SPAN&gt;txData&lt;/SPAN&gt; &lt;SPAN&gt;=&lt;/SPAN&gt; &lt;SPAN&gt;tx&lt;/SPAN&gt;&lt;SPAN&gt;;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;transfer&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;SPAN&gt;rxData&lt;/SPAN&gt; &lt;SPAN&gt;=&lt;/SPAN&gt; &lt;SPAN&gt;rx&lt;/SPAN&gt;&lt;SPAN&gt;;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;transfer&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;SPAN&gt;dataSize&lt;/SPAN&gt; &lt;SPAN&gt;=&lt;/SPAN&gt; &lt;SPAN&gt;3&lt;/SPAN&gt;&lt;SPAN&gt;;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;transfer&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;SPAN&gt;configFlags&lt;/SPAN&gt; &lt;SPAN&gt;=&lt;/SPAN&gt; &lt;SPAN&gt;kLPSPI_MasterPcs0&lt;/SPAN&gt;&lt;SPAN&gt;;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;LPSPI_MasterTransferBlocking&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;LPSPI3&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;&amp;amp;&lt;/SPAN&gt;&lt;SPAN&gt;transfer&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;PRINTF&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;"SPI TEST RX: &lt;/SPAN&gt;&lt;SPAN&gt;%02X&lt;/SPAN&gt; &lt;SPAN&gt;%02X&lt;/SPAN&gt; &lt;SPAN&gt;%02X&lt;/SPAN&gt;&lt;SPAN&gt;\r\n&lt;/SPAN&gt;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;rx&lt;/SPAN&gt;&lt;SPAN&gt;[&lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;], &lt;/SPAN&gt;&lt;SPAN&gt;rx&lt;/SPAN&gt;&lt;SPAN&gt;[&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;], &lt;/SPAN&gt;&lt;SPAN&gt;rx&lt;/SPAN&gt;&lt;SPAN&gt;[&lt;/SPAN&gt;&lt;SPAN&gt;2&lt;/SPAN&gt;&lt;SPAN&gt;]);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;while&lt;/SPAN&gt;&lt;SPAN&gt; (&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; { &amp;nbsp; &lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; /* Write HIGH */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;RGPIO_PinWrite&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;ADS1235_START_GPIO&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;ADS1235_START_PIN&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;1U&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;PRINTF&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;"START pin state (HIGH): &lt;/SPAN&gt;&lt;SPAN&gt;%d&lt;/SPAN&gt;&lt;SPAN&gt;\r\n&lt;/SPAN&gt;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;RGPIO_PinRead&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;ADS1235_START_GPIO&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;ADS1235_START_PIN&lt;/SPAN&gt;&lt;SPAN&gt;));&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;SDK_DelayAtLeastUs&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;500000&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;SystemCoreClock&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; /* Write LOW */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;RGPIO_PinWrite&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;ADS1235_START_GPIO&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;ADS1235_START_PIN&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0U&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;PRINTF&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;"START pin state (LOW): &lt;/SPAN&gt;&lt;SPAN&gt;%d&lt;/SPAN&gt;&lt;SPAN&gt;\r\n&lt;/SPAN&gt;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;RGPIO_PinRead&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;ADS1235_START_GPIO&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;ADS1235_START_PIN&lt;/SPAN&gt;&lt;SPAN&gt;));&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;SDK_DelayAtLeastUs&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;500000&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;SystemCoreClock&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; }&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Mar 2026 07:31:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configuring-P11-Expansion-Connector-Pin-as-GPIO-on-FRDM-IMX93-VS/m-p/2331110#M244449</guid>
      <dc:creator>Shanmugapriya</dc:creator>
      <dc:date>2026-03-12T07:31:08Z</dc:date>
    </item>
  </channel>
</rss>