<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX8-QM SCFW</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-QM-SCFW/m-p/2328172#M244358</link>
    <description>&lt;P&gt;Hi, i mean when i use your bsp layer the atf is build automatically without getting modified depending on my use case.how do i verify and load the next stage(bl32 or bl33) if i m not passing some arguments to the build (like load adress) or is this done by the atf auto by reading the container header?&lt;/P&gt;</description>
    <pubDate>Sat, 07 Mar 2026 08:21:07 GMT</pubDate>
    <dc:creator>anas-8888</dc:creator>
    <dc:date>2026-03-07T08:21:07Z</dc:date>
    <item>
      <title>IMX8-QM SCFW</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-QM-SCFW/m-p/2327822#M244348</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;so im working on imx8qm secure boot and my question is how to know the load adress of the next stage(ATF) used inside the firmware if its already prebuilt?&lt;/P&gt;</description>
      <pubDate>Fri, 06 Mar 2026 10:18:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-QM-SCFW/m-p/2327822#M244348</guid>
      <dc:creator>anas-8888</dc:creator>
      <dc:date>2026-03-06T10:18:46Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8-QM SCFW</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-QM-SCFW/m-p/2328158#M244356</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;What do you mean by prebuilt?&lt;BR /&gt;Please note that you may build your atf (bl31) and use it for your image.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Sat, 07 Mar 2026 02:35:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-QM-SCFW/m-p/2328158#M244356</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2026-03-07T02:35:56Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8-QM SCFW</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-QM-SCFW/m-p/2328172#M244358</link>
      <description>&lt;P&gt;Hi, i mean when i use your bsp layer the atf is build automatically without getting modified depending on my use case.how do i verify and load the next stage(bl32 or bl33) if i m not passing some arguments to the build (like load adress) or is this done by the atf auto by reading the container header?&lt;/P&gt;</description>
      <pubDate>Sat, 07 Mar 2026 08:21:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-QM-SCFW/m-p/2328172#M244358</guid>
      <dc:creator>anas-8888</dc:creator>
      <dc:date>2026-03-07T08:21:07Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8-QM SCFW</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-QM-SCFW/m-p/2329215#M244398</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Thank you for the clarification, so I believe that you are refering to yocto build, then yes, ATF source is downloaded and built.&lt;BR /&gt;&lt;BR /&gt;Also, yes you are correct each image has its own data structure (header) with information on: ​&lt;BR /&gt;The location of the image​&lt;BR /&gt;Size of the image​&lt;BR /&gt;Destination address​&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Mon, 09 Mar 2026 18:48:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-QM-SCFW/m-p/2329215#M244398</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2026-03-09T18:48:28Z</dc:date>
    </item>
  </channel>
</rss>