<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックflexbuild for imx8mpevk: Modifying u-boot and kernel sources</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/flexbuild-for-imx8mpevk-Modifying-u-boot-and-kernel-sources/m-p/2324318#M244215</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm struggling to understand the correct workflow for modifying u-boot/kernel using your flexbuild project.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Bord: based on imx8mpevk&lt;/P&gt;&lt;P&gt;flexbuild version: LSDK-25.06_Debian-12_LF-6.6.52&lt;/P&gt;&lt;P&gt;I can build a bootable image by running $bld -m imx8mpevk and the creating the .wic file using flex-installer that is located in the build/images/ directory.&lt;BR /&gt;&lt;BR /&gt;But when I modify u-boot my changes are not included and i can see on the timestamps that it is not re-built properly.&lt;BR /&gt;&lt;BR /&gt;I followed the instructions on:&lt;BR /&gt;&lt;A href="https://docs.nxp.com/bundle/UG10155/page/topics/how_to_modify_and_recompile_source_code.html" target="_blank"&gt;https://docs.nxp.com/bundle/UG10155/page/topics/how_to_modify_and_recompile_source_code.html&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;cd components_lsd2506/bsp/uboot&lt;BR /&gt;make imx8mp_evk_defconfig&lt;BR /&gt;make menuconfig &amp;lt;-- add some change&amp;nbsp;&lt;BR /&gt;make savedefconfig&lt;BR /&gt;cp defconfig configs/imx8mp_evk_defconfig&lt;BR /&gt;cd -&lt;BR /&gt;bld atf -m imx8mpevk -b sd&lt;BR /&gt;bld uboot -m imx8mpevk&lt;BR /&gt;bld boot -m imx8mpevk&lt;BR /&gt;&lt;BR /&gt;everything compiles without any issues but the u-boot shipped will be the one that i built initially, not the modified version.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also tried running bld clean-bsp before attempting to rebuild uboot but that did not seem to help.&lt;BR /&gt;&lt;BR /&gt;Thankful for any tips/insights!&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Willie&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 27 Feb 2026 10:05:02 GMT</pubDate>
    <dc:creator>wonkan123</dc:creator>
    <dc:date>2026-02-27T10:05:02Z</dc:date>
    <item>
      <title>flexbuild for imx8mpevk: Modifying u-boot and kernel sources</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/flexbuild-for-imx8mpevk-Modifying-u-boot-and-kernel-sources/m-p/2324318#M244215</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm struggling to understand the correct workflow for modifying u-boot/kernel using your flexbuild project.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Bord: based on imx8mpevk&lt;/P&gt;&lt;P&gt;flexbuild version: LSDK-25.06_Debian-12_LF-6.6.52&lt;/P&gt;&lt;P&gt;I can build a bootable image by running $bld -m imx8mpevk and the creating the .wic file using flex-installer that is located in the build/images/ directory.&lt;BR /&gt;&lt;BR /&gt;But when I modify u-boot my changes are not included and i can see on the timestamps that it is not re-built properly.&lt;BR /&gt;&lt;BR /&gt;I followed the instructions on:&lt;BR /&gt;&lt;A href="https://docs.nxp.com/bundle/UG10155/page/topics/how_to_modify_and_recompile_source_code.html" target="_blank"&gt;https://docs.nxp.com/bundle/UG10155/page/topics/how_to_modify_and_recompile_source_code.html&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;cd components_lsd2506/bsp/uboot&lt;BR /&gt;make imx8mp_evk_defconfig&lt;BR /&gt;make menuconfig &amp;lt;-- add some change&amp;nbsp;&lt;BR /&gt;make savedefconfig&lt;BR /&gt;cp defconfig configs/imx8mp_evk_defconfig&lt;BR /&gt;cd -&lt;BR /&gt;bld atf -m imx8mpevk -b sd&lt;BR /&gt;bld uboot -m imx8mpevk&lt;BR /&gt;bld boot -m imx8mpevk&lt;BR /&gt;&lt;BR /&gt;everything compiles without any issues but the u-boot shipped will be the one that i built initially, not the modified version.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also tried running bld clean-bsp before attempting to rebuild uboot but that did not seem to help.&lt;BR /&gt;&lt;BR /&gt;Thankful for any tips/insights!&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Willie&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Feb 2026 10:05:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/flexbuild-for-imx8mpevk-Modifying-u-boot-and-kernel-sources/m-p/2324318#M244215</guid>
      <dc:creator>wonkan123</dc:creator>
      <dc:date>2026-02-27T10:05:02Z</dc:date>
    </item>
    <item>
      <title>Re: flexbuild for imx8mpevk: Modifying u-boot and kernel sources</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/flexbuild-for-imx8mpevk-Modifying-u-boot-and-kernel-sources/m-p/2324600#M244220</link>
      <description>&lt;P&gt;Please refer to the following procedure to rebuild u-boot.&lt;/P&gt;
&lt;P&gt;cd components_lsd2506/bsp/uboot&lt;BR /&gt;make imx8mp_evk_defconfig&lt;BR /&gt;make menuconfig &amp;lt;-- add some change&amp;nbsp;&lt;BR /&gt;make savedefconfig&lt;BR /&gt;cp defconfig configs/imx8mp_evk_defconfig&lt;/P&gt;
&lt;P&gt;make distclean&lt;BR /&gt;cd –&lt;/P&gt;
&lt;P&gt;bld uboot -m imx8mpevk&lt;BR /&gt;bld atf -m imx8mpevk -b sd&lt;BR /&gt;bld &amp;nbsp;bsp -m mx8mpevk&lt;/P&gt;</description>
      <pubDate>Sat, 28 Feb 2026 07:27:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/flexbuild-for-imx8mpevk-Modifying-u-boot-and-kernel-sources/m-p/2324600#M244220</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2026-02-28T07:27:45Z</dc:date>
    </item>
  </channel>
</rss>