<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: No display on SabreSD imx6 with u boot configuration in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255792#M24413</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, LVDS screen is connected into LVDS1.&lt;/P&gt;&lt;P&gt;(I already tested video=mxcfb1:dev=ldb... video=mxcfb0:off ...)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Apr 2013 06:57:23 GMT</pubDate>
    <dc:creator>jbd64</dc:creator>
    <dc:date>2013-04-09T06:57:23Z</dc:date>
    <item>
      <title>No display on SabreSD imx6 with u boot configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255787#M24408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi eveyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to configure u-boot in order to enable display on my IMX6 SABRE SD.&lt;/P&gt;&lt;P&gt;Screen is a HannStar LVDS : 1024x768 i.e. LDB-XGA, RGB666&lt;/P&gt;&lt;P&gt;I've tried tons of u-boot config, with no success.&lt;/P&gt;&lt;P&gt;I've an SD Card already configured with an Android r13.4, and the screen works well with this boot.&lt;/P&gt;&lt;P&gt;For information, when my Ubuntu has finished starting, I type 'echo 0 &amp;gt; /sys/class/graphics/fbX/blank' and 4 or 5 penguin is displayed (normally displayed when booting) instead of Ubuntu GUI&lt;/P&gt;&lt;P&gt;Here is my u-boot config : &lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;MX6Q SABRESD U-Boot &amp;gt; printenv&lt;/P&gt;&lt;P&gt;bootdelay=3&lt;/P&gt;&lt;P&gt;baudrate=115200&lt;/P&gt;&lt;P&gt;ipaddr=192.168.1.103&lt;/P&gt;&lt;P&gt;serverip=192.168.1.101&lt;/P&gt;&lt;P&gt;netmask=255.255.255.0&lt;/P&gt;&lt;P&gt;loadaddr=0x10800000&lt;/P&gt;&lt;P&gt;rd_loadaddr=(0x1300000)&lt;/P&gt;&lt;P&gt;netdev=eth0&lt;/P&gt;&lt;P&gt;ethprime=FEC0&lt;/P&gt;&lt;P&gt;uboot=u-boot.bin&lt;/P&gt;&lt;P&gt;kernel=uImage&lt;/P&gt;&lt;P&gt;nfsroot=/opt/eldk/arm&lt;/P&gt;&lt;P&gt;bootargs_base=setenv bootargs console=ttymxc0,115200&lt;/P&gt;&lt;P&gt;bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp&lt;/P&gt;&lt;P&gt;bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; bootm&lt;/P&gt;&lt;P&gt;bootcmd_mmc=run bootargs_base bootargs_mmc; mmc dev 3; mmc read ${loadaddr} 0x800 0x2000; bootm&lt;/P&gt;&lt;P&gt;ethact=FEC0&lt;/P&gt;&lt;P&gt;bootcmd=run bootcmd_mmc&lt;/P&gt;&lt;P&gt;stdin=serial&lt;/P&gt;&lt;P&gt;stdout=serial&lt;/P&gt;&lt;P&gt;stderr=serial&lt;/P&gt;&lt;P&gt;bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Environment size: 738/8188 bytes&lt;/P&gt;&lt;P&gt;MX6Q SABRESD U-Boot &amp;gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is my kernel log boot : &lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;MX6Q SABRESD U-Boot &amp;gt; run bootcmd&lt;/P&gt;&lt;P&gt;mmc3(part 0) is current device&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MMC read: dev # 3, block # 2048, count 8192 ... 8192 blocks read: OK&lt;/P&gt;&lt;P&gt;## Booting kernel from Legacy Image at 10800000 ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; Linux-3.0.35-2310-gc27cb38&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; ARM Linux Kernel Image (uncompressed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 3851244 Bytes =&amp;nbsp; 3.7 MB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Load Address: 10008000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 10008000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Loading Kernel Image ... OK&lt;/P&gt;&lt;P&gt;OK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Uncompressing Linux... done, booting the kernel.&lt;/P&gt;&lt;P&gt;Linux version 3.0.35-2310-gc27cb38 (r65388@shlinux3) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #1 SMP PREEMPT Tue Dec 18 17:23:15 CST 2012&lt;/P&gt;&lt;P&gt;CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d&lt;/P&gt;&lt;P&gt;CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;/P&gt;&lt;P&gt;Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board&lt;/P&gt;&lt;P&gt;Ignoring unrecognised tag 0x54410008&lt;/P&gt;&lt;P&gt;Memory policy: ECC disabled, Data cache writealloc&lt;/P&gt;&lt;P&gt;CPU identified as i.MX6Q, silicon rev 1.2&lt;/P&gt;&lt;P&gt;PERCPU: Embedded 7 pages/cpu @8c008000 s5440 r8192 d15040 u32768&lt;/P&gt;&lt;P&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 227328&lt;/P&gt;&lt;P&gt;Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666&lt;/P&gt;&lt;P&gt;PID hash table entries: 4096 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)&lt;/P&gt;&lt;P&gt;Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;/P&gt;&lt;P&gt;Memory: 640MB 256MB = 896MB total&lt;/P&gt;&lt;P&gt;Memory: 896880k/896880k available, 151696k reserved, 0K highmem&lt;/P&gt;&lt;P&gt;Virtual kernel memory layout:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vector&amp;nbsp; : 0xffff0000 - 0xffff1000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 4 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fixmap&amp;nbsp; : 0xfff00000 - 0xfffe0000&amp;nbsp;&amp;nbsp; ( 896 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0xf4600000 - 0xffe00000&amp;nbsp;&amp;nbsp; ( 184 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vmalloc : 0xc0800000 - 0xf2000000&amp;nbsp;&amp;nbsp; ( 792 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; lowmem&amp;nbsp; : 0x80000000 - 0xc0000000&amp;nbsp;&amp;nbsp; (1024 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pkmap&amp;nbsp;&amp;nbsp; : 0x7fe00000 - 0x80000000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 2 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; modules : 0x7f000000 - 0x7fe00000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 14 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .init : 0x80008000 - 0x8003b000&amp;nbsp;&amp;nbsp; ( 204 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .text : 0x8003b000 - 0x80a886d0&amp;nbsp;&amp;nbsp; (10550 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0x80a8a000 - 0x80ae8a40&amp;nbsp;&amp;nbsp; ( 379 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .bss : 0x80ae8a64 - 0x80b368ec&amp;nbsp;&amp;nbsp; ( 312 kB)&lt;/P&gt;&lt;P&gt;SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=4, Nodes=1&lt;/P&gt;&lt;P&gt;Preemptible hierarchical RCU implementation.&lt;/P&gt;&lt;P&gt;NR_IRQS:496&lt;/P&gt;&lt;P&gt;MXC GPIO hardware&lt;/P&gt;&lt;P&gt;sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms&lt;/P&gt;&lt;P&gt;arm_max_freq=2&lt;/P&gt;&lt;P&gt;MXC_Early serial console at MMIO 0x2020000 (options '115200')&lt;/P&gt;&lt;P&gt;bootconsole [ttymxc0] enabled&lt;/P&gt;&lt;P&gt;Console: colour dummy device 80x30&lt;/P&gt;&lt;P&gt;Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)&lt;/P&gt;&lt;P&gt;pid_max: default: 32768 minimum: 301&lt;/P&gt;&lt;P&gt;Mount-cache hash table entries: 512&lt;/P&gt;&lt;P&gt;CPU: Testing write buffer coherency: ok&lt;/P&gt;&lt;P&gt;hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available&lt;/P&gt;&lt;P&gt;CPU1: Booted secondary processor&lt;/P&gt;&lt;P&gt;CPU2: Booted secondary processor&lt;/P&gt;&lt;P&gt;CPU3: Booted secondary processor&lt;/P&gt;&lt;P&gt;Brought up 4 CPUs&lt;/P&gt;&lt;P&gt;SMP: Total of 4 processors activated (6324.22 BogoMIPS).&lt;/P&gt;&lt;P&gt;print_constraints: dummy:&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 16&lt;/P&gt;&lt;P&gt;print_constraints: vddpu: 725 &amp;lt;--&amp;gt; 1300 mV at 700 mV fast normal&lt;/P&gt;&lt;P&gt;print_constraints: vddcore: 725 &amp;lt;--&amp;gt; 1300 mV at 1100 mV fast normal&lt;/P&gt;&lt;P&gt;print_constraints: vddsoc: 725 &amp;lt;--&amp;gt; 1300 mV at 1200 mV fast normal&lt;/P&gt;&lt;P&gt;print_constraints: vdd2p5: 2000 &amp;lt;--&amp;gt; 2775 mV at 2400 mV fast normal&lt;/P&gt;&lt;P&gt;print_constraints: vdd1p1: 800 &amp;lt;--&amp;gt; 1400 mV at 1100 mV fast normal&lt;/P&gt;&lt;P&gt;print_constraints: vdd3p0: 2625 &amp;lt;--&amp;gt; 3400 mV at 3000 mV fast normal&lt;/P&gt;&lt;P&gt;hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.&lt;/P&gt;&lt;P&gt;hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.&lt;/P&gt;&lt;P&gt;hw-breakpoint: maximum watchpoint size is 4 bytes.&lt;/P&gt;&lt;P&gt;L310 cache controller enabled&lt;/P&gt;&lt;P&gt;l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B&lt;/P&gt;&lt;P&gt;bio: create slab &amp;lt;bio-0&amp;gt; at 0&lt;/P&gt;&lt;P&gt;mxs-dma mxs-dma-apbh: initialized&lt;/P&gt;&lt;P&gt;print_constraints: SPKVDD: 4200 mV&lt;/P&gt;&lt;P&gt;print_constraints: vmmc: 3300 mV&lt;/P&gt;&lt;P&gt;SCSI subsystem initialized&lt;/P&gt;&lt;P&gt;spi_imx imx6q-ecspi.0: probed&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usbfs&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver hub&lt;/P&gt;&lt;P&gt;usbcore: registered new device driver usb&lt;/P&gt;&lt;P&gt;Freescale USB OTG Driver loaded, $Revision: 1.55 $&lt;/P&gt;&lt;P&gt;mc_pfuze 1-0008: ID: 0,Full lay: 1 ,Metal lay: 1&lt;/P&gt;&lt;P&gt;mc_pfuze 1-0008: FAB: 0 ,FIN: 0&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_SW1A: 300 &amp;lt;--&amp;gt; 1875 mV at 1300 mV&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_SW1B: 300 &amp;lt;--&amp;gt; 1875 mV at 300 mV&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_SW1C: 300 &amp;lt;--&amp;gt; 1875 mV at 1300 mV&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_SW2: 800 &amp;lt;--&amp;gt; 3950 mV at 3300 mV&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_SW3A: 400 &amp;lt;--&amp;gt; 1975 mV at 1500 mV&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_SW3B: 400 &amp;lt;--&amp;gt; 1975 mV at 1500 mV&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_SW4: 800 &amp;lt;--&amp;gt; 3950 mV at 3150 mV&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_SWBST: 5000 &amp;lt;--&amp;gt; 5150 mV at 5000 mV&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_VSNVS: 1200 &amp;lt;--&amp;gt; 3000 mV at 1800 mV&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_VREFDDR: at 750 mV&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_VGEN1: 800 &amp;lt;--&amp;gt; 1550 mV at 1500 mV&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_VGEN2: 800 &amp;lt;--&amp;gt; 1550 mV at 1500 mV&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_VGEN3: 1800 &amp;lt;--&amp;gt; 3300 mV at 2800 mV&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_VGEN4: 1800 &amp;lt;--&amp;gt; 3300 mV at 1800 mV&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_VGEN5: 1800 &amp;lt;--&amp;gt; 3300 mV at 3000 mV&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_VGEN6: 1800 &amp;lt;--&amp;gt; 3300 mV at 3300 mV&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)&lt;/P&gt;&lt;P&gt;mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed&lt;/P&gt;&lt;P&gt;mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a&lt;/P&gt;&lt;P&gt;MIPI CSI2 driver module loaded&lt;/P&gt;&lt;P&gt;Advanced Linux Sound Architecture Driver Version 1.0.24.&lt;/P&gt;&lt;P&gt;Bluetooth: Core ver 2.16&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 31&lt;/P&gt;&lt;P&gt;Bluetooth: HCI device and connection manager initialized&lt;/P&gt;&lt;P&gt;Bluetooth: HCI socket layer initialized&lt;/P&gt;&lt;P&gt;Bluetooth: L2CAP socket layer initialized&lt;/P&gt;&lt;P&gt;Bluetooth: SCO socket layer initialized&lt;/P&gt;&lt;P&gt;cfg80211: Calling CRDA to update world regulatory domain&lt;/P&gt;&lt;P&gt;max17135 2-0048: PMIC MAX17135 for eInk display&lt;/P&gt;&lt;P&gt;i2c-core: driver [max17135] using legacy suspend method&lt;/P&gt;&lt;P&gt;i2c-core: driver [max17135] using legacy resume method&lt;/P&gt;&lt;P&gt;Switching to clocksource mxc_timer1&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 2&lt;/P&gt;&lt;P&gt;IP route cache hash table entries: 32768 (order: 5, 131072 bytes)&lt;/P&gt;&lt;P&gt;TCP established hash table entries: 131072 (order: 8, 1048576 bytes)&lt;/P&gt;&lt;P&gt;TCP bind hash table entries: 65536 (order: 7, 786432 bytes)&lt;/P&gt;&lt;P&gt;TCP: Hash tables configured (established 131072 bind 65536)&lt;/P&gt;&lt;P&gt;TCP reno registered&lt;/P&gt;&lt;P&gt;UDP hash table entries: 512 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 1&lt;/P&gt;&lt;P&gt;RPC: Registered named UNIX socket transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered udp transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered tcp transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;/P&gt;&lt;P&gt;PMU: registered new PMU device of type 0&lt;/P&gt;&lt;P&gt;Static Power Management for Freescale i.MX6&lt;/P&gt;&lt;P&gt;wait mode is enabled for i.MX6&lt;/P&gt;&lt;P&gt;cpaddr = c0880000 suspend_iram_base=c091c000&lt;/P&gt;&lt;P&gt;PM driver module loaded&lt;/P&gt;&lt;P&gt;IMX usb wakeup probe&lt;/P&gt;&lt;P&gt;add wake up source irq 75&lt;/P&gt;&lt;P&gt;IMX usb wakeup probe&lt;/P&gt;&lt;P&gt;cpu regulator init ldo=1&lt;/P&gt;&lt;P&gt;_regulator_get: get() with no identifier&lt;/P&gt;&lt;P&gt;mx6_cpu_regulator_init: failed to get pu regulator&lt;/P&gt;&lt;P&gt;i.MXC CPU frequency driver&lt;/P&gt;&lt;P&gt;JFFS2 version 2.2. (NAND) Â© 2001-2006 Red Hat, Inc.&lt;/P&gt;&lt;P&gt;msgmni has been set to 1751&lt;/P&gt;&lt;P&gt;alg: No test for stdrng (krng)&lt;/P&gt;&lt;P&gt;io scheduler noop registered&lt;/P&gt;&lt;P&gt;io scheduler deadline registered&lt;/P&gt;&lt;P&gt;io scheduler cfq registered (default)&lt;/P&gt;&lt;P&gt;mxc_mipi_dsi mxc_mipi_dsi: i.MX MIPI DSI driver probed&lt;/P&gt;&lt;P&gt;MIPI DSI driver module loaded&lt;/P&gt;&lt;P&gt;mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb&lt;/P&gt;&lt;P&gt;_regulator_get: get() with no identifier&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)&lt;/P&gt;&lt;P&gt;Console: switching to colour frame buffer device 128x48&lt;/P&gt;&lt;P&gt;mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver ldb&lt;/P&gt;&lt;P&gt;mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver lcd&lt;/P&gt;&lt;P&gt;mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb&lt;/P&gt;&lt;P&gt;mxc_sdc_fb mxc_sdc_fb.3: ipu1-di1 already in use&lt;/P&gt;&lt;P&gt;mxc_sdc_fb: probe of mxc_sdc_fb.3 failed with error -16&lt;/P&gt;&lt;P&gt;imx-sdma imx-sdma: loaded firmware 1.1&lt;/P&gt;&lt;P&gt;imx-sdma imx-sdma: initialized&lt;/P&gt;&lt;P&gt;Serial: IMX driver&lt;/P&gt;&lt;P&gt;imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX&lt;/P&gt;&lt;P&gt;imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX&lt;/P&gt;&lt;P&gt;console [ttymxc0] enabled, bootconsole disabled&lt;/P&gt;&lt;P&gt;console [ttymxc0] enabled, bootconsole disabled&lt;/P&gt;&lt;P&gt;loop: module loaded&lt;/P&gt;&lt;P&gt;Can't recover from RESET HBA!&lt;/P&gt;&lt;P&gt;No sata disk.&lt;/P&gt;&lt;P&gt;m25p80 spi0.0: found m25p32, expected sst25vf016b&lt;/P&gt;&lt;P&gt;m25p80 spi0.0: m25p32 (4096 Kbytes)&lt;/P&gt;&lt;P&gt;Creating 2 MTD partitions on "m25p80":&lt;/P&gt;&lt;P&gt;0x000000000000-0x000000100000 : "bootloader"&lt;/P&gt;&lt;P&gt;0x000000100000-0x000000400000 : "kernel"&lt;/P&gt;&lt;P&gt;GPMI NAND driver registered. (IMX)&lt;/P&gt;&lt;P&gt;vcan: Virtual CAN interface driver&lt;/P&gt;&lt;P&gt;CAN device driver interface&lt;/P&gt;&lt;P&gt;flexcan netdevice driver&lt;/P&gt;&lt;P&gt;FEC Ethernet Driver&lt;/P&gt;&lt;P&gt;fec_enet_mii_bus: probed&lt;/P&gt;&lt;P&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00&lt;/P&gt;&lt;P&gt;hub 1-0:1.0: USB hub found&lt;/P&gt;&lt;P&gt;hub 1-0:1.0: 1 port detected&lt;/P&gt;&lt;P&gt;add wake up source irq 72&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00&lt;/P&gt;&lt;P&gt;hub 2-0:1.0: USB hub found&lt;/P&gt;&lt;P&gt;hub 2-0:1.0: 1 port detected&lt;/P&gt;&lt;P&gt;Initializing USB Mass Storage driver...&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usb-storage&lt;/P&gt;&lt;P&gt;USB Mass Storage support registered.&lt;/P&gt;&lt;P&gt;ARC USBOTG Device Controller driver (1 August 2005)&lt;/P&gt;&lt;P&gt;mousedev: PS/2 mouse device common for all mice&lt;/P&gt;&lt;P&gt;input: gpio-keys as /devices/platform/gpio-keys/input/input0&lt;/P&gt;&lt;P&gt;input: max11801_ts as /devices/platform/imx-i2c.1/i2c-1/1-0048/input/input1&lt;/P&gt;&lt;P&gt;egalax_ts 1-0004: egalax_ts: failed to read firmware version&lt;/P&gt;&lt;P&gt;egalax_ts: probe of 1-0004 failed with error -5&lt;/P&gt;&lt;P&gt;input: eGalax Touch Screen as /devices/platform/imx-i2c.2/i2c-2/2-0004/input/input2&lt;/P&gt;&lt;P&gt;elan - Read Hello Packet Failed&lt;/P&gt;&lt;P&gt;elan-touch: probe of 2-0010 failed with error -22&lt;/P&gt;&lt;P&gt;input: isl29023 light sensor as /devices/virtual/input/input3&lt;/P&gt;&lt;P&gt;isl29023 2-0044: driver version 1.0 enabled&lt;/P&gt;&lt;P&gt;i2c-core: driver [isl29023] using legacy suspend method&lt;/P&gt;&lt;P&gt;i2c-core: driver [isl29023] using legacy resume method&lt;/P&gt;&lt;P&gt;snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0&lt;/P&gt;&lt;P&gt;i2c /dev entries driver&lt;/P&gt;&lt;P&gt;Linux video capture interface: v2.00&lt;/P&gt;&lt;P&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16&lt;/P&gt;&lt;P&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17&lt;/P&gt;&lt;P&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18&lt;/P&gt;&lt;P&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19&lt;/P&gt;&lt;P&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20&lt;/P&gt;&lt;P&gt;mag3110 2-000e: check mag3110 chip ID&lt;/P&gt;&lt;P&gt;input: mag3110 as /devices/virtual/input/input4&lt;/P&gt;&lt;P&gt;mag3110 2-000e: mag3110 is probed&lt;/P&gt;&lt;P&gt;i2c-core: driver [mag3110] using legacy suspend method&lt;/P&gt;&lt;P&gt;i2c-core: driver [mag3110] using legacy resume method&lt;/P&gt;&lt;P&gt;input: mma845x as /devices/virtual/input/input5&lt;/P&gt;&lt;P&gt;imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)&lt;/P&gt;&lt;P&gt;Bluetooth: Virtual HCI driver ver 1.3&lt;/P&gt;&lt;P&gt;Bluetooth: HCI UART driver ver 2.2&lt;/P&gt;&lt;P&gt;Bluetooth: HCIATH3K protocol initialized&lt;/P&gt;&lt;P&gt;Bluetooth: Generic Bluetooth USB driver ver 0.6&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver btusb&lt;/P&gt;&lt;P&gt;sdhci: Secure Digital Host Controller Interface driver&lt;/P&gt;&lt;P&gt;sdhci: Copyright(c) Pierre Ossman&lt;/P&gt;&lt;P&gt;mmc0: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA&lt;/P&gt;&lt;P&gt;mmc1: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA&lt;/P&gt;&lt;P&gt;mmc2: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA&lt;/P&gt;&lt;P&gt;mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed&lt;/P&gt;&lt;P&gt;VPU initialized&lt;/P&gt;&lt;P&gt;mxc_asrc registered&lt;/P&gt;&lt;P&gt;Thermal calibration data is 0x56f4b67d&lt;/P&gt;&lt;P&gt;Anatop Thermal registered as thermal_zone0&lt;/P&gt;&lt;P&gt;anatop_thermal_probe: default cooling device is cpufreq!&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usbhid&lt;/P&gt;&lt;P&gt;usbhid: USB HID core driver&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver snd-usb-audio&lt;/P&gt;&lt;P&gt;mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio&lt;/P&gt;&lt;P&gt;Cirrus Logic CS42888 ALSA SoC Codec Driver&lt;/P&gt;&lt;P&gt;i2c-core: driver [cs42888] using legacy suspend method&lt;/P&gt;&lt;P&gt;i2c-core: driver [cs42888] using legacy resume method&lt;/P&gt;&lt;P&gt;imx-hdmi-soc-dai: probe of imx-hdmi-soc-dai.0 failed with error -12&lt;/P&gt;&lt;P&gt;mmc0: new high speed DDR MMC card at address 0001&lt;/P&gt;&lt;P&gt;mmcblk0: mmc0:0001 SEM08G 7.39 GiB&lt;/P&gt;&lt;P&gt;mmcblk0boot0: mmc0:0001 SEM08G partition 1 2.00 MiB&lt;/P&gt;&lt;P&gt;mmcblk0boot1: mmc0:0001 SEM08G partition 2 2.00 MiB&lt;/P&gt;&lt;P&gt; mmcblk0: p1&lt;/P&gt;&lt;P&gt; mmcblk0boot1: unknown partition table&lt;/P&gt;&lt;P&gt; mmcblk0boot0: unknown partition table&lt;/P&gt;&lt;P&gt;wm8962 0-001a: customer id 0 revision D&lt;/P&gt;&lt;P&gt;input: WM8962 Beep Generator as /devices/platform/imx-i2c.0/i2c-0/0-001a/input/input6&lt;/P&gt;&lt;P&gt;asoc: wm8962 &amp;lt;-&amp;gt; imx-ssi.1 mapping ok&lt;/P&gt;&lt;P&gt;imx_3stack asoc driver&lt;/P&gt;&lt;P&gt;ALSA device list:&lt;/P&gt;&lt;P&gt;&amp;nbsp; #0: wm8962-audio&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 26&lt;/P&gt;&lt;P&gt;TCP cubic registered&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 17&lt;/P&gt;&lt;P&gt;can: controller area network core (rev 20090105 abi 8)&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 29&lt;/P&gt;&lt;P&gt;can: raw protocol (rev 20090105)&lt;/P&gt;&lt;P&gt;can: broadcast manager protocol (rev 20090105 t)&lt;/P&gt;&lt;P&gt;Bluetooth: RFCOMM TTY layer initialized&lt;/P&gt;&lt;P&gt;Bluetooth: RFCOMM socket layer initialized&lt;/P&gt;&lt;P&gt;Bluetooth: RFCOMM ver 1.11&lt;/P&gt;&lt;P&gt;Bluetooth: BNEP (Ethernet Emulation) ver 1.3&lt;/P&gt;&lt;P&gt;Bluetooth: BNEP filters: protocol multicast&lt;/P&gt;&lt;P&gt;Bluetooth: HIDP (Human Interface Emulation) ver 1.2&lt;/P&gt;&lt;P&gt;lib80211: common routines for IEEE802.11 drivers&lt;/P&gt;&lt;P&gt;VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4&lt;/P&gt;&lt;P&gt;Bus freq driver module loaded&lt;/P&gt;&lt;P&gt;Bus freq driver Enabled&lt;/P&gt;&lt;P&gt;mxc_dvfs_core_probe&lt;/P&gt;&lt;P&gt;DVFS driver module loaded&lt;/P&gt;&lt;P&gt;regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:36:53 UTC (2213)&lt;/P&gt;&lt;P&gt;EXT3-fs: barriers not enabled&lt;/P&gt;&lt;P&gt;kjournald starting.&amp;nbsp; Commit interval 5 seconds&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p1): using internal journal&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p1): 8 orphan inodes deleted&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p1): recovery complete&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p1): mounted filesystem with writeback data mode&lt;/P&gt;&lt;P&gt;VFS: Mounted root (ext3 filesystem) on device 179:1.&lt;/P&gt;&lt;P&gt;Freeing init memory: 204K&lt;/P&gt;&lt;P&gt; * Starting network connection manager&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [ OK ]&lt;/P&gt;&lt;P&gt; * Starting configure network device security&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [ OK ]&lt;/P&gt;&lt;P&gt; * Starting mDNS/DNS-SD daemon&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [ OK ]&lt;/P&gt;&lt;P&gt; * Starting configure network device&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [ OK ]&lt;/P&gt;&lt;P&gt; * Starting load fallback graphics devices&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [ OK ]&lt;/P&gt;&lt;P&gt; * Starting Userspace bootsplash&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [ OK ]&lt;/P&gt;&lt;P&gt; * Stopping load fallback graphics devices&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [ OK ]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; * Starting Advanced Power Management daemon...&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [ OK ]&lt;/P&gt;&lt;P&gt;Last login: Thu Jan&amp;nbsp; 1 00:31:40 UTC 1970 on tty1&lt;/P&gt;&lt;P&gt;speech-dispatcher disabled; edit /etc/default/speech-dispatcher&lt;/P&gt;&lt;P&gt;Checking for running unattended-upgrades:&lt;/P&gt;&lt;P&gt;Welcome to Linaro 11.10 (development branch) (GNU/Linux 3.0.35-2310-gc27cb38 armv7l)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt; * Documentation:&amp;nbsp; &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://wiki.linaro.org/"&gt;https://wiki.linaro.org/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;New release '12.04 LTS' available.&lt;/P&gt;&lt;P&gt;Run 'do-release-upgrade' to upgrade to it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; * Starting bluetooth&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root@linaro-ubuntu-desktop:~#&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [ OK ]&lt;/P&gt;&lt;P&gt; * PulseAudio configured for per-user sessions&lt;/P&gt;&lt;P&gt;saned disabled; edit /etc/default/saned&lt;/P&gt;&lt;P&gt; 1 Jan 00:37:14 ntpdate[5639]: no servers can be used, exiting&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@linaro-ubuntu-desktop:~#&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on it since 3 days now -_- with no solution found.&lt;/P&gt;&lt;P&gt;Thanks for you help.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2013 14:57:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255787#M24408</guid>
      <dc:creator>jbd64</dc:creator>
      <dc:date>2013-04-08T14:57:00Z</dc:date>
    </item>
    <item>
      <title>Re: No display on SabreSD imx6 with u boot configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255788#M24409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Try this in your u-boot config:&lt;/P&gt;&lt;P&gt;video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb1:off&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2013 20:31:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255788#M24409</guid>
      <dc:creator>varsmolta</dc:creator>
      <dc:date>2013-04-08T20:31:53Z</dc:date>
    </item>
    <item>
      <title>Re: No display on SabreSD imx6 with u boot configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255789#M24410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;I tried it already, with no success.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2013 20:47:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255789#M24410</guid>
      <dc:creator>jbd64</dc:creator>
      <dc:date>2013-04-08T20:47:29Z</dc:date>
    </item>
    <item>
      <title>Re: No display on SabreSD imx6 with u boot configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255790#M24411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;naive question: are you connecting the LVDS into LVDS0 (the one between the MIC connector and the USB OTG)? LVDS0 is the default for linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2013 20:50:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255790#M24411</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2013-04-08T20:50:11Z</dc:date>
    </item>
    <item>
      <title>Re: No display on SabreSD imx6 with u boot configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255791#M24412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't know, i'll check this tomorrow.&lt;/P&gt;&lt;P&gt;Any other idea ?&lt;/P&gt;&lt;P&gt;My mentor found the solution 3 month ago but he forgot the solution.&lt;/P&gt;&lt;P&gt;So it can works.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2013 21:36:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255791#M24412</guid>
      <dc:creator>jbd64</dc:creator>
      <dc:date>2013-04-08T21:36:50Z</dc:date>
    </item>
    <item>
      <title>Re: No display on SabreSD imx6 with u boot configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255792#M24413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, LVDS screen is connected into LVDS1.&lt;/P&gt;&lt;P&gt;(I already tested video=mxcfb1:dev=ldb... video=mxcfb0:off ...)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2013 06:57:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255792#M24413</guid>
      <dc:creator>jbd64</dc:creator>
      <dc:date>2013-04-09T06:57:23Z</dc:date>
    </item>
    <item>
      <title>Re: No display on SabreSD imx6 with u boot configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255793#M24414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you booting Linux, right? if that is the case, then the touch screen should be on LVDS0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2013 15:22:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255793#M24414</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2013-04-09T15:22:01Z</dc:date>
    </item>
    <item>
      <title>Re: No display on SabreSD imx6 with u boot configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255794#M24415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes i'm booting Linux.&lt;/P&gt;&lt;P&gt;LVDS1 is written on the board, close to the port where the screen is plugged.&lt;/P&gt;&lt;P&gt;This is the original configuration, i've made no modification.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2013 15:31:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255794#M24415</guid>
      <dc:creator>jbd64</dc:creator>
      <dc:date>2013-04-09T15:31:03Z</dc:date>
    </item>
    <item>
      <title>Re: No display on SabreSD imx6 with u boot configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255795#M24416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;try adding the following to your bootargs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fbmem=10M vmalloc=400M no_console_suspend&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Apr 2013 00:37:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255795#M24416</guid>
      <dc:creator>varsmolta</dc:creator>
      <dc:date>2013-04-10T00:37:49Z</dc:date>
    </item>
    <item>
      <title>Re: No display on SabreSD imx6 with u boot configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255796#M24417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, but Leonardo already found the solution.&lt;/P&gt;&lt;P&gt;As he said, LVDS0 is the default port for Linux and screen was plugged on LVDS1.&lt;/P&gt;&lt;P&gt;Hence, when I plug on LVDS0 it works.&lt;/P&gt;&lt;P&gt;If someone wants to play with LVDS1, you have to add this option to the kernel command line : ldb=dul0&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Apr 2013 05:23:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-display-on-SabreSD-imx6-with-u-boot-configuration/m-p/255796#M24417</guid>
      <dc:creator>jbd64</dc:creator>
      <dc:date>2013-04-10T05:23:45Z</dc:date>
    </item>
  </channel>
</rss>