<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: ahab_close error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ahab-close-error/m-p/2320110#M244088</link>
    <description>&lt;P&gt;Hi, we are experiencing exactly the same failure. Can you please share the solution with me?&lt;/P&gt;</description>
    <pubDate>Thu, 19 Feb 2026 08:49:40 GMT</pubDate>
    <dc:creator>luca_calligaris</dc:creator>
    <dc:date>2026-02-19T08:49:40Z</dc:date>
    <item>
      <title>ahab_close error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ahab-close-error/m-p/2053283#M234570</link>
      <description>&lt;P&gt;I'm getting the following error when trying to close my board. What would cause this error?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;=&amp;gt; ahab_status
Lifecycle: 0x00000008, OEM Open


        No Events Found!
=&amp;gt; ahab_close
Warning: Please ensure your sample is in NXP closed state, OEM SRK hash has been fused, 
         and you are able to boot a signed image successfully without any SECO events reported.
         If not, your sample will be unrecoverable.

Really perform this operation? &amp;lt;y/N&amp;gt;
y
Error: ele_forward_lifecycle: ret -5, life_cycle 0x8, response 0xbb29
Error in forward lifecycle to OEM closed
exit not allowed from main input shell.&lt;/PRE&gt;&lt;P&gt;I also tried using nxpele with similar results.&lt;/P&gt;&lt;PRE&gt;~/src/imx-yocto-bsp-secureboot/build/tmp/deploy/images/imx8ulp-lpddr4-evk/imx-boot-tools/files$ sudo /home/ddresser/src/venv/bin/nxpele -f mimx8ulp forward-lifecycle-update -l OEM_CLOSED 
[sudo] password for ddresser:                                                                                                                                                                                     
ERROR:UUUState:Command FB:UCMD ele_message 0x80000000 0x20000 0602951708000000 failed with error code -1 (477ms since start, spsdk_uuu.py:106)                                                                    
SPSDKError: SPSDK: ELE Message failed.                                                                                                                                                                            
Command:         ELE_FWD_LIFECYCLE_UP_REQ - (0x95)                                                                                                                                                                
Command words:   2                                                                                                                                                                                                
Command data:    False                                                                                                                                                                                            
Response words:  2                                                                                                                                                                                                
Response data:   False                                                                                                                                                                                            
Response status: Failure                                                                                                                                                                                          
   Response indication: ELE_AUTH_SKIPPED_OR_FAILED_FAILURE_IND - (0xbb)                                                                                                                                           
   Response abort code: 0x0 &lt;/PRE&gt;</description>
      <pubDate>Thu, 27 Feb 2025 20:41:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ahab-close-error/m-p/2053283#M234570</guid>
      <dc:creator>dd_neu</dc:creator>
      <dc:date>2025-02-27T20:41:23Z</dc:date>
    </item>
    <item>
      <title>Re: ahab_close error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ahab-close-error/m-p/2055124#M234684</link>
      <description>&lt;P&gt;I've replied back to you in system email.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please let me know if you need further support.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Tue, 04 Mar 2025 02:27:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ahab-close-error/m-p/2055124#M234684</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-03-04T02:27:54Z</dc:date>
    </item>
    <item>
      <title>Re: ahab_close error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ahab-close-error/m-p/2171189#M240776</link>
      <description>&lt;P&gt;Hi, I'm seeing the same error code when attempting to forward the lifecycle from OEM open to OEM closed on an i.MX93 from userspace.&lt;BR /&gt;&lt;BR /&gt;My current sequence is:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Flash a secure boot image following the NXP security reference design with AHAB enabled and the kernel image in a signed container.&lt;/LI&gt;&lt;LI&gt;From userspace, burn in SRKH efuses using the imx-secure-enclave library&lt;/LI&gt;&lt;LI&gt;Attempt to forward the lifecycle to OEM closed now that the SRKH efuses are burned in.&lt;BR /&gt;At this point, I see the 0xbb29 error and I have to reboot before I can successfully forward the lifecycle.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Is there a process that would allow burning in the SRKH efuses and forwarding the lifecycle in a single boot, or is it inherently necessary to reboot between these steps (maybe to clear the ELE lifecycle events from the initial boot without the SRKH fuses burned)?&lt;/P&gt;</description>
      <pubDate>Wed, 17 Sep 2025 14:28:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ahab-close-error/m-p/2171189#M240776</guid>
      <dc:creator>devanlec</dc:creator>
      <dc:date>2025-09-17T14:28:19Z</dc:date>
    </item>
    <item>
      <title>Re: ahab_close error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ahab-close-error/m-p/2320110#M244088</link>
      <description>&lt;P&gt;Hi, we are experiencing exactly the same failure. Can you please share the solution with me?&lt;/P&gt;</description>
      <pubDate>Thu, 19 Feb 2026 08:49:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ahab-close-error/m-p/2320110#M244088</guid>
      <dc:creator>luca_calligaris</dc:creator>
      <dc:date>2026-02-19T08:49:40Z</dc:date>
    </item>
  </channel>
</rss>