<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8QM Display port in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-Display-port/m-p/2313365#M243884</link>
    <description>&lt;P&gt;this firmware is align to the nxp official bsp, I suggest that you can use nxp official bsp version&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 06 Feb 2026 04:21:12 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2026-02-06T04:21:12Z</dc:date>
    <item>
      <title>IMX8QM Display port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-Display-port/m-p/2306580#M243836</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to use the display port with an IMX8QM on a custom board.&lt;/P&gt;&lt;P&gt;With the kernel from freescale 6.6.101 and the last dpfw.bin I am getting the following errors :&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;[drm] Started firmware!&lt;BR /&gt;[drm] set maximum defer retry to 5&lt;BR /&gt;[drm] HDP FW Version - ver 35083 verlib 20560&lt;BR /&gt;[drm] Only HDCP 2.2 is enabled&lt;/P&gt;&lt;P&gt;[ 117.275150] cdns-mhdp-imx 56268000.hdmi: [drm:cdns_mhdp_mailbox_validate_receive [cdns_mhdp_drmcore]] Hmmm spurious mailbox data maybe, cleaning out…1:2:130 vs 1:2:2&lt;BR /&gt;[ 117.300044] cdns-mhdp-imx 56268000.hdmi: [drm:cdns_mhdp_mailbox_validate_receive [cdns_mhdp_drmcore]] Hmmm spurious mailbox data maybe, cleaning out…1:2:130 vs 1:2:2&lt;BR /&gt;[ 117.324855] cdns-mhdp-imx 56268000.hdmi: [drm:cdns_mhdp_mailbox_validate_receive [cdns_mhdp_drmcore]] Hmmm spurious mailbox data maybe, cleaning out…1:2:130 vs 1:2:2&lt;BR /&gt;[ 117.349728] cdns-mhdp-imx 56268000.hdmi: [drm:cdns_mhdp_mailbox_validate_receive [cdns_mhdp_drmcore]] Hmmm spurious mailbox data maybe, cleaning out…1:2:130 vs 1:2:2&lt;BR /&gt;[ 117.367633] cdns-mhdp-imx 56268000.hdmi: [drm:cdns_mhdp_get_edid_block [cdns_mhdp_drmcore]]&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;ERROR&lt;/EM&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;get block[0] edid failed: -22&lt;BR /&gt;[ 117.380368] [drm:cdns_dp_connector_get_modes [cdns_mhdp_drmcore]]&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;ERROR&lt;/EM&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;Invalid edid&lt;BR /&gt;[ 117.455078] cdns-mhdp-imx 56268000.hdmi: [drm:cdns_mhdp_mailbox_validate_receive [cdns_mhdp_drmcore]] Hmmm spurious mailbox data maybe, cleaning out…1:3:6 vs 1:3:5&lt;BR /&gt;[ 117.477757] cdns-mhdp-imx 56268000.hdmi: [drm:cdns_mhdp_mailbox_validate_receive [cdns_mhdp_drmcore]] Hmmm spurious mailbox data maybe, cleaning out…1:3:6 vs 1:3:5&lt;BR /&gt;[ 117.500832] cdns-mhdp-imx 56268000.hdmi: [drm:cdns_mhdp_mailbox_validate_receive [cdns_mhdp_drmcore]] Hmmm spurious mailbox data maybe, cleaning out…1:3:6 vs 1:3:5&lt;BR /&gt;[ 117.522285] cdns-mhdp-imx 56268000.hdmi: [drm:cdns_mhdp_mailbox_validate_receive [cdns_mhdp_drmcore]] Hmmm spurious mailbox data maybe, cleaning out…1:3:6 vs 1:3:5&lt;BR /&gt;[ 117.543825] cdns-mhdp-imx 56268000.hdmi: [drm:cdns_mhdp_mailbox_validate_receive [cdns_mhdp_drmcore]] Hmmm spurious mailbox data maybe, cleaning out…1:3:6 vs 1:3:5&lt;BR /&gt;[ 117.565803] cdns-mhdp-imx 56268000.hdmi: [drm:cdns_mhdp_mailbox_validate_receive [cdns_mhdp_drmcore]] Hmmm spurious mailbox data maybe, cleaning out…1:3:6 vs 1:3:5&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I tried to use others version of the dpfw without success.&lt;/P&gt;&lt;P&gt;In my dts file I use this to use the DP :&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&amp;amp;hdmi {&lt;BR /&gt;status = “okay”;&lt;BR /&gt;compatible = “cdn,imx8qm-dp”;&lt;BR /&gt;firmware-name = “dpfw.bin”;&lt;BR /&gt;lane-mapping = &amp;lt;0x1b&amp;gt;;&lt;BR /&gt;hdcp-config = &amp;lt;0x2&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The kernel error I wrote just before occur when the HPD change his level from low to high.&lt;BR /&gt;I see datas on the AUX pins of the DP.&lt;/P&gt;&lt;P&gt;With the kernel 6.6.94 and the dpfw.bin compiled from yocto the errors are identical.&lt;/P&gt;&lt;P&gt;Any idea ?&lt;/P&gt;</description>
      <pubDate>Wed, 04 Feb 2026 11:12:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-Display-port/m-p/2306580#M243836</guid>
      <dc:creator>Rbe78</dc:creator>
      <dc:date>2026-02-04T11:12:57Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM Display port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-Display-port/m-p/2313365#M243884</link>
      <description>&lt;P&gt;this firmware is align to the nxp official bsp, I suggest that you can use nxp official bsp version&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 06 Feb 2026 04:21:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-Display-port/m-p/2313365#M243884</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2026-02-06T04:21:12Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM Display port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-Display-port/m-p/2317922#M244029</link>
      <description>&lt;P&gt;I just tried the kernel in the package gived by NXP : L6.6.52_2.2.2_MX8QM&lt;/P&gt;&lt;P&gt;The kernel 6.6.52 boots but I have now this following errors :&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;[ 5.360352] [drm] Started firmware!&lt;BR /&gt;[ 6.021326] [drm:cdns_mhdp_firmware_init_imx8qm [cdns_mhdp_imx]] *ERROR* NO HDMI FW running&lt;BR /&gt;[ 6.657181] [drm:__cdns_dp_probe [cdns_mhdp_drmcore]] *ERROR* NO dp FW running&lt;BR /&gt;[ 6.664860] imx-drm display-subsystem: failed to bind 56268000.hdmi (ops cdns_mhdp_imx_ops [cdns_mhdp_imx]): -6&lt;BR /&gt;[ 6.676112] imx-drm display-subsystem: adev bind failed: -6&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;But when I rename the file dpfw.bin the kernel displays this error :&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;[ 5.462856] cdns-mhdp-imx 56268000.hdmi: Direct firmware load for dpfw.bin failed with error -2&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The firmware looks loaded in my case but it do not run ?&lt;BR /&gt;This is the firmware I found in the package.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Thanks&lt;/P&gt;</description>
      <pubDate>Fri, 13 Feb 2026 15:31:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-Display-port/m-p/2317922#M244029</guid>
      <dc:creator>Rbe78</dc:creator>
      <dc:date>2026-02-13T15:31:43Z</dc:date>
    </item>
  </channel>
</rss>